Mooring Ropes
- Matsuura Industry Nylon cross rope for winches (8 strokes)The strongest nylon cloth (8 strokes) rope made of general fiber material. It is shock resistant, flexible, easy to handle, and has excellent wear resistance. Since it is a cross-knitted rope, it is difficult to kink and it is easy to handle because there is no untwisting. An 8-strand cloth is a ... Read MoreColor Light gray
- Intercom Marine Double braid polyester black line ropeA double braided rope made of 16-strand braided rope using a multifilament high-strength polyester material with a special double structure of inner core and outer skin. It efficiently draws out the strength of the fiber and finishes it as a double blade rope with high strength and durability. It... Read MoreColor Black
- Intercom Marine Double braid polyester color ropeA double braided rope made of 16-strand braided rope using a multifilament high-strength polyester material with a special double structure of inner core and outer skin. It efficiently draws out the strength of the fiber and finishes it as a double blade rope with high strength and durability. It... Read Morefrom S$28.99Min. 2 days
- Matsuura Industry Nylon rope for winches (3 strokes)The strongest nylon rope (3 strokes) in general fiber materials. It is shock resistant, flexible, easy to handle, and has excellent wear resistance. The thickness is 8, 9, 10, 12, 16 mmΦ. There are 50/100/200m rolls for each size. With eye processing on both ends. (Satsuma knitting process) As a ... Read MoreColor Light gray
- IKURA SEIKI Cross ropeIt is 12 strokes. Both ends have been processed. (With protective tube) For cable entryfrom S$299.90Min. 2 days
- Top Water Boats Mooring Shock SnoverAn EPDM mooring snover that acts as a shock absorber for mooring ropes. This rubber snover absorbs the force applied to the shock when an abnormal force acts on the rope due to a gust such as a typhoon and the rope is damaged. The material is a synthetic rubber called ethylene polypropylene rubbe... Read Morefrom S$47.99Min. 8 days
- Intercom Marine Chaf guardThe chaff guard is a cover that protects the rope from rubbing against fair leaders and large cleats. Normally, it may not be a concern when mooring, but in most cases, the surface of the rope is considerably damaged by the friction that is received many times during a typhoon around the fair lea... Read MoreColor White Suitable Rope Diameter (Φmm) 16~22from S$23.99Min. 8 days
- No Brand Manila rope Three-strike Cut product 18mmSold out from 1M! You can purchase it in the required length. (Both ends are fixed with vinyl tape) Excellent water resistance, durability, and abrasion resistance. Since it is a natural material, it is environmentally friendly because it corrodes in the soil and water and returns to the soil. Sh... Read MoreMaterial Sisal hemp Rope Diameter (Φmm) 18from S$8.69Min. 8 days
- Aiwa Sangyo Spindle band (cotton blend)It is a braided string with a good texture made of cotton rayon blend. It is a soft string that can be easily bound and untied. For handicrafts such as attaching flags, fixing pipe tents, sewing, etc. * During manufacturing, the yarn may be connected in the middle. * If it gets wet with water, th... Read MoreColor Generate RoHS directive (corresponding to 10 substances) Correspondencefrom S$119.90Min. 8 days
- No Brand Manila rope Three-strike Cut product 14mmSold out from 1M! You can purchase it in the required length. (Both ends are fixed with vinyl tape) Excellent water resistance, durability, and abrasion resistance. Since it is a natural material, it is environmentally friendly because it corrodes in the soil and water and returns to the soil. Sh... Read MoreMaterial Sisal hemp Rope Diameter (Φmm) 14from S$5.39Min. 8 days
- No Brand Manila Rope Three Strands Cut Product 12mmSold out from 1M! You can purchase it in the required length. (Both ends are fixed with vinyl tape) Excellent water resistance, durability, and abrasion resistance. Since it is a natural material, it is environmentally friendly because it corrodes in the soil and water and returns to the soil. Sh... Read MoreMaterial Sisal hemp Rope Diameter (Φmm) 12from S$4.29Min. 8 days
- No Brand Manila rope Three-strike Cut product 9mmSold out from 1M! You can purchase it in the required length. (Both ends are fixed with vinyl tape) Excellent water resistance, durability, and abrasion resistance. Since it is a natural material, it is environmentally friendly because it corrodes in the soil and water and returns to the soil. Sh... Read MoreMaterial Sisal hemp Rope Diameter (Φmm) 9from S$2.59Min. 8 days
- No Brand Manila Rope Three Strands Cut Product 24mmSold out from 1M! You can purchase it in the required length. (Both ends are fixed with vinyl tape) Excellent water resistance, durability, and abrasion resistance. Since it is a natural material, it is environmentally friendly because it corrodes in the soil and water and returns to the soil. Sh... Read MoreMaterial Sisal hemp Rope Diameter (Φmm) 24from S$17.99Min. 8 days
- No Brand Manila Rope Three Strands Cut Product 20mmSold out from 1M! You can purchase it in the required length. (Both ends are fixed with vinyl tape) Excellent water resistance, durability, and abrasion resistance. Since it is a natural material, it is environmentally friendly because it corrodes in the soil and water and returns to the soil. Sh... Read MoreMaterial Sisal hemp Rope Diameter (Φmm) 20from S$11.99Min. 8 days
- No Brand Manila rope Three-strike Cut product 22mmSold out from 1M! You can purchase it in the required length. (Both ends are fixed with vinyl tape) Excellent water resistance, durability, and abrasion resistance. Since it is a natural material, it is environmentally friendly because it corrodes in the soil and water and returns to the soil. Sh... Read MoreMaterial Sisal hemp Rope Diameter (Φmm) 22from S$14.99Min. 8 days
- NIPPONSENTO Manual lead measurement HK inspection productThis product has passed the inspection of the Japan Ship Equipment Certification Association (HK). It is a tool for measuring the depth of the sea, which consists of a lead weight and a rope, and it is possible to know the soil quality by collecting the earth and sand on the seabed from the dent ... Read MoreMaterial Shackle: Iron (with plating) Pin Diameter (Φmm) (Shackle) 8from S$179.90Min. 9 days
- No Brand Manual lead measurement UninspectedThis product is uncertified. It is a tool for measuring the depth of the sea, which consists of a lead weight and a rope, and it is possible to know the soil quality by collecting the earth and sand on the seabed from the dent on the bottom.Material Shackle: Iron (with plating) Maximum Diameter (Φmm) 60 (hexagon) Pin Diameter (Φmm) (Shackle) 9from S$85.99Min. 9 days
- No Brand 3-Strand Manila Rope Cut Product 16mmSold out from 1M! You can purchase it in the required length. (Both ends are fixed with vinyl tape) Excellent water resistance, durability, and abrasion resistance. Since it is a natural material, it is environmentally friendly because it corrodes in the soil and water and returns to the soil. Sh... Read MoreMaterial Sisal hemp Rope Diameter (Φmm) 16from S$6.99Min. 8 days
- Aiwa Sangyo Spindle Rope (Vinylon)It is made of vinylon, which feels good to the touch. It is highly weather resistant and can be used outdoors for a long period of time. It is a very soft material that minimizes scratches on the mounting part. For handicrafts such as attaching flags, fixing pipe tents, sewing, etc. * During manu... Read MoreColor White RoHS directive (corresponding to 10 substances) Correspondencefrom S$129.90Min. 8 days
- No Brand Manila rope Three-strike Cut product 8mmSold out from 1M! You can purchase it in the required length. (Both ends are fixed with vinyl tape) Excellent water resistance, durability, and abrasion resistance. Since it is a natural material, it is environmentally friendly because it corrodes in the soil and water and returns to the soil. Sh... Read MoreMaterial Sisal hemp Rope Diameter (Φmm) 8from S$1.89Min. 8 days
- No Brand Manila rope Three-strike Cut product 10mmSold out from 1M! You can purchase it in the required length. (Both ends are fixed with vinyl tape) Excellent water resistance, durability, and abrasion resistance. Since it is a natural material, it is environmentally friendly because it corrodes in the soil and water and returns to the soil. Sh... Read MoreMaterial Sisal hemp Rope Diameter (Φmm) 10from S$3.19Min. 8 days
- No Brand Manila rope Three-strike Cut product 6mmSold out from 1M! You can purchase it in the required length. (Both ends are fixed with vinyl tape) Excellent water resistance, durability, and abrasion resistance. Since it is a natural material, it is environmentally friendly because it corrodes in the soil and water and returns to the soil. Sh... Read MoreMaterial Sisal hemp Rope Diameter (Φmm) 6from S$1.19Min. 8 days