Boat Cleaning Supplies
Other Related Pages
- BMO Japan BaylorIt is used to pump out the water that has accumulated on the bottom of the ship. 0.75L (S size) has a flat bottom, so it is suitable for when you want to pump out water firmly or in a narrow place. 1.75L (M size) has an uneven bottom, so it is perfect when you want to roughly pump out water.Capacity (L) 0.75from S$13.99Min. 2 days
- Settsu Metallon M + DegreaserIt is used as a detergent instead of washing oil, and can clean sticky stains such as grease. Since it is formulated for use at sea, cleaning with seawater also has an excellent effect. It can be used in 2-3% solution (20-30g of this product should be dissolved in 1L of water) and machine parts w... Read MoreAcidic / Alkaline alkalinity Standard Amount to Use 20-30g for 1L of water
- Star Brite Non-skid deck cleanerThe most major boat maintenance product in the United States, Star Bright's American-made non-skid deck cleaner. A detergent specialized for washing bumpy decks to prevent slipping. Most decks are slippery, so it's a great deck cleaner. Of course, the dirt will be surprisingly removed eve... Read Morefrom S$34.99Min. 2 days
- Intercom Marine Bucket with boat lidA bucket for marine boat washing with a lid and a large capacity of 20 liters. When diluting detergent, it is very convenient because you can make a large amount at a time. Since it has a lid, you can store it as a cleaning kit if you put detergent, sponge, etc. in it.
- MDR Amazon's Amazon Golden Teak OilSpeaking of teak oil in the United States, it is the most famous Amazon golden teak oil. To clean the cheek deck, use a cheek cleaner and thoroughly clean it before use.
- Intercom Marine With premium deck brush handleThe feature of this product is a wide brush head of about 20 cm and a high density. The brush gently removes dirt from the fiberglass surface. Since we are pursuing and developing quality that is comparable to the finest deck brushes made in the United States, the quality of the brushes and the a... Read MoreHandle Dimensions (mm) 1200~2000
- Star Brite Power pine boat wash & waxStar Bright's boat soap, the most major in the US boat maintenance supplies industry. A soap that contains a waxing polymer in a boat soap that has the highest cleaning ability of Star Bright. Apply an appropriate amount to the sponge and whisk it before use. Surprisingly cleans. It can be us... Read MoreCapacity (mL) 960from S$64.99Min. 2 days
- Universal Stone Universal stoneGerman boat cleaning soap using natural materials. Robust water with gray ingredients on the body of the boat, made from plant-made flake soap, green soap, perfume oil, vegetable oil (olive oil), clay containing natural alumina and natural alumina. Firmly removes red and dirt. As an eco-friendly ... Read Morefrom S$55.99Min. 2 days
- Rupp Marine AlmagardThis product is the best anticorrosion and polish coating agent for alumite processed products such as aluminum outriggers, aluminum pipes and fishing reels, and is suitable for luxury boats in the hot and humid Miami area such as Florida on the east coast of the United States. Many products are ... Read MoreCapacity (mL) 473from S$47.99Min. 2 days
- Star Brite Sea Safe Boat WashStar Bright's boat soap, which is the most major in the US boat maintenance supplies industry. It is an environmentally friendly boat soap because of its generation and decomposition action, which is named Sea Safe. Some marina only allow this type of detergent to protect the environment. To ... Read MoreCapacity (mL) 960from S$36.99Min. 2 days
- Star Brite Clear plastic polish STEP2Star Bright's clear plastic polish (step 2) that revives the view of the enclosure that has become whitish due to aging and UV deterioration. Polish shines and protects the surface. After cleaning with a clear plastic restore (STEP1) etc., spread the liquid on a cloth, and finally wipe it off... Read MoreCapacity (mL) 240from S$33.99Min. 2 days
- Star Brite Boat & fender cleaner / protectorThe most major boat maintenance product in the United States, Star Bright's American-made boat polish. This inflatable boat & fender cleaner removes dirt on inflatable boats and fenders, dry the dirty surface and apply this cleaner to a cloth and polish it in a circular motion, it will cl... Read MoreCapacity (mL) 473from S$47.99Min. 7 days
- Star Brite Startron fuel tank cleanerStar Bright's American fuel tank cleaner, the most major boat maintenance product in the United States. In the case of diesel boats, if the boat is operating almost every day like a fishing boat, the diesel fuel will always rotate in the tank and will not deteriorate, but it only operates onc... Read MoreCapacity (L) 1.9from S$139.90Min. 2 days
- Star Brite Clear plastic restore STEP1Star Bright's clear plastic restore (step 1) that restores the view of the enclosure that has become whitish due to aging and UV deterioration. Spread the liquid on a soft, dry cloth, and wipe it off with a rag after a while. Repeat this several times depending on the whitened part of the enc... Read MoreCapacity (mL) 240from S$33.99Min. 7 days
- San-Esu Engineering Machine clean"Machine Clean" is a cleaning agent for low-pollution metal parts. Dissolve 1 kg of this product in about 40 L of water or hot water. (The optimum temperature for machine clean is 40-80 ℃) Immersion time: Immerse for at least 30 minutes before washing and rinsing thoroughly. For hard ca... Read MorepH 10.5 (3% aqueous solution) Acidic / Alkaline alkalinityfrom S$69.99Min. 8 days
- Star Brite Super orange boat washA biodegradable detergent containing an orange component. Especially for stubborn stains such as oil, grease and fish blood. It can be used from fiber to metal, and can be used not only for fresh water but also for seawater. Does not remove wax or glass coat components. The citrus scent makes boa... Read MoreCapacity (mL) 946from S$39.99Min. 2 days
- Intercom Marine Premium deck brush headThe feature of this product is a wide brush head of about 20 cm and a high density. The brush gently removes dirt from the fiberglass surface. Since we are pursuing and developing quality that is comparable to the finest deck brushes made in the United States, the quality of the brushes and the a... Read Morefrom S$57.99Min. 7 days
- Star Brite MILDEW stain removerFor boat soap, it is a mildew remover for vinyl cushions and covers from Star Bright, which has a good reputation in the United States. It is the number one remover among these mold removers. 【how to use】 Spray directly onto a damp cabinet, canvas, vinyl or other moldy area, and rinse well with... Read MoreCapacity (mL) 650from S$39.99Min. 7 days
- Star Brite Power pine boat washThe most major American boat soap from Star Bright in the US boat maintenance supplies industry. It is the boat soap with the highest cleaning ability in Star Bright. Apply an appropriate amount to the sponge and whisk it before use. Surprisingly cleans. It can be used anywhere from fiberglass on... Read MoreCapacity (mL) 960from S$47.99Min. 7 days
- Star Brite Last Stain RemoverStar Bright's rust remover, which has a good reputation in the United States for boat soap. This "Last Stain Remover" is the most effective when metal rust and the rust adhere to the fiberglass. Simply spraying this remover on the rust on the hull, palpit, stainless rails, stainless... Read MoreCapacity (mL) 650
- Intercom Marine With scrub pad handleIt is a scrub pad suitable for cleaning the glass fiber hull and has a handle, so it is easy to apply force and it is easy to use. Be sure to keep it wet before use.Dimensions (cm) 15×9from S$7.29Min. 7 days
- Star Brite Screen Cleaner & ProtectantThe most major boat maintenance product in the United States, Star Bright's American-made screen cleaner and protectant. Very easy to use. Just spray it on the screen and wipe it off. After removing fingerprints, salt and dirt on the liquid crystal surface, it is coated with fluorine to prote... Read MoreCapacity (mL) 273from S$29.99Min. 7 days
- Collinite 870 Fleet Wax LiquidIt is the highest grade wax selected as the number one boat wax in the United States in 2007 by Collinite of the United States, which is said to be the number one wax manufacturer for marine in the world. It is a convenient professional wax that shines the hull and protects the hull for a long pe... Read MoreCapacity (mL) 473from S$63.99Min. 7 days
- Star Brite Fiberglass stain removerStar Bright's fiberglass stain remover, which has a good reputation in the United States for boat soap. Removes yellowing of fiberglass hulls and dirt near the waterline. Since it is a little gel-like, it can be used not only on parallel surfaces but also on vertical surfaces. 【how to use】 ... Read MoreCapacity (mL) 946from S$63.99Min. 7 days
- Star Brite Startron Fuel TreatmentThe most major boat maintenance product in the United States, Star Bright's American-made fuel treatment. This startron diesel fuel additive is a product developed for the purpose of keeping light oil in the best condition, it restores old light oil and evaporates the water in the tank. It al... Read MoreCapacity (mL) 240from S$47.99Min. 7 days
- Collinite 850 Metal WaxMetal wax from Collinite of the United States, which is said to be the number one marine wax manufacturer in the world. Metal wax for metals restores the brilliance of aluminum and stainless steel, which has lost its luster after being exposed to salt for a long period of time.Capacity (mL) 473from S$39.99Min. 7 days
- Shimada Oil absorbent blue sea mat ecoUses natural fiber (cotton). It is an oil adsorbent that is friendly to humans and the environment because there is no concern about toxic gas due to the material used during incineration. Since it is an excellent adsorbent, even a small amount can produce a great effect, and it is economical at ... Read MoreSize (mm) (Adsorbent) 500 × 500 × 4 Mass (kg) 10 Number of Page 120 sheets Eco Mark Certification Number 9105004 Absorption Capacity About 144L / case Eco Mark Certification Certificationfrom S$299.90Min. 7 days
- Collinite 920 fiberglass boat cleanerHeadquartered in New York, USA, Collinite, which has a history of 75 years, produces the finest automobiles and boat waxes. The marine wax produced by this manufacturer uses the best materials to block UV and dust for a long period of time. This 920 fiberglass boat cleaner is a cleaner that remov... Read MoreCapacity (mL) 473from S$29.99Min. 7 days
- Star Brite Corrosion BlockerA metal corrosion inhibitor manufactured by Star Bright. Mooring boats are constantly corroded faster than usual in harsh environments due to high humidity and salt in seawater. If you use this collision blocker to protect your important engine room, you can prevent corrosion and stop corroded pa... Read MoreCapacity (mL) 650from S$55.99Min. 7 days
- Collinite Te885 heavy duty fleet wax pasteHeadquartered in New York, USA, Collinite, which has a history of 75 years, produces the finest automobiles and boat waxes. The marine wax produced by this manufacturer uses the best materials to block UV and dust for a long period of time. This 885 Heavy Duty Fleet Wax is the finest paste wax fo... Read MoreMass (g) 336from S$63.99Min. 7 days
- Collinite 855 leather & vinyl waxHeadquartered in New York, USA, Collinite, which has a history of 75 years, produces the finest automobiles and boat waxes. The marine wax produced by this manufacturer uses the best materials to block UV and dust for a long period of time. This 855 Leather & Vinyl Wax removes dirt from leath... Read MoreCapacity (mL) 473from S$45.99Min. 7 days
- Star Brite Extreme cleanIt is the most major detergent from Star Bright in the US boat maintenance supplies industry. Extreme Clean is a detergent that can remove stubborn stains on vinyl, fiberglass, plastic, rubber, metal, carpets and painted surfaces. To use it, put a 3-cap cleaner in a bucket and wipe it with a clot... Read MoreCapacity (mL) 650from S$39.99Min. 7 days
- Star Brite Premium MARINE POLISHStar Bright's American boat polish, the most major boat maintenance product in the United States. This marine polish contains fluororesin and coats the hull's fiberglass, metal and plastic like Teflon to block UV and give it an amazing luster and luster. The effect lasts for about a year.... Read MoreCapacity (mL) 960from S$98.99Min. 2 days
- Star Brite Premium MARINE POLISH PTFE (Boat Polisher)Star Bright's American boat polish, the most major boat maintenance product in the United States. This marine polish contains fluororesin and coats the hull's fiberglass, metal and plastic like Teflon to block UV and give it an amazing luster and luster. The effect lasts for about a year.... Read MoreCapacity (mL) 480from S$64.99Min. 2 days
- Star Brite Star Bright Carpet Clean PTFFA cleaner for boat carpets manufactured by Star Bright in the United States. It's okay because it's barefoot, and if you go in and out of the deck and cabin with barefoot, the deck is outdoors, so dirt and dust will adhere to your barefoot and cause the carpet to get dirty. In the case of... Read MoreCapacity (mL) 650from S$36.99Min. 7 days
- Intercom Marine Premium Deck Brush Economy 10 inch Soft Yellow Set with handleThe head part is made of plastic resin, so it does not grow mold and does not fade. As it is a soft type deck brush, you can wash the inside of the ship softly and gently. The brush width is about 25 cm. The attached handle is 100 cm to 180 cm. The handle is a telescopic type, and the brush is ea... Read MoreBrush Width (mm) 250 Length (cm) Handle: 100-180from S$69.99Min. 7 days
- Intercom Marine With marine deck brush light handleThe feature of this product is a dense brush that gently cleans the inside of the boat and thoroughly removes dirt from the fiberglass surface. There are two types of brushes, soft (yellow) and medium (blue). Use soft brushes for hulls and medium brushes for gel coat surfaces on decks. The attach... Read MoreDiscontinued
- Star Brite Odergard Surface ScreenerThe most major boat maintenance product in the United States, Star Bright's American-made Oda Guard surface cleaner. A deodorant and disinfectant spray developed by Star Bright for boats. Bacteria outbreak in a closed boat cabin due to high heat and humidity. As a result, the area around the ... Read MoreCapacity (mL) 650Discontinued