Uses 316 stainless steel Φ25mm pipe that does not rust easily! A foldable stainless steel ladder that can be used by fixing it to a transom. The fixed blanket to the boat can be mounted on both vertical and horizontal surfaces. Because it is compact, it is also ideal for small boats with a narrow... Read More
The sealing material is designed to prevent water from entering. Two sizes, 4-inch type and 6-inch type, are available.
* Since it is not completely waterproof, do not install it in places where water intrusion is a problem.
Attach it to the deck or wall of a boat to make effective dead space! Water does not easily enter due to the sealing material!
* Since it is not completely waterproof, do not install it in places where water intrusion is a problem.
Made of marine grade SUS316. A marine grade SUS316 Φ22mm handrail that can be used as an assist grip when getting on and off the boat and when maneuvering, or as a base for rod holders for rail mounting.
The swivel window is a window that is attached to the windshield of a ship to disperse rain and snow and waves at high speed of the screen to ensure visibility.
An access hatch made of ABS (acrylonitrile, butadiene, styrene) resin that is strong against impact and has excellent durability. If you attach it to the deck of the boat, you can use the dead space in the boat that was previously inaccessible as a storage. It can be used in various ways, such as... Read More
Dimension h1 (mm) 192 Dimension H (mm) 270 Dimension L1 (mm) 291 Dimension L (mm) 375
An access hatch made of ABS (acrylonitrile, butadiene, styrene) resin that is strong against impact and has excellent durability. If you attach it to the deck of the boat, you can use the dead space in the boat that was previously inaccessible as a storage. It can be used in various ways, such as... Read More
A gunwale type rudder made of sturdy 316 stainless steel that can withstand the boat environment. By freely changing the angle of the mounting part, it can be stored compactly without waste even if it is fixed during storage. You can use it as it is if it can be hooked on the side gunwale of the ... Read More
Material Made of 316 stainless steel Width (cm) Maximum: 25
A motor is attached to the center of the circular glass, and the centrifugal force generated by rotating it is used to scatter water droplets and snow to ensure visibility.
A device that secures visibility by shaking off water droplets and snow that adhere to the entire window of the cockpit of a... Read More
It is an inspection port (inspection port / inspection hatch) made of ABS (acrylonitrile, butadiene, styrene) resin that is strong against impact and has excellent durability. It can be opened and closed by turning the lid, and the O-ring built into the base part enhances waterproofness.
The new rotation mechanism has greatly improved visibility. You don't have to worry about "hard to see" or "hit your head against the motor". The swivel window can be attached to the front glass of a ship, etc., and rain, snow, and waves can be scattered by the high-speed ... Read More