Rods, Fishing Rods
- MajorCraft Exhaust 5GA standard egging model that is often used throughout the year. It is a model with a wide strike zone that can handle small bait trees around 2.5 to deep type bait trees of 3.5. The blank, which can produce a sharp dirt, also has the flexibility to keep the caught squid from falling apart. M-seriesOperation Action: Regular Fast Size (Nominal No.) Egi: 2.0-4.0, PE line: 0.4-1.2 Specification Joint number: 2pcsfrom S$349.90Min. 10 days
- MajorCraft Crossride 5GA power game model that can aim for amberjack and migratory fish from the beach. It features not only strong butt power, but also a sticky berry part that can hook into the hard mouth of large fish. A full-fledged Rocky Shore game model that also has a flexible tip with excellent operability of a... Read MoreOverall Length 10'0”ft Operation Action: Regular Fast Specification Joint number: 2pcs Mass (g) Lure: 100±20 Size (Nominal No.) PE line: 1.5-4.0from S$459.90Min. 10 days
- MajorCraft Crostage SurfIt is the best model for aiming flounder on wave-dissipating blocks and reef zones. This length, which is light and maneuverable, technically captures flounder that has reached the pin spot while feeling changes in the bottom and tide. Of course, it also has a strong butt power that pulls flounde... Read Morenumber of joint shafts 2 Overall Length 9 feet 8 inches Suitable for Lure: 10-45g, Line: 8-20lb, PE0.8-2 Operation Regular Fastfrom S$239.90Min. 10 days
- MajorCraft Crostage SurfIn recent years, it is a popular long rod standard length. This model is for shallow surf, high tide, and rough conditions with high waves. Lightweight and sharp blanks that can be used to cast jigs and vibrations to explore a wide range have outstanding swing-through and operability. I would lik... Read MoreOverall Length 10 feet 6 inches number of joint shafts 2 Suitable for Lure: 10-45g, Line: 8-20lb, PE0.8-2 Operation Regular Fastfrom S$269.90Min. 10 days
- MajorCraft Solpara JiggingIt is the best model for using jigs around 150g. It will be active in areas with a depth of around 100m and points where the tide moves quickly. It is a must-have for aiming at large green objects.Overall Length 6'0”ft Operation Action: Regular Fast Specification Joint: Grip detachment Mass (g) Lure: 100-180 Size (Nominal No.) PE line: 2-4from S$189.90Min. 10 days
- MajorCraft Solpara JiggingThe most basic spinning model for inshore jigging. Ideal for fishing that uses a jig of around 120g and operates the jig with one pitch. Bat power that does not lose even in a fight with yellowtail is attractive.Overall Length 6'0”ft Operation Action: Regular Fast Specification Joint: Grip detachment Mass (g) Lure: 80-150 Size (Nominal No.) PE line: 1.5-3from S$189.90Min. 10 days
- MajorCraft Solpara Sea BassIt is a model that produces a long cast. The bat power that can shake off a slightly heavy metal vibe and spin tail jig is still alive when aiming for blue objects.Overall Length 10' 0”ft Operation Action: Regular Specification Joint number: 2pcs, Line: 8-20lb Mass (g) Lure: 15-42 Size (Nominal No.) PE line: 0.8-2.0from S$189.90Min. 10 days
- MajorCraft Firstcast Sea BassRecommended for fishing with 10-20g lures. It can also be used for standard sea bass games, rubber jigs and metal vibes for black sea bream, casting jigs for barracuda and mackerel, and jig head warming for flounder and root fish. In addition to lures, we also recommend kissing with Choi throwing... Read Morenumber of joint shafts 2 Overall Length 8 feet 6 inches Suitable for Lure: 7-23g, Line: 6-12lb, PE0.6-1.2 Operation Regular Fastfrom S$139.90Min. 10 days
- MajorCraft Crossstage sea bassEveryone will experience severe scenes where accurate casting greatly affects the hit rate. This model is excellent in such accuracy performance. It supports a wide range from slightly lighter minnows to metal vibes. Especially in the harbor area, where structures are often attacked tight, this m... Read Morenumber of joint shafts 2 Overall Length 8 feet 6 inches Suitable for Lure: 7-23g, Line: 6-12lb, PE 0.6-1.5 Operation Regular Fastfrom S$199.90Min. 10 days
- MajorCraft Crostage FunoctopusThis is a special model for targeting octopus from a boat. Ideal for fishing with octopus tenya and octopus egi. It features a soft glass material tip that holds the device without giving the octopus a sense of incongruity, and a powerful butt that can be reliably hung. If you want to aim right u... Read Morenumber of joint shafts 2 Overall Length 5 feet 0 inches Operation Fast Suitable for Lure: 30-60/110-230g, PE1-4from S$189.90Min. 10 days
- MajorCraft Crostage Magnum BaitIt is a model aiming for a larger ranker with a big bait or a giant bait with a Konoshiro pattern. In addition to the operability of all lures such as just reeling, jerk, drift, and giant top water plugs, it is designed to emphasize the bite and riding of ranker sea bass. You will be amazed at ho... Read Morenumber of joint shafts 2 Overall Length 6 feet 8 inches Suitable for Lure: 56-250g, Line: MAX50lb, PE2.8-8.0 Operation Regularfrom S$229.90Min. 10 days
- MajorCraft Crostage Egging modelIt is a standard model that is no longer explained. The secret to the popularity of the 862E, which is the most popular versatile model for all situations, is its exquisite balance of hardness and length. It has both butt power for targeting big squid in spring and delicate sensitivity and castin... Read Morenumber of joint shafts 2 Overall Length 8 feet 6 inches Suitable for Egg No. 2.5 to 3.5, PE No. 0.4 to 1.2 Operation Regular Fastfrom S$199.90Min. 10 days
- MajorCraft Sorpara Kishi OctopusThis model is recommended if you want to shoot the octopus lurking at your feet. It is ideal for "Tektro", where you aim for octopuses hidden between the embankment and the seabed while walking, and for fishing where you aim for octopuses that stick to the side of the embankment while d... Read MoreOverall Length 7'0”ft Operation Action: Regular Fast Specification Joint number: 2pcs Mass (g) Lure: MAX56 Size (Nominal No.) PE line: 2.0-5.0from S$159.90Min. 10 days
- MajorCraft Crostage Hairtail WINDThis model is perfect for beginners to wind games. Especially for women and junior anglers, the length is set just right for enjoying the wind. The slightly short blank makes it easy to produce a light dart with a little force, and the swing through when casting is outstanding. We recommend this ... Read Morenumber of joint shafts 2 Overall Length 8 feet 0 inches Suitable for Lure: 7-21g, PE 0.6-1.5 Operation Regular Fastfrom S$199.90Min. 10 days
- MajorCraft crossstage light jiggingIt is a model that aims at sea bass and hairtail with a jig up to 180g in a deep area with a depth of over 50m. If you are an angler with a lot of jigging experience, this is a model that you would like to enjoy a thrilling fight with a medium-sized blue-runner with a light tackle.number of joint shafts 1 Overall Length 6 feet 4 inches Operation Fast Type Grip detachable Suitable for Lure: 80-180g, PE0.8-1.5from S$199.90Min. 10 days
- MajorCraft Firstcast Light Game MEBARUThis model, which uses a solid tip that bites well, is the best one for rockfish and scorpion fish using a 1-2g jig head. This model, which excels in long-distance casting performance, demonstrates its power in wide fishing harbors, outside harbors, and high footing points. It is characterized by... Read MoreOverall Length 7'6”ft Operation Action: EX.Fast Specification Joint number: 2pcs, Line: 1-5lb Mass (g) Lure: 0.4-5 Size (Nominal No.) PE line: 0.1-0.6from S$109.90Min. 10 days
- MajorCraft Solpara boat octopus BAIT modelIt is a model dedicated to octopus fishing that targets using octopus egi and sutte from popular boats. The delicate tip part makes it possible to feel even the legs of the octopus entwined with the lure. The butt power that separates the octopus from the bottom of the sea at the same time as the... Read MoreOverall Length 5'6”ft Operation Action/1:9 Specification Joint number: 2pcs Size (Nominal No.) Lure: MAX60from S$159.90Min. 10 days
- MajorCraft Triple Cross Aging Tubular ModelThe high operability that cannot be experienced with a solid tip is a feature of the tubular type. This length was developed to give fine action to the lure. Once you experience a high-sensitivity blank that does not miss even the slightest bite, you will surely become addicted. It is perfect not... Read MoreOverall Length 6'8”ft Operation Action: Fast Specification Joint number: 2pcs, Line: 1-5lb Mass (g) Lure: 0.6-10 Size (Nominal No.) PE line: 0.1-0.6from S$239.90Min. 10 days
- MajorCraft Triple cross Aging solid tip modelThe length of 5 feet 8 inches is easy to handle and has excellent sensitivity performance. There is no model that will be such a big weapon in close range combat. It is a technical model that allows you to enjoy a direct operation feeling, so it is perfect for a number fishing game. Let's att... Read MoreOverall Length 5'8”ft Operation Action: EX.Fast Specification Joint number: 2pcs, Line: 1-5lb Mass (g) Lure: 0.6-10 Size (Nominal No.) PE line: 0.1-0.6from S$229.90Min. 10 days
- MajorCraft Solpara light jigging SPINNING modelUsing a jig of around 100g in the coastal waters (bay area), this model is ideal for sea bass and small blue-runners (mackerel, sagoshi, yellowtail). It is recommended for high-pitch action that makes use of the characteristics of spinning.Overall Length 6'4”ft Operation Action: Regular Fast Specification Joint: Grip detachment Mass (g) Lure: 60-150 Size (Nominal No.) PE line: 0.6-1.5from S$179.90Min. 10 days
- MajorCraft Crossstage Light Game AJI SOLID TIP modelIt is a standard model that emphasizes handling that hangs with the jig head alone. It is ideal for short game of horse mackerel that gathers at the light of the fishing port, and jigging that aims at a large horse mackerel that migrates outside the embankment at a good tempo.number of joint shafts 2 Overall Length 6 feet 4 inches Operation EX.Fast Suitable for Lure: 0.6-10g, Line: 1-5lb, PE0.1-0.6from S$189.90Min. 10 days
- MajorCraft Crossstage light game MEBARU TUBULAR modelSince it is a tubular model with tension, it is excellent in operability of micro jigs. In addition, the length that makes it easy to act is an exquisite setting that allows you to immediately hook the fall bite. Please capture the big rockfish by mebaring with a micro jig.number of joint shafts 2 Overall Length 7 feet 6 inches Suitable for Lure: 0.8-10g, Line: 2-8lb, PE0.3-0.8 Operation Regular Fastfrom S$189.90Min. 10 days
- MajorCraft Crossstage light game MEBARU TUBULAR modelIn mebaring, there are surprisingly many situations where long casts are required. For example, you can use sinking pencils and float rigs to cast long distances on shallow spots such as gorota fields and shallow seaweed beds. This works for decaval. Of course, compatibility with micro jigs is al... Read Morenumber of joint shafts 2 Overall Length 7 feet 9 inches Operation Fast Suitable for Lure: 0.5-7g, Line: 1-6lb, PE0.2-0.6from S$189.90Min. 10 days
- MajorCraft Crostage squid metal (lead sutte) SPINNINGIt is a model for exclusive use of the squid metal game aiming at spinning tackle. This model, which is a standard spinning model, is good at inviting the fall by making use of its length. This length is essential for aiming for the most responsive squid in stays and falls.number of joint shafts 2 Overall Length 7 feet 0 inches Operation EX.Fast Suitable for Lure: No. 8-15/20-60g, PE No. 0.4-1.0from S$199.90Min. 10 days
- MajorCraft Crossstage shore jigging shore jigging modelThere are many places where the tide is fast, and a metal jig of around 80g is required to capture there. This model is a torqueful one that can handle such situations, and the butt part boasts outstanding lift power due to the cross force manufacturing method. Experience its potential.number of joint shafts 2 Overall Length 9 feet 6 inches Suitable for Lure: 80g, PE1.5-3.5 Operation Regularfrom S$269.90Min. 10 days
- MajorCraft Crossstage shore jigging shore jigging modelThis is a versatile model that can be used regardless of whether it is an embankment, a surf, a rocky shore, or a field! This model is the best match because metal jigs around 60g are often the main ones in shore jigging. I'm sure it will be one you can't let go of.Overall Length 10 feet 0 inches number of joint shafts 2 Suitable for Lure: 60g, PE1.0-3.0 Operation Regularfrom S$269.90Min. 10 days
- MajorCraft Crossstage shore jigging shore jigging modelIf you want to cast a metal jig around 60g long, this model will be effective. Also, this length is effective for fishing from embankments with high scaffolding and rocky shores. I want you to cast the metal jig as far as you can and attack the migratory fish that run around.Overall Length 10 feet 6 inches number of joint shafts 2 Suitable for Lure: 60g, PE1.0-3.0 Operation Regularfrom S$299.90Min. 10 days
- MajorCraft Triple Cross Shore Jigging LIGHT SHORE JIGGINGLSJ that can be enjoyed in various fields. Long throw performance that is also active in shallow points such as surf.Overall Length 10'0”ft Operation Action: Regular Fast Specification Joint number: 2pcs Mass (g) Lure: 40±20 Size (Nominal No.) PE line: 1-2.5from S$299.90Min. 10 days
- MajorCraft Crossstage shore jigging light shore jigging modelIn shore jigging, the long casting power sometimes directly affects the fishing results. For example, in a shallow surf, whether or not you can reach the offshore nabla will be the turning point of the game. This model has excellent long cast performance, so please do not miss it.Overall Length 10 feet 0 inches number of joint shafts 2 Suitable for Lure: 40g, PE1.0-2.5 Operation Regular Fastfrom S$259.90Min. 10 days
- MajorCraft Triple Cross Shore Jigging SHORE SLOW & SHORE RUBBERDeveloped on the premise of using SRJ exclusive lures such as jig grabbers. Shore slow jigging with this one.Overall Length 9'6”ft Operation Action: Regular Fast Specification Joint number: 2pcs Mass (g) Lure: 20-40 Size (Nominal No.) PE line: 0.8-2.5from S$299.90Min. 10 days
- MajorCraft Crossstage Light Game MEBARU FLOAT RIG & MICRO JIG modelIt is a model that demonstrates its power when long casts are required in shallow Gorota Beach and rocky beaches. It is ideal for fishing with a heavy jig head that aims directly at the offshore tide with a long cast, or a rod that is set up and drifted into a tide pool. It is also recommended fo... Read Morenumber of joint shafts 2 Overall Length 8 feet 6 inches Suitable for Lure: 1.0-15g, Line: 2-8lb, PE0.4-1.0 Operation Regular Fastfrom S$229.90Min. 10 days
- GoldenMean Carbon <Soft> Swing Small Rod Yanagishin 120cmAdopts a swing-out type that is excellent in storage and portability. 0 and 0 are jointed, and 0 is jointed to achieve an extremely slim silhouette. The tip uses a roller top that reduces thread trouble. Employs an EVA grip that emphasizes weight reduction and operability. Uses a screw-type botto... Read MoreOverall Length (m) 1.2 Weight (g) 12 number of joint shafts 3 Material 98% carbon fiber/2% glass fiber Dimensions (cm) Close: 46.5from S$34.99Min. 8 days
- GoldenMean Ayu Game Rod Brainstorm Ayu Brainstorm AyuOriginal setting of Fuji stainless steel frame and alumina oxide O-ring guide. Adopted a put-in joint that realizes a beautiful bent curve. Equipped with a carbon solid tip with excellent operability. In addition, by painting the tip part in white and wrapping the guide in fluorescent yellow, it ... Read MoreWeight (g) 122 number of joint shafts 2 Overall Length (m) 2.70(9'0"ft) Material 99.9% carbon fiber/0.1% glass fiber Dimensions (cm) Close: 139 Suitable for Lure: 5-21g, Line: 3-10lb.from S$259.90Min. 8 days
- MajorCraft Crossride 5GA model for full-scale shore jigging in rocky shores and intense tetra bands. It is characterized by bat power that does not give the initiative in a fight with a big game while ensuring operability like MH. A full-fledged all-round model that can handle everything from jigs to diving pencils. H-... Read MoreOverall Length 10'0”ft Operation Action: Regular Fast Specification Joint number: 2pcs Mass (g) Lure: 80±20 Size (Nominal No.) PE line: 1.5-3.5from S$459.90Min. 10 days
- MajorCraft Crossride 5GFull-fledged shore jigging model from embankments and shores. Excellent operability for jigs around 60g. Compatible with blade vibrations, minnows and sinking pencils. It features a flexible tip that can handle even a small diving pencil. MH seriesOperation Action: Regular Fast Specification Joint number: 2pcs Mass (g) Lure: 60±20 Size (Nominal No.) PE line: 1.0-3.0from S$429.90Min. 10 days
- MajorCraft Solpara JiggingIt is the best bait model for jigs around 120g. It is recommended for games that aim at fish that are conscious of the bottom area and fall with one pitch. Bat power that is not inferior to yellowtail and root fish is attractive.Overall Length 6'0”ft Operation Action: Regular Fast Specification Joint: Grip detachment Mass (g) Lure: 80-150 Size (Nominal No.) PE line: 1.5-3from S$189.90Min. 10 days
- MajorCraft Giant Killing 5GA lineup that can cover inshore jigging. Length setting that supports from one pitch jerk to long jerk. A spinning series that is fun even after hanging with stickiness that makes use of T1100G carbon.Operation Action: Regular Fast Specification Joint number: 1pcsfrom S$389.90Min. 10 days
- MajorCraft Solpara Sea BassRecently, it is a model that goes well with metal vibes and spin tail jigs that are indispensable for capturing sea bass. Not only for sea bass, but also for small to medium-sized blue objects such as sagoshi and yellowtail.Overall Length 9' 6”ft Operation Action: Regular Specification Joint number: 2pcs, Line: 8-20lb Mass (g) Lure: 15-42 Size (Nominal No.) PE line: 0.8-2.0from S$189.90Min. 10 days
- MajorCraft Solpara Sea BassIt is a model that is active in areas that require long casts such as rocky beaches and surf. This model is recommended if you are aiming for sea bass or flounder.Overall Length 10' 6”ft Operation Action: Regular Specification Joint number: 2pcs, Line: 8-20lb Mass (g) Lure: 15-42 Size (Nominal No.) PE line: 0.8-2.0from S$239.90Min. 10 days
- MajorCraft Firstcast Sea BassRecommended for fishing with 20-40g lures. Since it has excellent long throw performance, it demonstrates its power in fields that require flight distance. It is also recommended for light shore jigging aiming for small blue objects such as mackerel and sagoshi using jigs. In addition to lure fis... Read MoreOverall Length 10 feet 0 inches number of joint shafts 2 Suitable for Lure: 15-42g, Line: 8-20lb, PE0.8-2.5 Operation Regular Fastfrom S$159.90Min. 10 days