Padlocks
Other Related Pages
- SOL HARD SOL Cylinder Padlock No.2500 (Same Key)It has excellent strength and durability. Uses a double lock that stops the vine at two points inside the main body. (15-25mm / 55mm is single lock) You can open the same number with one key (keys can be centrally managed). It is the same key type as the standard key number. Factory site storage ... Read MoreMaterial (Main Unit) Brass Material (Shackle) Brass Lock Key type Type Same key Specification With 3 keys
- ABUS Padlock TITALIUM-64TI (Same Key)[Hardened iron / NANO PROTECT] is a plating method that uses finer particles than before. (30 mm or more) Covers the shackle (suspended) surface without gaps, and is highly effective in guarding against outside air, moisture, dust and dirt, scratch resistance, wear resistance, and corrosion resis... Read MoreLock Key type Material (Main Unit) Titanium (special aluminum alloy)
- aiai TWE stainless steel hanging padlockRust resistant, double lock and sturdy (using rust resistant SUS304 stainless steel)Lock Key typefrom S$15.99Min. 2 days
- SOL HARD SOL cylinder lockIt has excellent strength and durability. Various doors, mailboxes, lockers, etc. * We do not accept orders with the same key and number.Lock Key type Material Brass Specification With 3 keysfrom S$13.99Min. 3 days
- Shimizu SOL NO. 2500 Common same lock 45Trusco Part No. 849-0153 Material Body / Tail: Brass, Key: Brass Lock Key type Mass (g) 167 Nominal Size 45 Included Accessories With 3 keysfrom S$27.99Min. 3 days
- ALPHA Padlock Kansai No KeyMade of brass that is resistant to rust and has outstanding durability. It can be used for various purposes such as school lockers, mailboxes, storerooms, and warehouses. It is a design that is loved and familiar as a synonym for padlocks. * # 1000-35 is also used as Kanto No.Material (Main Unit) Brass Lock Key type
- ALPHA Padlock Kanto No KeyMade of brass that is resistant to rust and has outstanding durability. It can be used for various purposes such as school lockers, mailboxes, storerooms, and warehouses. It is a design that is loved and familiar as a synonym for padlocks.Material (Shackle) Brass Material (Main Unit) Brass Lock Key type Type Same key
- MonotaRO PadlockNotches are made on both sides of the hanging part to prevent unauthorized unlocking. * We do not sell duplicate keys. We do not accept orders with the same key and number.Included Accessories 2 keys Type Another key Material (Main Unit) Brass Material (Shackle) Hardened iron Key number Individual key Lock Key type
- ALPHA Alpha Padlock* If you purchase more than one, it may not be an individual key. In addition, we cannot accept orders with a specified number. In addition, the attached keys are 3 (* AL-001 # 1000 only 2). Please be aware of this before purchasing.Material Brass Lock Key type Specification Keyed cylinder : Pin cylinder
- SOL HARD Cylinder Padlock (Vine Length, Same Type)It has excellent strength and durability. Uses a double lock that stops the vine at two points inside the main body. (15-25mm is single lock) You can unlock the same number with one key (keys can be centrally managed). Standard standard same key type. Various doors, mail boxes, lockers, bags, bic... Read MoreMaterial (Main Unit) Brass Lock Key type Type Same key Specification With 3 keys
- ALPHA Alpha hanging padlockAbundant variations according to the application * We do not accept orders with the same key and number. * If you purchase multiple items, they may or may not be delivered with the same key number.Material (Main Unit) Brass Material (Shackle) Iron / nickel plating Lock Key type
- MonotaRO Padlock + same key + NO2200A padlock with the same key type. Padlocks of the same size can be managed with just one key. Notches are made on the left and right sides of the vine (double lock * excluding NO2220) to improve security. When managing multiple padlocks with the same key * It is not an individual key. The keys ha... Read MoreIncluded Accessories 3 keys Material (Main Unit) Brass Material (Shackle) Hardened iron Type Same key
- ALPHA Alpha padlock same keyIt is convenient because you can lock and unlock multiple places with one key. Please use it for cases and lockers. * This product is different from the master key.Shackle Thickness (mm) 6 Material Brass Type Same key
- TAKIGEN MFG Padlock (# 0200)It can be locked and unlocked with the same key No. 0200 as the handle. One-touch lock type. Push the hanging metal all the way in to lock it.Mass (g) 125 Included Accessories 2 keys TAKIGEN code 24547 Dimension H (mm) 34 Material Hanging metal: Copper alloy (C3602BD) Material (Main Unit) Zinc alloy (ZDC)
- ALPHA padlockMade of brass that is resistant to rust and has outstanding durability. It can be used for various purposes such as school lockers, mailboxes, storerooms, and warehouses. It is a design that is loved and familiar as a synonym for padlocks. * We cannot accept orders with a specified key number.Number of Keys 3 Material (Main Unit) Brass Lock Key typefrom S$10.99Min. 2 days
- SOL HARD SOL sliding glass for lock doorIt can be adjusted according to the thickness of the glass door of the showcase. A simple type that can be removed. It is the same lock. For showcaseTrusco Part No. 380-1942 Suitable Door Thickness to Mount (mm) 3~7 Cylinder Diameter (Φmm) 6 Mass (g) 80 Key number Same number Material (Main Unit) Steel and zinc die casting Specification With 2 keys
- MonotaRO Sliding glass door lockIt is a key for locking a sliding door type glass door such as a showcase. It can be easily removed. The keys are the same key. For showcase * Do not use for any other purpose. * The same key will be used. We do not accept numbered orders. * Please be careful not to lose the key.Included Accessories 2 keys Suitable Door Thickness to Mount (mm) 3~7 Width (mm) About 109 Cylinder Diameter (Φmm) About 16 Key Same key Material Steel, zinc die casting
- MonotaRO Padlock + same key + NO1200A padlock with the same key type. Padlocks of the same size can be managed with just one key. Notches are made on the left and right sides of the vine (double lock * excluding NO1220) to improve security. When managing multiple padlocks with the same key * It is not an individual key. The keys ha... Read MoreIncluded Accessories 3 keys Material (Main Unit) Brass Material (Shackle) Hardened iron Type Same key
- SOL HARD Cylinder padlock (vine long type)It has excellent strength and durability. Uses a double lock that stops the vine at two points inside the main body. (15-25mm is single lock) Various doors, mailboxes, lockers, etc. * 20 mm and 25 mm are deformed vine shapes. * We cannot accept orders with a specified key number.Type Another key Material (Main Unit) Brass Lock Key type Specification With 3 keys
- ABUS Padlock TITALIUM-64TI (same length)[Hardened iron / NANO PROTECT] is a plating method that uses finer particles than before. (30 mm or more) Covers the shackle (suspended) surface without gaps, and is highly effective in guarding against outside air, moisture, dust and dirt, scratch resistance, wear resistance, and corrosion resis... Read MoreLock Key type Type Same key Material (Main Unit) Titanium (special aluminum alloy)
- aiai Stainless steel hanging padlock (double lock)Lock the suspension with both left and right stops. A mechanism that is strong against impact and cutting and has excellent crime prevention. Uses rust-resistant SUS304 stainless steel. * We cannot accept orders with a specified key number.Type Another key Material (Main Unit) Brass Locking System Double lock Lock Key type Material (Shackle) Stainless steel (SUS304) Number of Keys With three
- Tsuchino Cylinder padlock same keyA general brass padlock. A set of 5 padlocks with the same key number. Even if you purchase it additionally, it has the same key number, so if you use it in multiple places, you can lock and unlock it with one key. For closing doors of posts, lower leg boxes, warehouses, etc.Lock Key type Specification Number of keys: 3 Material Brass
- HILOGIK Cylinder string padlockPadlock / code lock / dial lock seriesType Another key Material (Main Unit) Brass Material (Shackle) Brass Lock Key typefrom S$22.99Min. 2 days
- ALPHA Sliding lockThe design matches any showcase. For glass showcase * It does not correspond to the specification of the key number.Key 2 pieces Applicable glass thickness (mm) 3~6 Key Cylinder 4 disc cylinder Door-to-door clearance dimension (mm) 4 or more (pass each other) Material Body/zinc die-cast fork/steel Color Silver
- TAKIGEN MFG Dial padlockYou can unlock it just by matching the security code. You can change it to any password. The number can be set in 10,000 ways. With cushion rubber, it prevents scratches on the housing. Large fence / inspection portSurface finish Body / Satin chrome plating (MBCr)from S$29.99Min. 2 days
- ALPHA Alpha GINO padlockA classic brass padlock * We do not accept orders with the same key and number. If you purchase more than one, they may or may not be delivered with the same key number.Type Another key Material (Main Unit) Brass Material (vine) Iron Lock Key type Number of Keys With three
- ABUS Padlock TITALIUM-64TI[Hardened iron / NANO PROTECT] is a plating method that uses finer particles than before. (30 mm or more) Covers the shackle (suspended) surface without gaps, and is highly effective in guarding against outside air, moisture, dust and dirt, scratch resistance, wear resistance, and corrosion resis... Read MoreLock Key type Material (Main Unit) Titanium (special aluminum alloy)
- MonotaRO Security lock with alarmA padlock type security lock with an alarm. If you vibrate to unlock the key, you will hear three warning sounds, and if you vibrate further, you will hear a continuous sound at a loud volume comparable to the horn sound of a car for 10 seconds. The suspension (U-shaped metal fittings) itself is ... Read MoreIncluded Accessories 3 keys Shackle Thickness (mm) About 10 Suitable Battery LR44 x 6 (sold separately) Type Padlock with alarm Mass (g) 553 (including battery)
- SOL HARD Stainless lock crane length Same keyThe vine is made of stainless steel (SUS-304) to increase its strength.Lock Key type
- HILOGIK Stainless steel string W lock cylinder padlock Same keyPadlock / code lock / dial lock seriesIncluded Accessories 3 keys Material (Main Unit) Brass Lock Key type Material (Shackle) SUS304 stainless steel Type Same keyfrom S$15.99Min. 2 days
- Guardlock Stainless padlock No.5000Rust-resistant stainless steel shackle! Strong security with double lock. Abundant key differences. Improved rust prevention effect. The exterior of the main body and cylinder plug is chrome-plated, and the internal parts are made of stainless steel springs, nickel-plated pins, etc. to improve th... Read MoreColor Silver Lock Key type Included Accessories With 3 keys
- SOL HARD All stainless lock (same key number not specified)The body, vines and internal springs are made of stainless steel, which makes them even stronger and more durable than brass. You can unlock the same number with one key, and you can centrally manage the keys. Various doors, mail boxes, lockers, bags, storage boxes at construction sites, tool box... Read MoreNumber of Keys 3 pieces Lock Key type Type Same key
- ABUS Padlock TITALIUM-64TI (hanging length)[Hardened iron / NANO PROTECT] is a plating method that uses finer particles than before. (30 mm or more) Covers the shackle (suspended) surface without gaps, and is highly effective in guarding against outside air, moisture, dust and dirt, scratch resistance, wear resistance, and corrosion resis... Read MoreType Another key Lock Key type Material (Main Unit) Titanium (special aluminum alloy)from S$22.99Min. 2 days
- Tsuchino Alpha padlockMade of brass that is resistant to rust and has outstanding durability.Material (Main Unit) Brass Lock Key typefrom S$10.99Min. 2 days
- ABUS Nano Protect Padlock 70/35Stable movement even when used several times a year. Ideal for locking chains, lockers, toolboxes, etc. Crane length type that can be used in various situations. Design that does not spoil the atmosphere of the installation target. Hardened iron shackle that is resistant to cutting (nanoprotect f... Read MoreFinish (Vine) nano protect Dimension D (mm) 15 Dimension C (mm) 19 Dimension E (mm) 25 Included Accessories 3 keys Size 35 Dimension A (mm) 35 Dimension F (mm) 6.5 Dimension B (mm) 65 Material (Main Unit) Brass Material (vine) Hardened iron Lock Key type Key Cylinder Pin cylinder Specification With protective cover (PE)
- TAKIGEN MFG Padlock (# 0200) hanging typeIt can be locked and unlocked with the same key No. 0200 as the handle. One-touch lock type. Push the hanging metal all the way in to lock it.Mass (g) 132 Included Accessories 2 keys TAKIGEN code 24546 Dimension H (mm) 54 Material Hanging metal: Copper alloy (C3602BD) Material (Main Unit) Zinc alloy (ZDC)from S$34.99Min. 2 days
- aiai Stainless steel hanging padlock (single lock)Uses rust-resistant SUS304 stainless steel. * We cannot accept orders with a specified key number.Thickness (mm) 12.5 Dimension e (mm) 13.5 Dimension d (mm) 18.8 Dimension c (mm) 22.0 Dimension a (mm) 25 Dimension b (mm) 40.8 Material (Main Unit) Brass Lock Key type Locking System Single lock Material (Shackle) Stainless steel (SUS304) Number of Keys With three Dimension f (mm) Φ4.0from S$9.69Min. 2 days
- HILOGIK Stainless steel string length W lock cylinder padlockPadlock / code lock / dial lock seriesType Another key Material (Main Unit) Brass Lock Key type Material (Shackle) SUS304 stainless steelfrom S$27.99Min. 2 days
- SOL HARD All stainless steelThe body, vines and internal springs are made of stainless steel, which makes them even stronger and more durable than brass. Various doors, mailboxes, lockers, bags, storage boxes at construction sites, tool boxes, car stop poles, etc. * We do not accept orders with the same key and number.Number of Keys 3 pieces Type Another key Lock Key type Specification With 3 keys
- ABUS Dimple Cylinder Brass PadlockStrong against cutting! Hardened iron vine brass padlock. "Safety design" without a key number stamped on the main body prevents serious unlocking crimes (key number stamped on the key) Uses a precise dimple cylinder. Overwhelming number of key differences. (8000 ways for 30 and 40 mm t... Read MoreIncluded Accessories 3 keys Type Another key Material (Main Unit) Brass Key Cylinder Dimple cylinder Material (Shackle) Hardened iron Lock Key type