Road & Traffic Safety Equipment
Road goods are safety mirrors, direction indicators, reflective tapes, and other items designed to alert and prevent accidents on roads and passages. There are curved mirrors and guide posts for public roads, arrow plates necessary to alert road construction sites, and step plates and mirrors for safety confirmation for entrances to parking lots. There are also mirrors and braille mats for the aisles and windsocks for construction sites and highways.
Other Related Pages
- MonotaRO Step Plate for Wheels Straight RubberEco Mark certified product made by recycling high-quality natural synthetic rubber. Unlike recycled rubber, it has excellent elasticity and is considerably less odorous. It has excellent durability, heat resistance, and cold resistance, and is resistant to deterioration and cracking. There is lit... Read MoreMaterial Natural rubber + EPDM + nylon fiber Color Black Type Straight Bolt Hole Diameter (Φmm) About 10
- MonotaRO Slopes, for Sidewalk Edge, ResinBy installing it on the garage or on the step in front of the entrance, you can reduce the impact when moving and move smoothly. In addition, the uneven shape of the surface prevents the tires of the car from slipping, making it comfortable for the car to enter. Horizontal connection and connecti... Read MoreType Straight
- MonotaRO Reflective Black and Yellow Warning TapeIt reflects the light of the light, which enhances visibility in the evening and at night. Ideal as a danger sign or off-limits sign in factories and work sites. With separator For danger / off-limits markings at work sites and factories * Do not use for any other purpose. * Wipe off any dust on ... Read MoreColor Black/Yellow striped Adhesive Acrylic Tensile Strength (N/25mm) 65
- Hikari Mirror Everywhere with Adhesive0.5 mm thick. Easy to cut with scissors! Adhesive type for easy installation. Made of highly impact-resistant polycarbonate resin, it is hard to break and highly safe and can be used conveniently. For bathrooms, furniture, etc.Specification With adhesive tape Adhesive Acrylic RoHS directive (corresponding to 10 substances) Correspondence
- Hikari Acrylic Mirror PlateLightweight and hard to break. For indoor use onlyMaterial Acrylic Type Square
- Richell Load-up G (Straight Line)Full lineup. You can choose according to the step. By installing it on the pavement in front of the garage or on the step in front of the entrance, you can soften the impact of crossing the step and enter and exit smoothly. Considering the environment, recycled rubber is used. Because it is made ... Read MoreMaterial Recycled rubber Shape Straight line Color Black Load capacity (t) About 2
- MISUGI Safety SlopeA slope made of rubber chips, which is a safe and secure material. It is twice as strong as plastic products (compatible with 6t vehicles). SS-100 weighs 8.5 kg and has excellent stability without being washed away by rainwater. It is non-slip and has excellent durability. It is easy to adapt to ... Read MoreIncluded Accessories Bolts, nuts, washers Material Rubber chips Material / Finish Synthetic rubber chip / resin pigment Load capacity (t) 6
- TRUSCO Lightweight safety mirror that can be cut with a cutterA plastic and aluminum composite mirror that can be cut with a cutter. Lightweight and easy to install and handle. It is resistant to rust and has excellent impact resistance.Set Contents 4 double-sided adhesive sheets Material Aluminum, impact-resistant styrene resin 2018 Trusco page 6 1402
- Shinei Bussan Joy step (step slope)The step slope made of special plastic makes the passage quiet and smooth. You can easily get in vehicles and pass strollers and wheelchairs. We have 3 sizes of 50mm, 100mm and 150mm steps. Made of durable and easy-to-use special plastic, it does not make a sound like an iron plate. Horizontal co... Read MoreMaterial High pressure polyethylene Color Gray Load capacity (t) 8
- ARAO Norire CorpsIt uses recycled rubber tires and can accommodate 10-ton vehicles. Made of rubber, it makes very little noise and prevents noise when entering a vehicle. In addition to the weight of the main body, it is firmly fixed by connecting bolts. A product made from recycled waste tires. We also considere... Read MoreMaterial Recycled rubber Color Black
- Richell Load up G (corner)Full lineup. You can choose according to the step. By installing it on the pavement in front of the garage or on the step in front of the entrance, you can soften the impact of crossing the step and enter and exit smoothly. Considering the environment, recycled rubber is used. Because it is made ... Read MoreMaterial Recycled rubber Shape corner Color Black Load capacity (t) About 2
- MISUGI Safety sideA slope made of rubber chips, which is a safe and secure material. It is twice as strong as plastic products (compatible with 6t vehicles). It is non-slip and has excellent durability. It is easy to adapt to uneven bases and has elasticity. There is no rattling noise at all. * The main body may e... Read MoreIncluded Accessories Bolts, nuts, washers Material / Finish Synthetic rubber chip / resin pigmentfrom S$16.99Min. 2 days
- Amon Industry Garage mirrorEnsuring safety by eliminating blind spots when leaving the warehouse. Lightweight resin mirror that is light and hard to break. For short distances. Can be easily attached to a wide range of attachments and metal fittings. * Attachment is not included with this product. Please purchase the attac... Read MoreViewing distance ~ About 5m
- TRUSCO Normal reflective sheetA retroreflective sheet that reflects incident light in the direction of the light source with minute glass beads built into the sheet (3M Scotchlight [[TM]] reflective sheet specification). Since it uses a PVC film, you can easily cut letters. It shines brightly in response to headlights, etc., ... Read MoreSpecification Encapsulated lens type Material Acrylicfrom S$42.99Min. 2 days
- ARAO Norire Corps 50HMade of rubber to prevent noise when entering the vehicle. In addition to the weight of the main body, it is firmly fixed by connecting bolts. It can also handle 200H by stacking 50H and 150H. * When using for 200H, it is assumed that the vehicle is tall, such as a truck, so in the case of a gene... Read MoreSpecification With connection bolt Material Rubberfrom S$119.90Min. 2 days
- TSUKUSHI KOBO Rubber rope staticUses high-strength rubber with excellent durability. (Same material as other general tire caterpillars) Grooved so it is not slippery. There is no rattling and no sound, so you can rest assured even at night. Firmly fixed by connecting with bolts.Material High strength rubberfrom S$169.90Min. 6 days
- ESCO 600x150x45mm step plateHorizontal connection is possible with the attached bolts.Material Recycled rubber Load capacity (t) Up to 8from S$39.99Min. 2 days
- ESCO 297x210mm fluorescent adhesive sheet (orange)Color Fluorescent orange Mass (g) 23
- Japan Green Cross Step plate Straight type Recycled rubberIt is a connection type step elimination plate that can be firmly fixed with the attached bolts. It is made of recycled rubber that does not slip easily even on rainy days, is quiet, has few cracks and deformations, and is environmentally friendly. For eliminating steps when vehicles pass. For mi... Read MoreIncluded Accessories Bolt x 1 Nut x 1 Washer x 2 Type Articulated Material / Finish Recycled rubber Color Black Installation Easy to put Load capacity (t) 2 Consolidation method Bolt stop (included)from S$67.99Min. 2 days
- MYST Fluorescent reflection sheetFluorescent during the day Reflected at night For danger signs on gate posts, fences, etc. For safety marks on bicycles, tricycles, etc. For school bags, bags, umbrellas, etc.from S$13.99Min. 2 days
- ESCO 297x210mm fluorescent adhesive sheet (lemon yellow)Color Fluorescent lemon yellow Mass (g) 23from S$9.79Min. 3 days
- ESCO 420x600x50mm step plateIt can be used in vehicles up to 10 tons. It is made of rubber and makes very little noise, which prevents noise when the vehicle is used.Included Accessories Connecting bolt Material Recycled rubber Load capacity (t) Up to 10
- WAKI Safety reflective sheetThe reflection function provides clear markings with a small amount of light even at night or in dark places. It is a tough polyester with a beautiful surface and is a glass bead enclosed type.from S$15.99Min. 4 days
- MYST Fluorescent sheetBright fluorescent color that stands out in the daytime For danger signs on gate posts, fences, etc. For safety marks on bicycles, tricycles, etc. For school bags, bags, umbrellas, etc.
- ESCO 330x600x145mm step plateIt can be used in vehicles up to 10 tons. It is made of rubber and makes very little noise, which prevents noise when the vehicle is used.Included Accessories Connecting bolt Material Recycled rubber Load capacity (t) Up to 10from S$229.90Min. 3 days
- Fujimoto Sangyo Absorb level difference (recycled rubber elastic body) right angle cornerRubber chip material that is not slippery even in the rain. Absorbs shocks with moderate elasticity that is safe. It has a certain amount of weight, so you don't have to worry about it being washed away during heavy rain.from S$389.90Min. 24 days
- ESCO 300x300mm Braille panel (Temporary use / Line)Uses foamed PE tape on the back side, leaving no tape marks Ideal for temporary construction for about a month. Strong adhesiveness Easy to remove. With adhesiveSpecification linefrom S$31.99Min. 3 days
- SEKISUI JUSHI Free DeliElastic small reflector Easy to install on struts and curbs For calling attention from a distance at night.Material Urethane resinfrom S$57.99Min. 6 days
- TSUKUSHI KOBO Marker omegaSince it uses a micro-prism reflector, it returns light straight to the plateau and maintains vivid visibility even at night. It has amazing resilience even when laid on tires on the road.Material Polyolefin Mass (g) 20from S$8.99Min. 6 days
- Japan Green Cross Eco stepSpecification With reflective seal Material Waste tire recycled rubber Color Blackfrom S$489.90Min. 6 days
- ESCO 0.4x1850mmx5m tarpaulin fluorescent sheet (orange)Ideal for armbands, safety curtains, and safety tapes.Material PVCfrom S$279.90Min. 9 days
- MonotaRO Soft Delineator Post Traffic PostMade of polyurethane, it has excellent flexibility. As it comes with a reflective sheet, it is also useful for calling attention at night. For vehicle traffic regulation, division, etc. * For asphalt, we recommend using a two-component adhesive (sold separately).Material Polyurethane Color Red x white Diameter (Φmm) (Pole part) approximately 80
- MonotaRO Step plate Car corner RubberEco Mark certified product made by recycling high-quality natural synthetic rubber. Unlike recycled rubber, it has excellent elasticity and is considerably less odorous. It has excellent durability, heat resistance, and cold resistance, and is resistant to deterioration and cracking. There is lit... Read MoreSuitable for It is possible~pass up to 10 tons Material Natural rubber + EPDM + nylon fiber Color Black Type corner Bolt Hole Diameter (Φmm) About 10
- MonotaRO LED warning light round solar typeIt is a warning light for cut cones (a type with a hole so that the upper part can be inserted). It can also be used for color cones (without holes) by using the optional cone adapter. Since it is solar rechargeable, there is no need to worry about running out of batteries. Even if it rains or is... Read MoreMass (g) About 130 Operating Temperature Range (℃) -20~65 Power Supply Ni-MH (Nickel Metal Hydride) LED Color Red Cover Color Clear Number of Blinks (Times / Minute) About 90 Number of LED (pieces) 4
- MonotaRO Curve mirror for temporary installationMade of polycarbonate, it is lightweight and durable. Garage doorways, factory premises, etc. * A protective film is attached to the surface to prevent scratches. Please peel off the film before use. There may be dirt on the surface, but there is no problem with the mirror surface. * This product... Read MoreMaterial (Mirror) Polycarbonate, (Body) ABS
- MonotaRO Solar LED Warning LightIt is a warning light for cut cones (a type with a hole so that the upper part can be inserted). It can also be used for color cones (without holes) by using the optional cone adapter. Since it is solar rechargeable, there is no need to worry about running out of batteries. Even if it rains or is... Read MoreMaterial Polycarbonate, polypropylene Mass (g) About 150 Operating Temperature Range (℃) -20~65 Power Supply Ni-MH (Nickel Metal Hydride) Service Life About 3 years Number of Blinks (Times / Minute) 90
- MonotaRO Adapter Warning light for cut cone For mounting color coneIt is an adapter for attaching a warning light for a cut cone to a color cone (without holes). Used when attaching Monotaro brand / solar LED warning lights, battery-powered LED warning lights, and solar flash warning lights (cut cone mounting type only) to uncut color cones * Do not use for any ... Read MoreMaterial Polypropylene Color Orange Mass (g) About 72
- IRIS OHYAMA Step plateA step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. Since the surface is stepped, you can get in the car smoothly. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with... Read MoreIncluded Accessories Connecting bolt Material Polypropylene Color Gray Load capacity (t) 10
- GREEN CROSS curve-mirrorMade of polycarbonate, it is lightweight and durable. At garage doorways, narrow road doorways, corners, factories and premises * Peel off the protective film before use. * This product is for temporary use. It cannot be installed on public roads.Material Polycarbonate
- MonotaRO WindsockSince the opening is a mesh specification, the air flow is good even in strong winds, and it can be prevented from getting entangled in the columns. A carabiner is attached to the end of the string, so it can be easily hooked on the metal fittings of the support. As a windsock such as a road * Do... Read MoreIncluded Accessories Carabiner Color Green / white Diameter (Φmm) 300