A retroreflective sheet that reflects incident light in the direction of the light source with minute glass beads built into the sheet (3M Scotchlight [[TM]] reflective sheet specification). Since it uses a PVC film, you can easily cut letters. It shines brightly in response to headlights, etc., ... Read More
Thickness (mm) 0.3 Material Acrylic Specification Encapsulated lens type
Fluorescent during the day Reflected at night
For danger signs on gate posts, fences, etc. For safety marks on bicycles, tricycles, etc. For school bags, bags, umbrellas, etc.
The reflection function provides clear markings with a small amount of light even at night or in dark places. It is a tough polyester with a beautiful surface and is a glass bead enclosed type.
Bright fluorescent color that stands out in the daytime
For danger signs on gate posts, fences, etc. For safety marks on bicycles, tricycles, etc. For school bags, bags, umbrellas, etc.
Since it uses a micro-prism reflector, it returns light straight to the plateau and maintains vivid visibility even at night. It has amazing resilience even when laid on tires on the road.
Mass (g) 20 Dimensions, Width W x Depth D x Height H (mm) 90×50×30 Material Polyolefin
Achieves high brightness with a capsule structure. (Approximately 3 times that of a general reflective sheet) Abundant color variations.
It shines brightly in response to headlights, etc., helping to improve safety at night.
Tape Width (mm) 50 Tape Length (m) 50 Material PVC
Since reflectors are attached to both sides, it has excellent visibility. With a handle (dent) that is convenient for mounting.
For calling attention on curbs.
* Do not use for any purpose other than its intended purpose. * It is recommended to use a two-component adhesive (sold separately) for f... Read More
Reflective sheets and tapes on bags, helmets, fences and gateposts clearly inform the driver of their presence and prevent traffic accidents at night. It comes with an adhesive so it can be easily attached.
Prevents traffic accidents at night.
Size (mm) 45×75 Material Prism lens type reflection sheet
A warning message has been added to the sheet that reflects the flashlight and headlights.
By using it in a dark place such as a warehouse, factory, or office, you can call attention to dangerous places in an easy-to-understand manner.
* Cannot be adhered to the following parts. Areas that are we... Read More
Length (mm) 200 Thickness (mm) 1 Material Body / PVC adhesive / Acrylic adhesive Display Items Overhead Caution Width (mm) 45 Mass (g) 4
By adopting a newly developed lens, the reflection performance is 3 to 8 times that of the conventional product. Since it is a special acrylic resin, it has excellent impact resistance and wear resistance. One more high-brightness lens was added on the road side, and a total of three reflectors w... Read More
Reflection performance 3 to 8 times that of conventional products. The headlamp (light source) of the car hits the reflector and reflects back, guiding the driver's line of sight and promptly recognizing the dangerous zone.
Material (Reflective lens) acrylic Dimensions, Vertical x Horizontal x Height (mm) 44×101×23 Material (Main Unit) ABS Type One side
A warning message has been added to the sheet that reflects the flashlight and headlights.
By using it in a dark place such as a warehouse, factory, or office, you can call attention to dangerous places in an easy-to-understand manner.
* Cannot be adhered to the following parts. Areas that are we... Read More
Length (mm) 200 Thickness (mm) 1 Width (mm) 45 Mass (g) 4 Material Body / PVC adhesive / Acrylic adhesive
Fluorescent during the day Reflected at night
For danger signs on gate posts, fences, etc. For safety marks on bicycles, tricycles, etc. For school bags, bags, umbrellas, etc.
A specular reflective sheet with a high-density trihedral cube placed inside the sheet to reflect incident light in the direction of the light source (3M Scotchlight [[TM]] Diamond Grade Consciousness Sheet Specification). Compared to conventional products, it has a particularly high brightness (... Read More
Thickness (mm) 0.465 Material Acrylic Type Prism type
Increased strength such as impact resistance. Epoxy resin material is injected inside to improve the strength. Improved adhesive strength. By flattening the bottom surface and increasing the adhesive area, the adhesive strength has been greatly improved. The headlamp (light source) of the car hit... Read More
Dimensions, Vertical x Horizontal x Height (mm) 101×101×19 Material (Main Unit) ABS Type Both sides
It is a reflective adhesive road stud. Ideal for various alerts such as on curbs. Even at night, the visual effect is great due to the reflectors installed on both sides. It improves visibility at night and is excellent for alerting with curbs and guiding drivers. Since the bottom shape is design... Read More
Thickness (mm) 0.2 Mass (kg) 23 Dimension (mm) 297 x 210 (A4 size) Specification Adhesive Esco Part No. EA983GG-22 Type High brightness and long persistence
It is a new type of line-of-sight guide that allows the driver to see from a straight line to a curve with a single line, enabling smooth guidance of the vehicle. This beam deli succeeded in obtaining a special viewing angle by using a reflector with a special reflecting element. This viewing ang... Read More
Tape Length (m) 1.5 Tape Width (mm) 50 Material (Main Unit) ABS resin Type For class B ・ C Material (Lens) acrylic resin
Since it is a solar type, it is not necessary to replace the battery in places exposed to sunlight (about 2 to 3 years). It can be attached with the included double-sided tape or a special adhesive.
Safety display in the factory. Where there is no outdoor light at night. Simple guidance in danger... Read More
Width (mm) 100 Length (mm) 120 Height (mm) 18 Number of Blinks (Times / Minute) 180±20 Mass (g) 220 Number of LED (pieces) 4 Specification Automatic flashing at night (no switch) Included Accessories Double-sided tape Power Supply Solar type
Fluorescent during the day, reflected at night
For danger signs on gate posts, fences, etc. For safety marks on bicycles, tricycles, etc. For school bags, bags, umbrellas, etc.
It will continue to be issued for 8 to 10 hours just by irradiating it with sunlight or fluorescent light for about 10 to 30 minutes. Marking in the dark It shines in the dark and you can easily see the destination. I can do it
A recurrence-reflective curb stud with high reflectance and excellent attractiveness and weather resistance.
For straight and curved roads, as well as roads with many intersections and store entrances.
* Please use the separately sold special adhesive "Road Bond" for construction.
It is a product with a high retroreflective effect of the light source with a special reflector. At night, the light source is reflected in a dangerous place where there is no light source to call attention. It can be cut with a cutter etc. according to the required length.
Various signs such as ... Read More
Glitter that stands out in the daytime
For danger signs on gate posts, fences, etc. For safety marks on bicycles, tricycles, etc. For school bags, bags, umbrellas, etc.
Thin and easy to apply! Shine even in dark nights for peace of mind and traffic safety at night. A reflective tape that uses a trihedral prism element and has high reflection performance even when light is incident from various angles. High quality and durable, it is also used for road signs and ... Read More
It is a large line-of-sight guide (derinator) actually used on highways and general national highways. A large lens (Φ300) that can be clearly seen even from 500m ahead is used to further enhance the warning effect in dangerous places such as guardrails, median noses, curves, and factories. It is... Read More
Uses a prism reflection method. The ultra-bright, high-angle reflective lens returns the light from the headlights directly to the incident direction without diffuse reflection, and has excellent long-distance visibility, which is very effective when guiding the target in bad weather such as rain... Read More
Dimensions, Vertical x Horizontal x Height (mm) 100×100×17 RoHS directive (corresponding to 10 substances) Correspondence Installation Location For curb Type Same color reflection on both sides
Improved gaze guidance to pedestrians due to the constant light specification (almost lit). We call attention to dangerous places such as premises in the park, bicycle paths, etc. to bicycles and pedestrians. Expansion of applications with abundant color variations. It can be used for various pur... Read More