Threshold Plates
A step plate is used to eliminate steps in the garage or entrance in front of a store or building. In general, it has the advantage that it can move smoothly without tripping over steps when entering a car, stroller, wheelchair, bicycle, pedestrian, etc. There are various types of step plates such as step height, plate width and length, and materials. Materials include resin, rubber, ductile cast iron, and aluminum. The plates can be connected using bolts. Use the corner type for the end.
- MonotaRO Step Plate for Wheels Straight RubberEco Mark certified product made by recycling high-quality natural synthetic rubber. Unlike recycled rubber, it has excellent elasticity and is considerably less odorous. It has excellent durability, heat resistance, and cold resistance, and is resistant to deterioration and cracking. There is lit... Read MoreBolt Hole Diameter (Φmm) About 10 Color Black Material Natural rubber + EPDM + nylon fiber Type Straight
- MonotaRO Slopes, for Sidewalk Edge, ResinBy installing it on the garage or on the step in front of the entrance, you can reduce the impact when moving and move smoothly. In addition, the uneven shape of the surface prevents the tires of the car from slipping, making it comfortable for the car to enter. Horizontal connection and connecti... Read MoreHeight (mm) 100 Length (mm) 270 Type Straight
- Richell Load-up G (Straight Line)Full lineup. You can choose according to the step. By installing it on the pavement in front of the garage or on the step in front of the entrance, you can soften the impact of crossing the step and enter and exit smoothly. Considering the environment, recycled rubber is used. Because it is made ... Read MoreLoad capacity (t) About 2 Color Black Material Recycled rubber Shape Straight line
- MISUGI Safety SlopeA slope made of rubber chips, which is a safe and secure material. It is twice as strong as plastic products (compatible with 6t vehicles). SS-100 weighs 8.5 kg and has excellent stability without being washed away by rainwater. It is non-slip and has excellent durability. It is easy to adapt to ... Read MoreLength (mm) 600 Load capacity (t) 6 Included Accessories Bolts, nuts, washers Material Rubber chips Material / Finish Synthetic rubber chip / resin pigment
- Shinei Bussan Joy step (step slope)The step slope made of special plastic makes the passage quiet and smooth. You can easily get in vehicles and pass strollers and wheelchairs. We have 3 sizes of 50mm, 100mm and 150mm steps. Made of durable and easy-to-use special plastic, it does not make a sound like an iron plate. Horizontal co... Read MoreLoad capacity (t) 8 Color Gray Material High pressure polyethylene
- ARAO Norire CorpsIt uses recycled rubber tires and can accommodate 10-ton vehicles. Made of rubber, it makes very little noise and prevents noise when entering a vehicle. In addition to the weight of the main body, it is firmly fixed by connecting bolts. A product made from recycled waste tires. We also considere... Read MoreWidth (mm) 600 Color Black Material Recycled rubber
- Richell Load up G (corner)Full lineup. You can choose according to the step. By installing it on the pavement in front of the garage or on the step in front of the entrance, you can soften the impact of crossing the step and enter and exit smoothly. Considering the environment, recycled rubber is used. Because it is made ... Read MoreLoad capacity (t) About 2 Color Black Material Recycled rubber Shape corner
- MISUGI Safety sideA slope made of rubber chips, which is a safe and secure material. It is twice as strong as plastic products (compatible with 6t vehicles). It is non-slip and has excellent durability. It is easy to adapt to uneven bases and has elasticity. There is no rattling noise at all. * The main body may e... Read MoreIncluded Accessories Bolts, nuts, washers Material / Finish Synthetic rubber chip / resin pigmentfrom S$16.99Min. 2 days
- ARAO Norire Corps 50HMade of rubber to prevent noise when entering the vehicle. In addition to the weight of the main body, it is firmly fixed by connecting bolts. It can also handle 200H by stacking 50H and 150H. * When using for 200H, it is assumed that the vehicle is tall, such as a truck, so in the case of a gene... Read MoreMass (kg) 12 Dimension (mm) 50×420×600 Material Rubber Specification With connection boltfrom S$119.90Min. 2 days
- TSUKUSHI KOBO Rubber rope staticUses high-strength rubber with excellent durability. (Same material as other general tire caterpillars) Grooved so it is not slippery. There is no rattling and no sound, so you can rest assured even at night. Firmly fixed by connecting with bolts.Material High strength rubberfrom S$169.90Min. 5 days
- ESCO 600x150x45mm step plateHorizontal connection is possible with the attached bolts.Mass (kg) 3.1 Dimension (mm) 600×150×45 Material Recycled rubber Load capacity (t) Up to 8from S$39.99Min. 2 days
- Japan Green Cross Step plate Straight type Recycled rubberIt is a connection type step elimination plate that can be firmly fixed with the attached bolts. It is made of recycled rubber that does not slip easily even on rainy days, is quiet, has few cracks and deformations, and is environmentally friendly. For eliminating steps when vehicles pass. For mi... Read MoreLoad capacity (t) 2 Color Black Consolidation method Bolt stop (included) Included Accessories Bolt x 1 Nut x 1 Washer x 2 Installation Easy to put Material / Finish Recycled rubberfrom S$64.99Min. 2 days
- ESCO 420x600x50mm step plateIt can be used in vehicles up to 10 tons. It is made of rubber and makes very little noise, which prevents noise when the vehicle is used.Mass (kg) 12 Dimension (mm) 50×420×600 Included Accessories Connecting bolt Material Recycled rubber Load capacity (t) Up to 10
- ESCO 330x600x145mm step plateIt can be used in vehicles up to 10 tons. It is made of rubber and makes very little noise, which prevents noise when the vehicle is used.Dimension (mm) 145×330×600 Mass (kg) 17 Included Accessories Connecting bolt Material Recycled rubber Load capacity (t) Up to 10from S$229.90Min. 4 days
- Fujimoto Sangyo Absorb level difference (recycled rubber elastic body) right angle cornerRubber chip material that is not slippery even in the rain. Absorbs shocks with moderate elasticity that is safe. It has a certain amount of weight, so you don't have to worry about it being washed away during heavy rain.Thickness (mm) (Minimum) 8 Length (mm) Outside 690 × 690, inside 510 × 510from S$329.90Min. 23 days
- Japan Green Cross Eco stepJapanese Green Cross No. 121040 Length (mm) 250 Width (mm) 600 Height (mm) 95 Color Black Material Waste tire recycled rubber Specification With reflective sealfrom S$489.90Min. 7 days
- MonotaRO Step plate Car corner RubberEco Mark certified product made by recycling high-quality natural synthetic rubber. Unlike recycled rubber, it has excellent elasticity and is considerably less odorous. It has excellent durability, heat resistance, and cold resistance, and is resistant to deterioration and cracking. There is lit... Read MoreBolt Hole Diameter (Φmm) About 10 Color Black Suitable for It is possible~pass up to 10 tons Material Natural rubber + EPDM + nylon fiber Type corner
- IRIS OHYAMA Step plateA step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. Since the surface is stepped, you can get in the car smoothly. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with... Read MoreLoad capacity (t) 10 Included Accessories Connecting bolt Color Gray Material Polypropylene
- MonotaRO Step plate for cornerA triangular step plate that is convenient for the corners of the step plate. By installing it on the garage or on the step in front of the entrance, you can reduce the impact when moving and move smoothly. In addition, the uneven shape of the surface prevents the tires of the car from slipping, ... Read MoreDimensions, Width W x Depth D x Height H (mm) 270×270×100 Mass (g) About 760 Type corner
- IRIS OHYAMA Mini Step Ramp PlateA step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with the attached bolts. The height can be adjusted in 3 steps. * P... Read MoreLength (mm) 150 Applicable Height (mm) 40・50・60 Trusco Part No. 413-0898 Width (mm) 600 Dimensions, Width W x Depth D x Height H (mm) 600×150×40 Mass (g) 840 Color Gray Material Polypropylene
- IRIS OHYAMA Rubber step plateA rubber step plate that softens the impact and makes it easier to get in. It is made of rubber and has a non-slip surface treatment, and the sound is quiet. It is a design that harmonizes with the exterior.Material Recycled rubber
- MISUGI High Step CornerPlastic type general-purpose product *Please refrain from using it on caterpillars, bulldozers, and dump trucks. * Cannot be used for vehicles over 4t such as bulldozers.Included Accessories Bolts, nuts, washers Material / Finish Synthetic resin / resin pigment
- IRIS OHYAMA Step plate (corner)A step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. Since the surface is stepped, you can get in the car smoothly. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with... Read MoreIncluded Accessories Connecting bolt Color Gray Material Polypropylene
- Fujimoto Sangyo Absorb level difference (recycled rubber elastic body)Rubber chip material that is not slippery even in the rain. Absorbs shocks with moderate elasticity that is safe. It has a certain amount of weight, so you don't have to worry about it being washed away during heavy rain.
- Sunself Recycled step plate Eco stepExcellent durability with recycled waste tires! Uses high-brightness reflective tape with excellent visibility. Compared to plastic products, it has a structure that is hard to break, has less noise, and is hard to slip. Since the anti-slip function is attached to the surface of the main body, it... Read MoreColor (Body) Black / (Reflective) Yellow Length (mm) 250 Width (mm) 600 Dimensions, Width W x Depth D x Height H (mm) 600×250×95 Height (mm) 95 Mass (kg) About 9 Included Accessories Connecting bolt Type For 100mm step Material Recycled rubber
- MonotaRO Step slopeIt can be used for various thicknesses of iron plates (9.22.25 mm). You can quickly eliminate small steps and consider pedestrians and bicycles. When used in combination with corners, steps at the corners can be eliminated. * When using together, cut the step slope and adjust the length.Length (mm) 1500 Width (mm) 155 Material Vinyl chloride (PVC) Color Yellowfrom S$119.90Min. 2 days
- MISUGI High step corner (side corner)Plastic type general-purpose product *Please refrain from using it on caterpillars, bulldozers, and dump trucks. * Cannot be used for vehicles over 4t such as bulldozers.Included Accessories Bolts, nuts, washers Material / Finish Synthetic resin / resin pigment
- MISUGI Silent Cass CornerIt is made of rubber and absorbs shocks, so it has excellent strength. (Compatible with 4t vehicles) Made of rubber, it is heavy and compact, so it has excellent stability. It is made of rubber and has a non-slip surface treatment, so it is not slippery and has excellent durability. It is easy to... Read MoreLength (mm) 335 Color Black Included Accessories Bolts, nuts, washers Material Natural rubber + synthetic rubberfrom S$48.99Min. 2 days
- MISUGI Cass corner M classApplicable vehicle: M class (up to 8t vehicle) Made of ductile cast iron with abundant stickiness and elasticity. Ductile cast iron = the same material as manhole. It will last for a long time semi-permanently without cracking or deforming. Due to the baking finish, it does not rust easily and do... Read MoreIncluded Accessories Bolts, nuts, washers Material Ductile iron (casting) Width (mm) 300 Color Metallic gray Length (mm) 335
- ARAO Step slopeIt can be used for various thicknesses of iron plates (9.22.25 mm). You can quickly eliminate small steps and consider pedestrians and bicycles. When used in combination with corners, steps at the corners can be eliminated. * When using together, cut the step slope and adjust the length.Length (mm) 1500 Width (mm) 155 Material Vinyl chloride (PVC) Color Yellow
- ARAO Step slope (for corners)It can be used for various thicknesses of iron plates (9.22.25 mm). You can quickly eliminate small steps and consider pedestrians and bicycles. * When using together, cut the step slope and adjust the length.Width (mm) 155 Color Yellowfrom S$269.90Min. 2 days
- Sunself Recycled step plate Eco step (corner)Excellent durability with recycled waste tires! Uses high-brightness reflective tape with excellent visibility. Compared to plastic products, it has a structure that is hard to break, has less noise, and is hard to slip. Since the anti-slip function is attached to the surface of the main body, it... Read MoreColor (Body) Black / (Reflective) Yellow Dimensions, Width W x Depth D x Height H (mm) 250×250×95 Mass (kg) About 3 Included Accessories Connecting bolt Material Recycled rubber
- Car-boy Pain Kunaizo for corner slopeProtects the feet of children and the elderly from tripping accidents on steps To eliminate the steps between the room and the corridor! By attaching this product to both ends of "It doesn't hurt!", The ends become sloped, and you can enter and exit the room more smoothly than ever ... Read MoreMaterial EVA resin / acrylic adhesive Color grain
- MISUGI Cass corner M class side cornerApplicable vehicle: M class (up to 8t vehicle) Made of ductile cast iron with abundant stickiness and elasticity. Ductile cast iron = the same material as manhole. It will last for a long time semi-permanently without cracking or deforming. Due to the baking finish, it does not rust easily and do... Read MoreLength (mm) 335 Included Accessories Bolts, nuts, washers Material Ductile iron (casting) Color Metallic grayfrom S$129.90Min. 2 days
- Hikari Step matIt is effective in eliminating steps between Japanese-style rooms and corridors, steps such as sill, and preventing trips. Preventing trips due to steps such as sill Protects against steps in offices, hospitals, warehouses, homes, and all thresholds.Material Rubber non-migrationfrom S$11.99Min. 6 days
- Shinyei Home Create (Former Shinkyowa) Assist slope (step auxiliary plate)Because it is a polyethylene resin foam, it is light and durable. Both ends of the slope are also sloped, so you can use it with confidence. The height can be easily adjusted by cutting with a utility knife or the like. If you fix it with the attached double-sided tape, you will be covered by lon... Read MoreLength (mm) 235 Height (mm) 24 Width (mm) 775 Material Polyethylene foamfrom S$76.99Min. 5 days
- MISUGI Cass corner class HApplicable vehicle: H class (up to 30t vehicle) Made of ductile cast iron with abundant stickiness and elasticity. Ductile cast iron = the same material as manhole. It will last for a long time semi-permanently without cracking or deforming. Due to the baking finish, it does not rust easily and d... Read MoreIncluded Accessories Bolts, nuts, washers Color Metallic gray Material Ductile iron (casting) Width (mm) 300from S$149.90Min. 7 days
- Japan Green Cross Step plate Corner type Recycled rubberIt is a connection type step elimination plate that can be firmly fixed with the attached bolts. It is made of recycled rubber that does not slip easily even on rainy days, is quiet, has few cracks and deformations, and is environmentally friendly. For eliminating steps when vehicles pass. For mi... Read MoreLoad capacity (t) 2 Color Black Consolidation method Bolt stop (included) Included Accessories Bolt x 1 Nut x 1 Washer x 2 Installation Easy to put Material / Finish Recycled rubberfrom S$33.99Min. 4 days
- ESCO 600x150x40mm step plateThe surface is processed to prevent slipping and prevent falls. It can be connected horizontally with the attached bolts. * Please avoid passing over 1.5t. (Even if it is less than 1.5t, it cannot withstand the load of automobiles, etc.)Load capacity (t) 1.5 (Cannot withstand the load of a car) Dimension (mm) 600×150×40 Mass (g) 840 Material Polypropylenefrom S$58.99Min. 4 days
Filter by categories