Plastic Threshold Plates
- MonotaRO Slopes, for Sidewalk Edge, ResinBy installing it on the garage or on the step in front of the entrance, you can reduce the impact when moving and move smoothly. In addition, the uneven shape of the surface prevents the tires of the car from slipping, making it comfortable for the car to enter. Horizontal connection and connecti... Read MoreType Straight
- Shinei Bussan Joy step (step slope)The step slope made of special plastic makes the passage quiet and smooth. You can easily get in vehicles and pass strollers and wheelchairs. We have 3 sizes of 50mm, 100mm and 150mm steps. Made of durable and easy-to-use special plastic, it does not make a sound like an iron plate. Horizontal co... Read MoreMaterial High pressure polyethylene Color Gray Load capacity (t) 8
- IRIS OHYAMA Step plateA step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. Since the surface is stepped, you can get in the car smoothly. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with... Read MoreIncluded Accessories Connecting bolt Material Polypropylene Color Gray Load capacity (t) 10
- MonotaRO Step plate for cornerA triangular step plate that is convenient for the corners of the step plate. By installing it on the garage or on the step in front of the entrance, you can reduce the impact when moving and move smoothly. In addition, the uneven shape of the surface prevents the tires of the car from slipping, ... Read MoreMass (g) About 760 Type corner
- IRIS OHYAMA Mini Step Ramp PlateA step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with the attached bolts. The height can be adjusted in 3 steps. * P... Read MoreMaterial Polypropylene Color Gray Mass (g) 840
- MISUGI High Step CornerPlastic type general-purpose product *Please refrain from using it on caterpillars, bulldozers, and dump trucks. * Cannot be used for vehicles over 4t such as bulldozers.Included Accessories Bolts, nuts, washers Material / Finish Synthetic resin / resin pigment
- IRIS OHYAMA Step plate (corner)A step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. Since the surface is stepped, you can get in the car smoothly. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with... Read MoreIncluded Accessories Connecting bolt Material Polypropylene Color Gray
- Fujimoto Sangyo Absorb level difference (recycled rubber elastic body)Rubber chip material that is not slippery even in the rain. Absorbs shocks with moderate elasticity that is safe. It has a certain amount of weight, so you don't have to worry about it being washed away during heavy rain.
- MISUGI High step corner (side corner)Plastic type general-purpose product *Please refrain from using it on caterpillars, bulldozers, and dump trucks. * Cannot be used for vehicles over 4t such as bulldozers.Included Accessories Bolts, nuts, washers Material / Finish Synthetic resin / resin pigment
- Car-boy Pain Kunaizo for corner slopeProtects the feet of children and the elderly from tripping accidents on steps To eliminate the steps between the room and the corridor! By attaching this product to both ends of "It doesn't hurt!", The ends become sloped, and you can enter and exit the room more smoothly than ever ... Read MoreMaterial EVA resin / acrylic adhesive Color grain
- Shinyei Home Create (Former Shinkyowa) Assist slope (step auxiliary plate)Because it is a polyethylene resin foam, it is light and durable. Both ends of the slope are also sloped, so you can use it with confidence. The height can be easily adjusted by cutting with a utility knife or the like. If you fix it with the attached double-sided tape, you will be covered by lon... Read MoreMaterial Polyethylene foamfrom S$76.99Min. 6 days
- ESCO 600x150x40mm step plateThe surface is processed to prevent slipping and prevent falls. It can be connected horizontally with the attached bolts. * Please avoid passing over 1.5t. (Even if it is less than 1.5t, it cannot withstand the load of automobiles, etc.)Material Polypropylene Mass (g) 840 Load capacity (t) 1.5 (Cannot withstand the load of a car)from S$58.99Min. 3 days
- ESCO 900x250x95mm step plateHorizontal connection is possible with the attached bolts.Material Recycled rubber Load capacity (t) Up to 12from S$88.99Min. 3 days
- ESCO 900x270x100mm step plateThe surface is processed to prevent slipping and prevent falls. Horizontal connection is possible with the attached bolts. * Please avoid passing vehicles over 10t.Material Polypropylene Mass (g) 2950 Load capacity (t) Less than 10from S$59.99Min. 3 days
- UNIT (UNIT SAFETY SIGNS) Step plate 900Included Accessories Joint bottle x 2 Material Polypropylene Type For slopefrom S$99.90Min. 5 days
- Safe-Run Safety Supplies Curb Ramp Round End CapTo prevent bicycles and pedestrians from falling or tripping! Installed in front of the garage, in front of the entrance, etc. to mitigate the impact of the step. Easy to install just by placing it, and when using horizontal connection, fix it with the attached screws. For steps such as in front ... Read MoreIncluded Accessories Horizontal connection bolt Material PP Color Grayfrom S$32.99Min. 8 days
- ESCO 600x270x100mm step plateThe surface is processed to prevent slipping and prevent falls. Horizontal connection is possible with the attached bolts. * Please avoid passing vehicles over 10t.Material Polypropylene Mass (g) 2100 Load capacity (t) Less than 10from S$47.99Min. 3 days
- IRIS OHYAMA Step plateThe slope shape eliminates steps and prevents pedestrians from tripping and bicycles and motorcycles from tipping over. You can get in the car smoothly without the car body jumping up. It is a non-slip surface step processing. Bottom shape that makes it easy for water to escape so that it will no... Read MoreMaterial Polypropylene Color BlackDiscontinued
- IRIS OHYAMA Step plateA step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. Since the surface is stepped, you can get in the car smoothly. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with... Read MoreIncluded Accessories Connecting bolt Material Polypropylene (PP) Color Black Allowable Load 10t or lessDiscontinued
- TRUSCO Step plate cornerIt softens the impact of steps and does not make a sound like an iron plate. Design registration acquired stand 070697/1070968 Can be fixed to the ground with all anchor C-645BT. It can be connected using the attached bolts and nuts.Cold resistance -15℃ Weatherability GoodDiscontinued
- MonotaRO 10cm step plate (straight)By installing it on the garage or on the step in front of the entrance, you can reduce the impact when moving and move smoothly. In addition, because the surface shape is processed, it is easy for cars to enter and it is difficult for slips to occur. Horizontal connection and connection with corn... Read MoreSuitable for Ordinary passenger car Material PP Color Black Type Straight Load capacity (t) 1.5 (with uniform load)Discontinued
- Japan Green Cross Safety upEasy installation makes it easy to get in the vehicle. It does not make a sound like an iron plate. Withstand load is OK up to 8t. Strong against ultraviolet rays. High cold resistance that does not deteriorate even at -20 degrees.Included Accessories Bolts, nuts, washers Material (Main Unit) Polyethylene resin Allowable Load 8tDiscontinued
- IRIS OHYAMA Step plateThe surface is processed to prevent slipping and prevent falls. It is less likely to crack than concrete.Material Polypropylene Color GrayDiscontinued
- MonotaRO 10cm step plate (corner)By installing it on the garage or on the step in front of the entrance, you can reduce the impact when moving and move smoothly. In addition, because the surface shape is processed, it is easy for cars to enter and it is difficult for slips to occur. Horizontal connection and straight connection ... Read MoreMaterial PP Color Black Type corner Load capacity (t) 1.5 (with uniform load)Discontinued
- TRUSCO Step plate bodyIt softens the impact of steps and does not make a sound like an iron plate. Design registration acquired stand 070697/1070968 Can be fixed to the ground with all anchor C-645BT. It can be connected using the attached bolts and nuts.Cold resistance -15℃ Weatherability GoodDiscontinued
- Shoko Bussan Resin Step Ramp PlateA light and durable resin slope. With connecting bolts. Where you are worried about steps. * Do not use with a gap between the curb and the stone. * Please note that it is slippery on snowy and rainy days. * The load capacity is assumed to be about that of a passenger car. * Durability varies gre... Read MoreMaterial Recycled resin Allowable Load About an ordinary passenger carDiscontinued