Dangerous Goods Signs
Dangerous goods / hazardous substance relations are safety signs based on general high-pressure gas safety regulations, organic solvent poisoning prevention regulations, dangerous goods regulations, occupational safety and health regulations, fire prevention regulations. Posting is required in an easy-to-read place to ensure the safety of workers and first aid. In addition to magnets and stickers such as strict fire, high-pressure gas, and pharmaceutical poisonous deleterious substances, PVC and iron plate plates, boards containing specific chemical substances, cylinder storage location signs, worker knowledge signs, etc. There are also many types.
Other Related Pages
- Japan Green Cross JIS laser markingThis standard specifies the safety of laser products. However, this standard does not apply to medical laser products. 1. 1. Protect the human body from laser radiation in the wavelength range of 180 nm to 1 mm by introducing a system that shows the safe operating level of laser radiation and cla... Read MoreSpecification With D release paper Material Olefin sticker Type of Sign With D release paper
- MonotaRO Hazardous material signThis is an essential sign for avoiding danger. It is made of iron so it is durable. * When posting, avoid places exposed to direct sunlight or water. * When storing, avoid places in the sun or places with high temperature and humidity.Specification There are holes in the four corners Material Iron plate (Meijiyama) Sign Meaning No fires Type of Sign 4 corner holes
- MonotaRO Magnet Label LP high pressure gasMandatory sign based on "General High Pressure Gas Safety Act" and "Rules for Regulation of Dangerous Goods". Easy to install and remove from the vehicle with a magnet type. * When attaching to the car body, remove dust and dirt from the surface before attaching. There is a ri... Read MoreMaterial Rubber magnet Type of Sign Magnet type
- MonotaRO Hazardous material sign Fire ban Hard PVCThis is an essential sign for avoiding danger. A light and durable sign made of hard PVC. * When posting, please post in a place where there is no fire. * When storing, avoid places with fire, sunlight, and high temperature and humidity.Specification There are holes in the four corners Material Hard PVC Sign Meaning No fires Type of Sign 4 corner holes
- MonotaRO Sticker Signs LP high pressure gas relatedMandatory sign based on "General High Pressure Gas Safety Act" and "Rules for Regulation of Dangerous Goods". A sticker type that peels off the release paper on the back side and attaches it. * Please remove dirt on the surface of the object before pasting. * When storing, avo... Read MoreMaterial Fluorescent sticker Type of Sign Sticker
- MonotaRO Label Organic solvent typeIt is an indispensable sign for labeling according to the Organic Solvent Poisoning Prevention Regulations. Type 2 organic solvent, etc. * When posting, please post in a place where there is no fire. * When storing, avoid places with fire, sunlight, and high temperature and humidity.Material PVC Sign Meaning Second-class organic solvent, etc. Type of Sign Hole 4
- MonotaRO Label Use of organic solvent PrecautionsIt is a precautionary sign when handling organic solvents. It is divided into 3 parts. Since each has holes at the four corners, you can use it by fixing it to a wall surface with commercially available screws. * When posting, please post in a place where there is no fire. * When storing, avoid p... Read MoreMaterial PVC Type of Sign 4 corner holes
- MonotaRO Hazardous material sign Category name responsible person Iron plateThis is an essential sign when handling dangerous goods. It is made of iron so it is durable. * When posting, avoid places exposed to direct sunlight or water. * When storing, avoid places in the sun or places with high temperature and humidity.Specification There are holes in the four corners Material Iron plate (Meijiyama) Type Rip-cut Type of Sign 4 corner holes
- MonotaRO Hazardous material label Category product name responsible Hard PVCThis is an essential sign when handling dangerous goods. Made of hard PVC, it is light and durable. * When posting, please post in a place where there is no fire. * When storing, avoid places with fire, sunlight, and high temperature and humidity.Specification There are holes in the four corners Material Hard PVC Type of Sign 4 corner holes
- UNIT (UNIT SAFETY SIGNS) Dangerous goods sign vertical (eco-board)Vertical signMaterial Recycled polypropylene Mass (g) 200 Type of Sign Hole 4 Sumi
- MonotaRO Dangerous goods labelingThis is an essential sign when handling dangerous goods. Made of hard PVC, it is light and durable. * When posting, please post in a place where there is no fire. * When storing, avoid places with fire, sunlight, and high temperature and humidity.Specification There are holes in the four corners Material Hard PVC Sign Meaning Small-quantity dangerous goods storage Type of Sign 4 corner holes
- MonotaRO Label Specified chemical substanceIt is a chemical substance hazard prevention rule sign based on the provisions of the Industrial Safety and Health Act and the Industrial Safety and Health Act Enforcement Ordinance by the Ministry of Health, Labor and Welfare. Since there are holes in the four corners, you can post it by screwin... Read MoreMaterial Clean eco board Type of Sign Hole 4from S$27.99Min. 2 days
- UNIT (UNIT SAFETY SIGNS) Specified chemical substance label (Eco Uniboard)Specification Φ2.5mm hole 4 sumi Material Eco Uniboard
- UNIT (UNIT SAFETY SIGNS) Rotating double-sided display boardIt is a display based on the dangerous goods regulations. It is very convenient because it can be operated with one touch with the empty charge display attached. Since it is a double-sided display, you can check it from either side. For cylinders * Ball chain is sold separately. Screw tape is sol... Read MoreMaterial ABS resin
- MonotaRO Hazardous material labelingThis is an essential sign when handling dangerous goods. It is made of iron and is durable. * When posting, avoid places exposed to direct sunlight or water. * When storing, avoid places in the sun or places with high temperature and humidity.Specification There are holes in the four corners Material Iron plate (Meijiyama) Sign Meaning Small-quantity dangerous goods storage Type Rip-cut Type of Sign 4 corner holes
- UNIT (UNIT SAFETY SIGNS) Dangerous goods sign Eco uniboardIt is a display based on the dangerous goods regulations. For trucks and tank trucks. * The listed products may not always match depending on the regulations of the local government. Screw tape is sold separately.Material Eco Uniboard (2.5mmΦ hole 4 Sumi) Mass (g) 200 Type of Sign Hole 4
- TRUSCO High pressure gas related magnetic signsType of Terminal Fitting magnet
- Japan Green Cross Dangerous goods signs (category / product name / responsible person, etc.)* The listed products may not always match depending on the regulations of the local government.Material Lami plate Shape Sign Size 300×600×1mm Classification Firefighting and dangerous goodsfrom S$25.99Min. 2 days
- Japan Green Cross GHS labelSpecification With D release paper Material Deposition PET sticker Type of Sign With D release paper
- UNIT (UNIT SAFETY SIGNS) Hazardous material sign Iron plateIt is a sign to be displayed at the storage location of dangerous goods based on the dangerous goods regulations and fire prevention regulations. * The listed products may not always match depending on the regulations of the local government.Mass (g) 700 Type of Sign Hole 4
- UNIT (UNIT SAFETY SIGNS) LP high pressure gas related sticker corner "danger"[High Pressure Gas] "Marking General High Pressure Gas Safety Regulations Article 70" [Danger] The "Rules for Regulation of Dangerous Signs, Article 17" stipulates that the vehicle must be placed in an easily visible position in front of and behind the vehicle.Specification With D release paper Type Vehicle sticker Material Sticker Shape Square Sign Meaning Danger Classification LP high pressure gas Mass (g) 42 Type of Sign Sticker Letter Color Reflective yellow
- UNIT (UNIT SAFETY SIGNS) LP high pressure gas related sign Magne angle "danger""Rules for Regulation of Hazardous Materials" Articles 17 and 47. It must be placed in a position that is easy to see in front of and behind the vehicle.Type Vehicle warning sign Material Rubber magnet Sign Meaning Danger Classification LP high pressure gas Mass (g) 230 Type of Sign Magnet type Letter Color Reflective yellow
- UNIT (UNIT SAFETY SIGNS) Toxic substance stickerA sticker type that can be easily attached. As a display accompanying Article 12 of the Poisonous and Deleterious Substances Control Law. A sticker for wall sticking.Material PVC sticker
- UNIT (UNIT SAFETY SIGNS) Asbestos sign (news about demolition work such as buildings)* We do not deliver to private homes (detached houses / apartments).from S$11.99Min. 2 days
- Japan Green Cross Dangerous goods sign (horizontal)Material Steel (baked melamine) Mass (g) 570 Type of Sign Hole 4
- Japan Green Cross Dangerous goods sign (vertical)Specification Φ4.0mm hole x 4, Mt.Meiji, borderless Material Steel (baked melamine) Mass (g) 570 Type of Sign Hole 4
- Japan Green Cross Dangerous goods sign (classification / product name / responsible person, etc.)* The listed products may not always match depending on the regulations of the local government.Material Lami plate Shape Sign Size 600×300×1mm Classification Firefighting and dangerous goods Mass (g) 260
- Japan Green Cross LP high-pressure gas related sticker horizontal "high-pressure gas"[High pressure gas] "Label general high pressure gas safety regulations related example standards 1-4-1, 2"Specification With D release paper Type Hazardous Material Material Fluorescent Envi Sticker Sign Meaning High pressure gas Classification LP high pressure gas Type of Sign Sticker Letter Color Fluorescent color
- UNIT (UNIT SAFETY SIGNS) Organic solvent type labelArticle 25 of the Organic Solvent Poisoning Prevention Regulations When a business operator engages a worker in an organic solvent work in an indoor workplace, the worker can easily know the classification of the organic solvent, etc. related to the organic solvent work. The solvent must be displ... Read MoreMaterial Eco Uniboard Shape Sign Size 600 × 300mm (2.5mmΦ hole 4 sumi) Classification Organic solvents Mass (g) 200 Type of Sign 4 holes
- GREEN CROSS Dangerous goods sign length sticker specificationIt is a sign based on the regulations on dangerous goods regulation and the fire prevention regulations.Specification Laminating Material PVC seal Mass (g) 80 Type of Sign Stickerfrom S$19.99Min. 2 days
- Japan Green Cross Pharmaceutical poisonous deleterious substancesSince the characters are sealed by laminating, the characters will not disappear due to friction.Specification Laminating Material Hard vinyl chloride Mass (g) 260 Screw Hole No hole (processing free)
- Japan Green Cross Dangerous goods sign (dangerous goods storage / manufacturing factory) Lami verticalType place Material Lami plate Shape Sign Size 600×300×1mm
- UNIT (UNIT SAFETY SIGNS) Asbestos sign (asbestos usage survey results)Material Eco Uniboard (hole 4) Mass (g) 200 Type of Sign Hole 4from S$11.99Min. 2 days
- MonotaRO Sticker Toxic substancesSince it is a PVC sticker, it can be easily attached to the steel or glass surface of the library. For storage * When posting, please post in a place where there is no fire. * Remove dirt and dust from the surface to be pasted before pasting. * When storing, avoid places with fire, sunlight, and ... Read MoreMaterial PVC sticker Sign Meaning Non-medical deleterious substancefrom S$8.39Min. 2 days
- Shinwa Automotive Industry Danger mark 300 cornerMaterial Aluminum Suitable for 65KMH300F・65KMH300R
- UNIT (UNIT SAFETY SIGNS) Asbestos disorder prevention rule measures articleIt is a sign that must be posted in accordance with the Asbestos Disorder Prevention Regulations.Material Eco Uniboard Mounting Hole 4 holes Type of Terminal Fitting Screw stopfrom S$14.99Min. 2 days
Filter by categories