Supervisor Name Signs
- MonotaRO Work of the chief workerIt is a job sign required by the Occupational Safety and Health Regulations. * When posting, please post in a place where there is no fire. * When storing, avoid places with fire, sunlight, and high temperature and humidity.Type of Sign 4 corner holes Dimensions, Height x Width (mm) 500×400 Material Polypropylene
- Japan Green Cross Job chief's job indicatorThickness (mm) 1 Mass (g) 380 Dimension (mm) 600×450 Included Accessories Double-sided sheet tape x 6 sheets Material Hard envy Type of Sign Hole 4 Specification Φ3mm hole x 4
- MonotaRO Sticker responsible person signIt is a sticker type sticker. Suitable for displaying the person in charge. * Do not use for anything other than its intended purpose.Dimension (mm) 200×80 Material Envi sticker Type of Sign Sticker
- UNIT (UNIT SAFETY SIGNS) Work chief job boardUses 50% recycled polypropylene. It is a display based on Article 18 of the Occupational Safety and Health Regulations. In the workplace where the work chief is selected. * Screws are sold separately.Thickness (mm) 1.2 Mass (g) 320 Mounting Hole 4 places Dimension (mm) 600×450
- UNIT (UNIT SAFETY SIGNS) Nomination signIn order to clearly display the name of the person in charge, various materials are used!Thickness (mm) 1.2
- TSUKUSHI KOBO Job chief's job indicatorThickness (mm) 1 Number of Holes 4 Material SC board
- UNIT (UNIT SAFETY SIGNS) Work chief duty display boardCovers the types of work specified by the Safety Law. * We do not deliver to private homes (detached houses / apartments).
- MonotaRO Magnet responsible person signIt is a responsible person sign with a magnet. It can be easily attached to and removed from steel machines, doors and partitions. You can fill in with an oil-based pen. To display the person in charge * Do not use for any other purpose. * Keep objects that are affected by magnetic force away fro... Read MoreType of Sign magnet Material Magnet sheet Dimensions, Height x Width (mm) 200×80
- Japan Green Cross Name sign (resin type) (vertical)Thickness (mm) 1 Dimension (mm) 300×100 Mass (g) 42 Material Hard envy Specification Name writing type
- TOGUE ANZEN KOUGYOU Manager display stickerWe will clearly display the type of work and the person in charge.Dimensions, Width x Length (mm) 80×200 Type of Sign Sticker / Stickerfrom S$26.99Min. 2 days
- Japan Green Cross Work chief job signOccupational Safety and Health Regulations Volume 1, Chapter 2, Section 5, Article 18 When a business operator appoints a work chief, he / she posts the name of the work chief and the matters to be performed by that person in an easily visible place in the workplace. It must be made known to the ... Read MoreThickness (mm) 1 Trusco Part No. 113-8423 Mass (g) 378 Japanese Green Cross No. 49519 Dimension (mm) 600×450 Included Accessories Double-sided sheet tape x 6 sheets Material Hard envy Sign Meaning Specific chemical substances Specification Φ3mm hole x 4
- UNIT (UNIT SAFETY SIGNS) Nomination signIt's perfect for posting in a small space! A wide variety of strip-shaped signs. * Company name cannot be entered.
- Japan Green Cross Qualified person job indicatorThickness (mm) 1 Mass (g) 380 Dimension (mm) 600×450 Included Accessories Double-sided sheet tape x 6 sheets Material Hard envy Type of Sign Hole 4 Specification Φ3mm hole x 4
- UNIT (UNIT SAFETY SIGNS) Plug-in nomination signA type in which the person in charge can be entered in the blank.
- UNIT (UNIT SAFETY SIGNS) Sticker nomination signSince it is a sticker, it is low cost. Please replace and use when changing the person in charge.Specification Backside adhesive
- Japan Green Cross Personnel name sign board Vertical type Name tag insertion typeMaterial Hard envyfrom S$9.69Min. 2 days
- AIM Person in charge display plate Food hygiene officerMaterial: Acrylic. pierced. With double-sided tape on the back.Dimensions, Height x Width x Thickness (mm) 200×85×2 TKG Part No. (2017) 6-2385-1401 TKG Part No. 8-2549-1301 Material Acrylic Type of Sign Affix tapefrom S$8.99Min. 2 days
- Japan Green Cross Personnel name sign board Vertical type Name tag insertion typeMaterial Hard envy Type Name sign Classification Person in charge
- Japan Green Cross Responsible person name sign board (PVC)Material Hard envy Classification Person in charge
- Anzen Kougyou The duties of the chief workerIt is a low foam polypropylene board. It's 1mm thick so it's not bulky. Ideal for disseminating the duties of the work chief and the name of the chief. Occupational Safety and Health Regulations Volume 1, Chapter 2, Section 5, Article 18 When a business operator appoints a work chief, he ... Read MoreDimension (mm) 500×400 Material PP (polypropylene) Shape Sign Classification The duties of the chief worker Type information
- Japan Green Cross Name sign (vertical)With back tapeThickness (mm) 1 Dimension (mm) 140×40 Mass (g) 8 Material Hard envy Specification Name writing type Type of Sign With back tapefrom S$4.79Min. 2 days
- GREEN CROSS General safety signIt is a strip-shaped safety sign. Easy to install. To instruct the information Double-sided tape and screws are not includedMounting Double-sided tape, screws, etc. Material Eco boardfrom S$5.99Min. 2 days
- GREEN CROSS General safety sign (PVC seal)It is a strip-shaped safety sign. Easy to install. It is laminated and resistant to rubbing. To instruct the informationMounting PVC seal Material Stickerfrom S$5.79Min. 2 days
- GREEN CROSS Job chief's job indicatorIt is a sign about the duties of the work chief. Safety signSpecification Eco board with four corner holes Type of Sign Hole 4 Sumi Size 400×500
- UNIT (UNIT SAFETY SIGNS) Qualified Person Relation SignIt is a sign that you can enter the name of a qualified person. * We do not deliver to private homes (detached houses / apartments).from S$2.89Min. 2 days
- Japan Green Cross Personnel name sign (Steel)Classification Person in charge
- TSUKUSHI KOBO Small stickerDimension (mm) 75×35 Material Sticker Type of Sign Sticker
- GREEN CROSS General safety sign (magnet)It is a strip-shaped safety sign. Easy to install. To instruct the informationMounting magnet Material magnetfrom S$11.99Min. 2 days
- UNIT (UNIT SAFETY SIGNS) Magnet signDimension (mm) 170×80 Mass (g) 40 Type of Sign Rubber magnet Material Rubber magnetfrom S$11.99Min. 2 days
- UNIT (UNIT SAFETY SIGNS) Work chief duty display boardThe face of the work chief is clear at a glance compared to the one with only the registration ceremony! The vinyl case for face photography has a structure that prevents rain from entering, so it is safe to use outdoors. You can also write a series of primary and secondary work chiefs.Dimension (mm) 500 × 400 × 1 thickness Material Eco Uniboard (Hole 4 holes)from S$19.99Min. 5 days
- UNIT (UNIT SAFETY SIGNS) Fire protection signMass (g) 18 Dimension (mm) 200×100×1.2 Trusco Part No. 333-9831 Sign Meaning Fire extinguisherfrom S$6.99Min. 2 days
- TOGUE ANZEN KOUGYOU Manager magnetWe will clearly display the type of work and the person in charge.Dimensions, Width x Length (mm) 80×200 Type of Sign magnetfrom S$57.99Min. 2 days
- TOGUE ANZEN KOUGYOU Fire chief stickerWe will clearly display the type of work and the person in charge.Manufacturer Product Code 263441 Dimensions, Width x Length (mm) 90×300 Sign Meaning Fire source manager Type of Sign Sticker / Stickerfrom S$25.99Min. 2 days
Filter by categories