It is a job sign required by the Occupational Safety and Health Regulations.
* When posting, please post in a place where there is no fire. * When storing, avoid places with fire, sunlight, and high temperature and humidity.
Type of Sign 4 corner holes Dimensions, Height x Width (mm) 500×400 Material Polypropylene
Thickness (mm) 1 Mass (g) 380 Dimension (mm) 600×450 Included Accessories Double-sided sheet tape x 6 sheets Material Hard envy Type of Sign Hole 4 Specification Φ3mm hole x 4
Uses 50% recycled polypropylene. It is a display based on Article 18 of the Occupational Safety and Health Regulations.
In the workplace where the work chief is selected.
* Screws are sold separately.
Occupational Safety and Health Regulations Volume 1, Chapter 2, Section 5, Article 18 When a business operator appoints a work chief, he / she posts the name of the work chief and the matters to be performed by that person in an easily visible place in the workplace. It must be made known to the ... Read More
Thickness (mm) 1 Trusco Part No. 113-8423 Mass (g) 378 Japanese Green Cross No. 49519 Dimension (mm) 600×450 Included Accessories Double-sided sheet tape x 6 sheets Material Hard envy Sign Meaning Specific chemical substances Specification Φ3mm hole x 4
Thickness (mm) 1 Mass (g) 380 Dimension (mm) 600×450 Included Accessories Double-sided sheet tape x 6 sheets Material Hard envy Type of Sign Hole 4 Specification Φ3mm hole x 4
It is a low foam polypropylene board. It's 1mm thick so it's not bulky. Ideal for disseminating the duties of the work chief and the name of the chief. Occupational Safety and Health Regulations Volume 1, Chapter 2, Section 5, Article 18 When a business operator appoints a work chief, he ... Read More
Dimension (mm) 500×400 Material PP (polypropylene) Shape Sign Classification The duties of the chief worker Type information
The face of the work chief is clear at a glance compared to the one with only the registration ceremony! The vinyl case for face photography has a structure that prevents rain from entering, so it is safe to use outdoors. You can also write a series of primary and secondary work chiefs.
Simply slide the sliders on both sides of the front cover up to insert and replace the face photo with the main unit attached. Contains face photos for 24 people. Since the surface vinyl cover is fixed with the left and right vinyl fasteners, it is a structure that does not allow rain to enter ev... Read More
The face of the work chief is clear at a glance compared to the one with only the registration ceremony. The vinyl case for face photography has a structure that prevents rain from entering, so it is safe to use outdoors. You can also write a series of primary and secondary work chiefs.
Mass (g) 200 Type of Sign Hole 4 Sumi Thickness (mm) 1 Material Eco Uniboard Dimensions, Height x Width (mm) 500×400