Emergency Exit / Evacuation Guidance Signs
Emergency exit signs (guide signs) are safety signs that are installed for fire fighting, disaster prevention, and crime prevention. It is installed in places where people use such as commercial facilities, schools, hospitals, and stations. The purpose of non-feeling signs (guide signs) is to guide people to evacuate safely in the event of a disaster or fire. Many things are made of phosphorescent material so that you can find the display even when the visibility is lost due to power failure or smoke. There are various types of designs, such as a green base with a picture of a person going to the exit, an emergency exit only, or an arrow.
Other Related Pages
- MonotaRO Sensor Light LED Door Opening and Closing Caution Sign LampOn the other side of the door, a sensor detects moving objects such as people, and the light on the other side flashes to notify you. It can be attached to a steel door with a magnet on the back. It can also be fixed to wooden doors with screws. * For alerting when opening and closing the door * ... Read MoreType of Sign Magnet type / screw type Cable Length (m) About 160 Sensor sensing range Approx. 120 ° horizontal, 110 ° vertical Color Green
- KING JIM Notification light for the door (wireless type)Lights and buzzers in various scenes inform you that there are people near the installed main unit. You can choose the notification method from three settings: light only / buzzer only / light + buzzer. Easy installation by sandwiching the iron door with the magnet on the back of the main body. F... Read MoreMass (g) Approx. 300 (excluding battery) Outer Dimensions, Width W x Depth D x Height H (mm) About 140 × 75 × 105
- Japan Green Cross Escape exit sign (phosphorescent type)It glows for a long time even when the electricity goes out. Since it is a phosphorescent type, only the surrounding white part (milky white part) shines. Japan Fire Fighting Sign Industry Association Quality Voluntary Control Sign Passed Product * Since it is a certified product with medium brig... Read MoreDimensions, Height x Width x Thickness (mm) 120×360×1 Mass (g) 80 Classification Evacuation guidance Type emergency exit
- KING JIM Notification light on the doorFlashes to let you know that there is a person behind the door. No tools required! Easy installation. Easy installation so that the door is sandwiched between the magnets on the back of the main unit. * Can be installed on doors that meet the following conditions. Open doors with magnets on both ... Read MoreCable Length (m) About 160 Sensor sensing range Approx. 120 ° horizontal, 110 ° vertical Type of Sign Magnet type Mass (g) 140 (excluding battery) Color Green
- MonotaRO Sticker evacuationIt is an evacuation display sticker that sticks to the partition board of the balcony of an apartment or building. Comes with adhesive tape on the back. It uses UV-resistant light-resistant ink for printing and is ideal for outdoor use. For attaching a partition plate * Do not use for any other p... Read More
- FIRST Evacuation sticker 150 x 400 (2-color type)An evacuation sticker that is easy to recognize with black and red letters on a yellow background. It is a display sticker that can easily display laws and regulations. It is a display sticker to be attached to the partition board of the balcony. * Wipe off any dust or dirt on the diaphragm befor... Read MoreDimensions, H x W (mm) 150×400 Color Base: Yellow Text: Black and red Material Polyester PET Type of Sign Sticker Back Side With adhesive tape
- MonotaRO Emergency Exit SignFor evacuation display in warehouses and offices * It is not a phosphorescent type. * Please use it as a support product.Dimensions, Height x Width x Thickness (mm) 120×360×1 Material PP Shape Sign Type emergency exit
- Japan Green Cross Evacuation guide signDimensions, Height x Width x Thickness (mm) 120×360×1 Mass (g) 62 Material Lami plate Shape Sign Type emergency exit
- ACE Evacuation stickerIt is a display sticker to be attached to the partition board of the balcony. * If the board is painted, it may not stick. * Wipe off any dust or dirt before applying.Type of Sign Sticker
- Japan Green Cross Medium brightness phosphorescent evacuation guide sticker signIt glows for a long time even when the electricity goes out. Convenient sticker type. Peel off the release paper and paste it. It is a fire-fighting certified product and is also suitable for fire-fighting and disaster prevention. * Since it is a certified product with medium brightness, it may n... Read MoreMaterial PET sticker Type of Sign Sticker
- MonotaRO Sticker Non-reflective Fire brigade entranceIt is a sticker that displays the entrance of the fire brigade. It is a non-reflective type. There are two types, one is pasted from the inside and the other is pasted from the outside. As an entrance display for the fire brigade * Do not use for any other purpose. * Wipe off any dust or dirt on ... Read MoreDimension (mm) 200 / side Material PVC sticker Shape trianglefrom S$3.69Min. 2 days
- UNIT (UNIT SAFETY SIGNS) Evacuation guide phosphorescent signSince it is a phosphorescent type, it can be reliably guided even at night. (With double-sided tape / Even if the light in the room goes out, the letters will be scattered.)Specification With two double-sided tapes
- UNIT (UNIT SAFETY SIGNS) Escape exit guidance sign Emergency exitIt is a certified product of the Fire Equipment and Safety Center of Japan. It is effective for evacuation guidance in the event of a fire power outage due to long-term light emission. It is a sign for evacuation guidance. For wall / door installation. * Be sure to use the phosphorescent product ... Read MoreType of Sign Double-sided tape Mass (g) 48 Material Hard phosphorescent plate Dimensions, Height x Width x Thickness (mm) 120×360×1.2
- Sanyo Shokai (AMENITY COX) Evacuation equipment, rescue bag, evacuation ladder plate signMaterial PVC plate Dimensions, Height x Width x Thickness (mm) 120×360×1
- UNIT (UNIT SAFETY SIGNS) Arrow stickersFor traffic restrictions such as stairsSpecification Backside adhesive
- UNIT (UNIT SAFETY SIGNS) High-intensity phosphorescent signIt is a high-intensity phosphorescent sign that emits light even after the lights are turned off and is intended to facilitate evacuation guidance in dark places. Enforced on December 1, 2009 It is a product conforming to the revision of the Fire Service Act Enforcement Regulations. Fire and Disa... Read MoreMaterial Phosphorescent vinyl chloride (PVC)
- Sanyo Shokai (AMENITY COX) Evacuation equipment installation location / installation room Plate signMaterial PVC plate Dimensions, Height x Width x Thickness (mm) 120×360×1
- Shinyei Home Create (Former Shinkyowa) Evacuation stickerSince the back side has double-sided tape, you can use it by pasting it as it is. It is a display sticker to be attached to the partition board of the balcony. * Before pasting, wipe off any moisture or dust on the board surface before pasting.Back Side Adhesive tape Material Aluminum foil Type of Sign Sticker Surface Vinyl coating
- Sanyo Shokai (AMENITY COX) Evacuation ladder sticker* Wipe off any dirt or dust on the sticking surface before sticking.Type of Sign Sticker / Sticker Material PVC sticker Dimensions, Height x Width x Thickness (mm) 100×300×1
- Japan Green Cross Evacuation guide sign (phosphorescent type)It shines for a long time even if the medium-brightness electricity that can be reliably guided at night is turned off. Japan Fire Fighting Sign Industry Association Quality voluntary control sign passed productDimension (mm) 100×300×1 Mass (g) 55 Other Conforms to JIS Z9107 Classification Evacuation guidance
- UNIT (UNIT SAFETY SIGNS) Passage guide sign Emergency exitIt is a certified product of the Fire Equipment and Safety Center of Japan. It is effective for evacuation guidance in the event of a fire power outage due to long-term light emission. It is a sign for evacuation guidance. For wall / door installation. * Be sure to use the phosphorescent product ... Read MoreMass (g) 48 Dimensions, Height x Width x Thickness (mm) 100×300×1.2 Type of Sign Double-sided tape Material Hard phosphorescent platefrom S$37.99Min. 2 days
- Japan Green Cross Fire brigade entrance markDimension (mm) 200 triangles Mass (g) 58 Sign Meaning Fire brigade entrance Classification Firefighting and dangerous goods Material Reflective sticker (acrylic film)
- MonotaRO Sticker reflection fire brigade entranceIt is a sticker that displays the entrance of the fire brigade. It is a type that reflects light even in the dark. There are two types, one is pasted from the inside and the other is pasted from the outside. As an entrance display for the fire brigade * Do not use for any other purpose. * Wipe of... Read MoreDimension (mm) 200 / side Material Acrylic reflective sticker Shape trianglefrom S$7.49Min. 2 days
- Japan Green Cross Medium brightness phosphorescent evacuation guide sticker signIt glows for a long time even when the electricity goes out. Convenient sticker type. Peel off the release paper and paste it. It is a fire-fighting certified product and is also suitable for fire-fighting and disaster prevention. * Since it is a certified product with medium brightness, it may n... Read MoreDimension (mm) 120×360 Mass (g) 30 Material PET sticker Type of Sign Stickerfrom S$43.99Min. 2 days
- Japan Green Cross Medium brightness phosphorescent evacuation guide sticker signIt glows for a long time even when the electricity goes out. Convenient sticker type. Peel off the release paper and paste it. It is a fire-fighting certified product and is also suitable for fire-fighting and disaster prevention. * Since it is a certified product with medium brightness, it may n... Read MoreMass (g) 10 Dimension (mm) 120×120 Material PET sticker Type of Sign Sticker
- ACE Entry reflective stickersIt is a display sticker of the fire brigade entrance. Peel off the tape on the back side and stick it from the inside of the glass as it is. * Wipe off any dust or dirt before applying.Size 200mm on each side Material Acrylic encapsulated red plate Specification Inner paste Color Red x silver Type of Sign Sticker Finish capsule
- TSUKUSHI KOBO Partition stickerDimension (mm) 150×400 Type of Sign Sticker Material Sticker
- TSUKUSHI KOBO Partition sticker (UR city organization standard specification)Dimension (mm) 150×400 Material PET (silver) sticker Type of Sign Sticker
- LTI Corp. Mid-intensity phosphorescent induction sign Fire-fighting certified product"Α-FLASH" TSN series. Obtained certification for medium-brightness phosphorescent induction sign. Brightness more than twice the certified standard value (brightness 80mcd / m2 or more after 20 minutes). In the case of a fluorescent lamp (common light source D65), the "JB standard&... Read MoreType of Sign Sticker / Sticker Thickness (mm) 0.35from S$33.99Min. 2 days
- Shinyei Home Create (Former Shinkyowa) Fire brigade entrance markIt is a display sticker of the fire brigade entrance. It is a type that is pasted from the outside of the window. The display is red on the outside of the window and white on the inside. Peel off the tape on the back side and stick it as it is. * Before pasting, wipe off any moisture, oil, dust, ... Read MoreDimension (mm) (One side) 200 Specification Adhesive surface: white surface Type For external application Color One side: Red / One side: Whitefrom S$11.99Min. 2 days
- Shinyei Home Create (Former Shinkyowa) Fire brigade entrance markIt is a display sticker of the fire brigade entrance. It is a type that is pasted from the inside of the window. The display is red on the outside of the window and white on the inside. Peel off the tape on the back side and stick it as it is. * Before pasting, wipe off any moisture, oil, dust, e... Read MoreDimension (mm) (One side) 200 Specification Adhesive surface: red surface Type For internal application Color One side: Red / One side: White Material Vinyl chloride red reflective sheetfrom S$9.69Min. 2 days
- UNIT (UNIT SAFETY SIGNS) Floor surface induction phosphorescent sign stickerSpecification Backside adhesive
- Japan Green Cross Evacuation equipment signDimension (mm) 120×360×1 Mass (g) 60 Material Hard envy Specification Table printing
- Japan Green Cross High-intensity phosphorescent exit signThe Fire Equipment and Safety Center of Japan certified the 2006 "Fire and Disaster Management Agency Notification No. 5" conformity. Products with a certificate do not need to be individually tested by the fire department.Material PET sticker Type of Sign Sticker
- GREEN CROSS Next door evacuation sign Spray plateSince it uses an aluminum composite plate, it is durable and can be used multiple times. It is a sheet that sprays letters on the partition board of the balcony of an apartment or building. * Unlike stainless steel, it deforms when a strong force is applied.Mass (g) 200 Dimension (mm) 320×450×t1 Material Aluminum composite plate
- UNIT (UNIT SAFETY SIGNS) Evacuation / guide sign Phosphorescent stickerDimensions, Height x Width (mm) 130×230 Material Phosphorescent stickers Type of Sign Sticker
- Japan Green Cross Evacuation guide signThickness (mm) 1 Dimension (mm) 100×300 Mass (g) 45 Classification Evacuation guidance Material Lami platefrom S$7.29Min. 2 days
- ESCO 120x360mm phosphorescent evacuation equipment signIt will shine for a few minutes even if the light goes out. * Mounting holes, double-sided tape, etc. are not processed.Thickness (mm) 1 Dimension (mm) 120×360 Esco Part No. EA983AF-94A Sign Meaning Evacuation ladder Material Hard PVC Specification Single-sided printing, phosphorescent
- LTI Corp. High Brightness Phosphorescent Induction StickerThe high-brightness phosphorescent guide sign SN << C class certification >> series has acquired "firefighting certification" as the "high-brightness phosphorescent guide sign" for the first time in Japan as a sticker type. In addition, it is the first product in t... Read MoreSpecification C200 grade Material PET / urethane / acrylic adhesivefrom S$57.99Min. 2 days
- Japan Green Cross Door evacuation displayJapanese Green Cross No. 069003 Dimension (mm) 150×400 Mass (g) 28 Trusco Part No. 814-8732 Classification Evacuation guidance Material Lumi Sticker (Phosphorescent Soft Enbi) Specification With D release paper Type of Sign With D release paper Type emergency exit Sign Meaning emergency exit