A telescopic whiteboard that is convenient for on-site shooting. Please use a magnetic display sticker on the iron plate at the tip. A whiteboard marker is attached on the back side.
For shooting at construction sites, for shooting during inspections and inspections
* Do not use for any other pur... Read More
It comes with a handbag and is convenient to carry. It comes with a stand and a pocket on the back that can be used to erase the blackboard and store markers.
As a shooting blackboard for various works
* Do not use for any other purpose.
You can easily shoot by yourself anytime, anywhere! It can be erased with a water-based marker. A marker with an eraser is set.
* The items displayed on the spare label are printed only on the factory name and location.
It is hard to reflect when shooting !! You can shoot with a flash or against the sun! Ideal for inspections and inspections of buildings, etc. Magnet can be attached. You can shoot on-site by yourself. Water-based crayons, whiteboard markers, and water-based markers can also be used. (* Oil-based... Read More
It is a construction blackboard that allows you to take pictures on site by yourself. You can use two sides, a whiteboard and a greenboard. Since the board is replaceable, you can use it according to the site if you prepare a replacement board sold separately. The green board has low reflection, ... Read More
Board Dimensions (width W x height H) (mm) 175×145
A low-reflection type that is less likely to reflect when shooting than a normal whiteboard. Made of steel, it is highly durable and can be fitted with a magnet. Writable even when wet. If you use a special kit pass, no powder will come out even if you write or erase it.
* If you use a normal whi... Read More
Shaft dimensions (mm) About 200-550 Display Items Construction name / location / date
It is easy to write with dark lines, and you can erase characters neatly. It is easy to take a picture of the site and it can be read clearly. Comes with a back stand.
It is a blackboard for on-site recording photography. (Excluding H)
Included Accessories Blackboard eraser, chalk (3 pieces)
There are two colors on the board, green and black! Please use your favorite color. It is used by writing directly on the resin plate surface. Because it is a resin, it is resistant to rain and water! The plate surface is specially processed and has low reflection!
* When erasing characters, wipe... Read More
Shaft dimensions (mm) About 200-550 Included Accessories Board marker fine white Display Items Construction name / location
The flash at the time of taking a picture is hard to reflect, and you can take a clear picture. Comes with an item mug sheet.
Whiteboard for site recording and photography
* Please do not use for any other purpose.
RoHS directive (corresponding to 10 substances) Correspondence
A steel board that is 1.5% lighter than conventional products and has excellent durability. Comes with a triangle net that is easy to put in and take out.
Site photo construction record
Mass (kg) 1.3 Included Accessories 2 white chalks, 1 Rahul (80 × 40 × 20mm) Type Green plate surface Specification With dark line
Single-sided vertical type and single-sided horizontal type can be used on both sides. Since the shaft comes to the end, it can be stored compactly and is convenient to carry. It can be erased with a water-based marker. A marker with an eraser is set. Item name: You can enter the construction nam... Read More
It is a sturdy steel surface. The strength is increased with an aluminum frame. Comes with a blackboard eraser and 3 chalks. Comes with a foldable stand on the back. Comes with a storage case. It has a dark line that is easy to write. Comes with a handle that is convenient to carry. Magnets can b... Read More
RoHS directive (corresponding to 10 substances) Correspondence
You can write smoothly. Since the cap has a magnet, it can be attached to the board. Easy-to-read white characters.
Replacement frame telescopic + board green marker
* Do not use for any other purpose.
Main Unit Dimensions (mm) 135×13.5×16 Mass (g) 9 RoHS directive (corresponding to 10 substances) Correspondence Type Fine print (round core) Ink Color White
A green mini board that does not easily reflect the flash when taking pictures. The flash when taking a picture is hard to reflect, and you can take a clear picture. With marker holder. You can attach the marker holder to any place on the back of the frame and fix the special marker for storage. ... Read More
Main Unit Dimensions (mm) 198 × 176 × 30 (when folded) Mass (g) 175
Comes with a back stand. Comes with a handle that is convenient to carry.
Whiteboard for site recording and photography
* Please use the whiteboard marker.
RoHS directive (corresponding to 10 substances) Correspondence
You can easily shoot by yourself anytime, anywhere! It can be erased with a water-based marker. Shooting can be adjusted by expanding and contracting the shaft. You can use it as a turtle stick by removing the board. A marker with an eraser is set as an accessory.
A low-reflection type that is less likely to reflect when shooting than a normal whiteboard. Made of steel, it is highly durable and can be fitted with a magnet. Writable even when wet. If you use a special kit pass, no powder will come out even if you write or erase it.
* If you use a normal whi... Read More
Shaft dimensions (mm) 200~550 Specification Magnet mounting possible
A whiteboard with a stand on the back. With a handle, it is convenient to carry. Comes with a pen and a blackboard eraser storage bag.
For on-site recording and photography
* Please use the whiteboard marker.
Dedicated to site memos, how to use depends on the idea.
* MD-1F: The reattachment sticker is a sticker for memo sticks M and D-1F. A replacement sticker for D-1 type can also be used. * MD-2CF: The reattachment sticker is a sticker for memo sticks M and D-2CF. A replacement sticker for D-2 / C6 ... Read More
Shaft dimensions (mm) 200~550 Specification Can be used as a sticker
A telescopic green board that is convenient for on-site shooting! The long-awaited appearance of a sticker-type green that has never existed before! Lightweight because it is a seal type! Can be replaced. It's green so it's hard to reflect.
Shaft dimensions (mm) About 200-550 Display Items Construction name / location / date
Since the cover is fixed with a magnet, it is very easy to put in and take out paper. Since the base is made of aluminum, the appearance is beautiful and durable. It is a rainproof type and it is difficult for rain to enter. (Waterproof for daily life)
For on-site pre-work meetings
A smooth surface with good chalk glue. A paint that suppresses light reflection prevents shooting failures. A highly durable blackboard that does not easily warp or crack. With dark lines (line width 1 mm / 5 cm grid).
Hard to reflect. The flash when taking a picture is hard to reflect, and you can take a clear picture. You can easily change it by simply pasting the item mug sheet (sold separately). The unused item mug sheet can be protected by pasting it on the back side. It can be firmly fixed at any angle.
Main Unit Dimensions (mm) (When folded) 198 x 176 x 30 Mass (g) 206 RoHS directive (corresponding to 10 substances) Correspondence Included Accessories Whiteboard eraser, whiteboard marker
By using a water-resistant blackboard chalk for the water-resistant blackboard, characters will not flow. You can take construction record photos even on rainy days. Comes with a back stand. It has a dark line that is easy to write.
Blackboard for site records and photography
* You can only write... Read More
RoHS directive (corresponding to 10 substances) Correspondence Type Water resistant Material Wood
With eraser. You can erase the written characters. With magnet. Since the cap has a magnet, it can be attached to the board. Narrow marker. The line width is about 1.0 mm and you can write small characters.
Dimension (mm) 135×13.5×16 Mass (g) 9 RoHS directive (corresponding to 10 substances) Correspondence
A low-reflection type that is less likely to reflect when shooting than a normal whiteboard. Made of steel, it is highly durable and can be fitted with a magnet. Writable even when wet. If you use a special kit pass, no powder will come out even if you write or erase it.
* If you use a normal whi... Read More
Shaft dimensions (mm) About 200-550 Specification Magnet mounting possible
It is a magnet type and stronger than before. It is a rainproof type and it is difficult for rain to enter. There are three sizes: A3 horizontal, A4 vertical, and A4 horizontal. Other types can be supported by replacing the paper inside.
For on-site pre-work meetings
You can attach a digital camera and use it in video mode or self-timer. It is convenient for shooting at angles that are difficult to shoot with your hands and for shooting at high places.
The plate is a sliding type and can be easily replaced!
Introducing a board that can be used by replacing the display plate according to the situation!
* Replacement plate is not included. * Accessories will be changed to the writing tools listed in sequence.
Included Accessories Kit pass (white) Shaft dimensions (mm) About 200 to about 550
[Magnets can be attached to both the front and back!] POINT1: The main body uses a material that is resistant to water. POINT2: The length of the handle can be adjusted according to the situation. POINT3: Comes with a storage bag that is convenient to carry.
Mass (g) About 400 Included Accessories Writing instrument: 1 / Storage bag: 1 Shaft dimensions (mm) About 280-720 Dimensions, H x W (mm) (Board) Approx. 230 x 320 Effective display dimensions (mm) About H195 × W about 310
Handle, foldable stand, aluminum frame, large storage net, 1 marker (black), ruffle with magnet (size: 115 x 55 x 20 mm)
Site photo construction record