Chemical Bottles
A medicinal solution bottle is a tool for containing chemicals (liquids) such as distilled water and culture solutions. Also called medicine bottle. The main body is made of glass or plastic, so you should choose the material according to the type of liquid you put inside. It is a tool used in medical institutions and research facilities, and there is also a type that is compatible with the autoclave used when sterilizing the instruments used and extracting in research. Not only can it be stored, but there are also types with stopcocks and spray types, so you can choose the appropriate one depending on the site where you use it.