Cleanroom Caps
A clean cap is a work wear that is designed to prevent dust from flying around or adhering to the body due to static electricity by weaving conductive thread into the fabric and taking measures against static electricity. Mainly used in clean room areas where anti-static measures are taken. It is an effective item when used in conjunction with cleanroom shoes and clothing. In addition, by using it together with an inner cap, it is possible to more effectively prevent hair from getting mixed in and falling out.
- ESCO Helmet-compatible disposable hood (SMS non-woven fabric / 10 sheets)The front has a film that does not easily fog. Prevents light dust. * Helmet is sold separately.Size Free Specification Helmet compatible Material Polypropylene, PET
- TOYO LINT FREE Clean CapClean room capMaterial 100% polyester Grade Class 1000 Size LLfrom S$18.99Min. 2 days
- AS ONE Disposable Color CapIt can be used by color-coding by department or work.Material Non-wovenfrom S$27.99Min. 2 days
- Ozu Mobcap WhiteIt is a stick-shaped bellows type that is spread and worn. After use, pull both ends to return to their original shape.Material Non-wovenfrom S$46.99Min. 2 days
- AS ONE Inner CapAs it dries quickly, you can wash the cap, which is easy to get stuffy, frequently to keep it hygienic. The three-dimensional type prevents the hairstyle from collapsing significantly, and the round type has a shape that completely wraps around the neckline.Material Nylonfrom S$139.90Min. 4 days
- AS ONE Fit HoodIt is a cover type hood with excellent fit and little individual difference when worn. Good stain removal and excellent washability. It is hygienic because it does not use a hook-and-loop fastener. Even if you use glasses, there will be no gap between the hat and the temples. You can put on and t... Read Morefrom S$28.99Min. 13 days
- AS ONE Fit InnerAn inner hood that is a cover type and has excellent fit, with little individual difference when worn. You can put your ears out, so you can put your glasses directly on your ears.As ONE Part Number 3-5399-01 Type Mfrom S$17.99Min. 4 days
- AS ONE Disposable Hoods StandardSince it wraps the entire head, it prevents dust and can be used for spraying chemicals.As ONE Part Number 3-4752-01from S$43.99Min. 4 days
- AS ONE Hair NetComes with a soft band that has a sweat-preventing effect to prevent hair from falling out of the gaps around the face. You can adjust the size with the hook-and-loop fastener on the back.from S$199.90Min. 4 days
- AS ONE Hair NetComes with a soft band that has a sweat-preventing effect to prevent hair from falling out of the gaps around the face. It is a type that fits comfortably and does not have a hook-and-loop fastener under the chin.from S$339.90Min. 9 days
- AS ONE HoodThe face is made of sweat-absorbing and quick-drying knit, which fits perfectly on the forehead and cheeks. Comes with a masking function.from S$44.99Min. 4 days
- Buruneezu Disaster Prevention HoodA cushion that can be used as a disaster prevention hood in an emergency. Honeycomb mesh is used for the head, and it has excellent breathability and durability. It can usually be used as a multipurpose cushion.As ONE Part Number 3-7709-01 Type Skit twistfrom S$159.90Min. 11 days
- AS ONE Hair NetComes with a soft band that has a sweat-preventing effect to prevent hair from falling out of the gaps around the face. The ears are processed so as not to block the sound or voice.from S$249.90Min. 13 days
- Nissei Denki NS mobcapIt has excellent breathability and is comfortable for long hours of work.Material 1 bag of non-woven fabric (100 pieces) TKG Part No. 8-1435-1301from S$15.99Min. 5 days
- TOKUSHUIRYOU Protective cap (BOU0I abonet)Since it can be folded, it saves space in the storage area. By hooking the folded chin strap on the hook, it is also convenient to keep under the desk or in a locker. When folded, it has about 1/3 the volume of a helmet.Discontinued