All Category

Cutting Mats

View : Grid List
Filter

15 Item(s)

Set Ascending Direction
  1. Cutting Mat with Scale 1100
    YAYOI CHEMICAL INDUSTRY Cutting Mat with Scale 1100
    When used as an underlay when cutting cloth, the blade will not shake much and stable cutting will be possible. The blade of the cutter and kitchen knife is not easily damaged and lasts a long time. It can be used on both sides and has a scale on one side. * Avoid using or storing in places with ... Read More
    Width x Length (mm)  170×1100  Thickness (mm)  About 3.1 
    Rating:
    100%
    from S$39.99
    Min. 8 days
  2. Cross cutting mat
    KYOKUTO (Kyokuto-Sanki) Cross cutting mat
    It is a mat for cutting that does not open the cut even if the blade of the cutter is inserted. Unlike plywood, the blade is less damaged, the cutter blade does not escape, and running is smooth. Can be used on both sides.
    Thickness (mm) 
    Rating:
    80%
    from S$48.99
    Min. 2 days
  3. Cutting mat with scale 1400
    YAYOI CHEMICAL INDUSTRY Cutting mat with scale 1400
    When used as an underlay when cutting cloth, the blade will not shake much and stable cutting will be possible. The blade of the cutter and kitchen knife is not easily damaged and lasts a long time. It can be used on both sides and has a scale on one side. * Avoid using or storing in places with ... Read More
    Width x Length (mm)  170×1400  Thickness (mm)  About 3.1 
    Rating:
    93%
    from S$59.99
    Min. 8 days
  4. Cross-cutting mat
    HIROSHIMA Cross-cutting mat
    The cutter blade does not run along the front cut like plywood. As it is a mat type, it can be used repeatedly. There is less damage to the cutter blade. Can be used on both sides. * Since it is not a heat-resistant type, do not leave it in a place where it gets hot indoors such as a car.
    Rating:
    67%
    from S$39.99
    Min. 2 days
  5. Cutting mat joint type 600
    YAYOI CHEMICAL INDUSTRY Cutting mat joint type 600
    It is convenient because it can be connected and used according to the length of the object you want to cut. Easy to carry in-vehicle or on-site. Made of olefin resin, it can be used on both sides, and has a scale on one side. * Please use it on a flat surface with no steps.
    Dimension (mm)  600 (effective 580) x 290  Thickness (mm)  About 3.1 
    Rating:
    40%
    from S$33.99
    Min. 9 days
  6. NEW cutting mat
    YAYOI CHEMICAL INDUSTRY NEW cutting mat
    It is a large cutting mat that can be used as a workbench for sliding sliding doors and covering. There is little blurring of the blade during cutting, and it can be cut smoothly and neatly. It lasts a long time without damaging the blade of the cutter or kitchen knife. Can be used on both sides.... Read More
    Thickness (mm) 
    from S$669.90
    Min. 5 days
  7. Joint underlay
    KYOKUTO (Kyokuto-Sanki) Joint underlay
    If you lay a joint underlay between the wallpaper and the board, you can protect the base and cut the joint. Please help prevent opening after construction. It is very economical because it can be used repeatedly.
    Thickness (mm)  0.2  Overall Length (m)  10  Width (mm)  35  Material  Stainless steel 
    from S$43.99
    Min. 2 days
  8. NEW cutting mat
    YAYOI CHEMICAL INDUSTRY NEW cutting mat
    It is a large cutting mat that can be used as a workbench for sliding sliding doors and covering. There is little blurring of the blade during cutting, and it can be cut smoothly and neatly. It lasts a long time without damaging the blade of the cutter or kitchen knife. Can be used on both sides ... Read More
    Dimension (mm)  1000×2000  Thickness (mm) 
    from S$469.90
    Min. 5 days
  9. Cutting mat
    YAYOI CHEMICAL INDUSTRY Cutting mat
    There is little blurring of the blade during cutting, and it can be cut smoothly and neatly. It lasts a long time without damaging the blade of the cutter or kitchen knife. It uses environmentally friendly recycled olefin resin and has double-sided ruled lines, so it can be used on both sides.
    Thickness (mm)  Dimension (mm)  450×600 
    from S$48.99
    Min. 5 days
  10. Stainless joint underlay
    YAYOI CHEMICAL INDUSTRY Stainless joint underlay
    It is an underlay to prevent the base from being cut when cross-joint lap cutting. Made of stainless steel, it is resistant to rust and can be used repeatedly.
    Width (mm)  35  Length (m)  1.2  Thickness (mm)  0.2 
    from S$57.99
    Min. 5 days
  11. Cutting mat joint type 600
    YAYOI CHEMICAL INDUSTRY Cutting mat joint type 600
    from S$32.99
    Min. 5 days
  12. Stainless joint underlay
    HIROSHIMA Stainless joint underlay
    After sticking the cloth on the wall, insert it into the joint and use it. Prevents the cutter blade from biting into the base, board, etc., and eliminates the opening of the cloth.
    Length (m)  10  Material  Stainless steel  Width (mm)  35  Thickness (mm)  0.2 
    Discontinued
  13. Samurai cutting mat
    HIROSHIMA Samurai cutting mat
    It protects the board and also protects the cutting edge of the blade.
    Discontinued
View : Grid List
Filter

15 Item(s)

Set Ascending Direction