Automotive Spark Plugs
Other Related Pages
- NGK Spark Plug (B ~)Standard plug (plug for new car assembly) * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.
- NGK Ignition CoilWe provide ignition coils with excellent performance by using the advanced ignition system technology and strict quality standards cultivated over many years of NGK spark plugs. In an internal combustion engine that uses a spark plug, a high voltage of 20,000 to 35,000 V is required to discharge ... Read More
- NGK Spark Plug (C ~)Standard plug (plug for new car assembly) * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.
- NGK NGK iridium plugIt will be the iridium plug installed in the new car. * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.
- NGK Plug CordApplicable to a wide range of vehicle models and provides excellent driving performance Metal resistance windings have stable resistance values and excellent transmission performance, which is the original function of the cord. Radio interference caused by noise generated from the ignition system... Read More
- NGK Premium RX PlugThe world's first new material "ruthenium compound center electrode" and "platinum protrusion + oval shape" outer electrode are adopted. A next-generation premium plug that achieves outstanding ignitability and achieves total performance such as low fuel consumption, stain... Read MorePart No. -
- NGK Spark Plug (L ~)Standard plug (plug for new car assembly) * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.
- NGK Spark Plug (D ~)Standard plug (plug for new car assembly) * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.
- HITACHI Ignition Coil"Rotation does not increase when accelerating, or there is a breathing noise" "Idling becomes unstable or stops" "Battery or alternator is normal but the engine does not start easily" Ignition coil There is a possibility of a malfunction! The ignition coil is a devic... Read More
- NGK Iridium Max PlugAchieve a long life while maintaining the performance of the IX plug! Iridium alloy is used for the center electrode, platinum chips are used for the outer electrodes, and precious metals are used for both electrodes. In addition to improving the ignitability and fuel efficiency of the IX plug, t... Read MoreGenuine Part No. -
- NGK Iridium IX PlugIridium IX is an iridium plug that can be replaced with a standard heat value mounting (new car mounting) plug. Combustion spreads faster than general plugs, and a thermo-edge is provided at the tip of the insulator to improve plug fouling. A high-value-added plug that enables ignition, accelerat... Read MoreGenuine Part No. - Cross Reference Part No. (DENSO) -
- NGK Spark Plug (Z ~)The center electrode has a "copper cored" structure in which copper is sealed close to the tip so that a large amount of heat can be released quickly. This provides an ultra-wide range plug that is resistant to burning and smoldering. Uses new ceramic insulator. The register plug has an... Read More
- TORCH Spark plugIt is a manufacturer of spark plugs for automobiles, motorcycles, small gasoline engines, etc., and has a track record of delivery to automobile manufacturers' production lines. With a share of more than 40% of the domestic market in China, it is used habitually in more than 20 countries arou... Read MoreTerminal Shape Integrated type
- NGK Platinum PlugPlatinum alloy or iridium alloy is used for the center electrode. Platinum alloy is also used for the outer electrode discharge part. Platinum plugs are high-performance, long-life plugs that can reduce electrode wear. * We recommend that you ask a maintenance company to replace this product. Com... Read More
- NGK Iridium Max PlugAchieve a long life while maintaining the performance of the IX plug! Iridium alloy is used for the center electrode, platinum chips are used for the outer electrodes, and precious metals are used for both electrodes. In addition to improving the ignitability and fuel efficiency of the IX plug, t... Read MoreMain Compatible Genuine Part No. 1A14-18-110
- TORCH Iridium spark plugThis iridium plug is a product with improved ignition performance compared to ordinary spark plugs. It is a manufacturer of spark plugs for automobiles, motorcycles, small gasoline engines, etc., and has a track record of delivery to automobile manufacturers' production lines. With a share of... Read MoreMain Compatible Genuine Part No. 09482-00527 Thread Diameter (mm) 12 Hex Width Across (mm) 16 Screw Length (mm) 19 Base Flat sheet Cross Reference Part No. (DENSO) IXU22 Terminal Shape Integrated type Cross Reference Part No. (NGK) KR7AI Screw Dimensions M12×1.25
- Champion Iridium PlugChampion Spark Plug is one of the world's leading spark plug manufacturers with history and tradition! Iridium is used for the center electrode and platinum pad is used for the ground electrode to guarantee durability of 100,000 km. Excellent ignitability improves fuel efficiency. High ignita... Read MoreRecommended Timing to Replace 100,000km Electrode Dimension (mm) Φ0.7 Terminal Shape -
- NGK Glow PlugCompression ignition Internal combustion engine (mainly diesel engine) Auxiliary heat source plug that helps start when cold. * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.
- NGK Power CableHigh performance that maximizes the performance of the machine The NGK power cable uses low resistance variable pitch winding and hyper silicon to reliably transmit the spark energy sent from the ignition coil and maximize performance. * We recommend that you ask a maintenance company to replace ... Read More
- NGK Racing PlugThe racing plug can be selected to maximize the performance when it is used by increasing the engine output due to racing, circuit driving or tuning, compared to the standard plug installed in new cars. The shape is different from the standard plug, and the life of the plug and the performance at... Read MoreGenuine Part No. -
- NGK Spark plug (A ~)Standard plug (plug for new car assembly) * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.Cross Reference Part No. (DENSO) -
- NGK Premium RX PlugThe world's first ruthenium-blended center electrode and platinum protrusion + oval-shaped outer electrode are used. A next-generation premium plug that achieves outstanding ignitability and achieves total performance such as low fuel consumption, stain resistance, and long life. * We recomme... Read More
- DENSO Two Tops (TT) plugAchieves improved fuel efficiency by improving ignition and flying performance. Furthermore, since 45 models can be consolidated into 6 models, it is possible to reduce the inventory burden of stores! * We recommend that you ask a maintenance company to replace this product. Compensation may not ... Read More
- NGK ignition coilWe provide ignition coils with excellent performance by using the advanced ignition system technology and strict quality standards cultivated over many years of NGK spark plugs. * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the repl... Read More
- NGK Spark plug (U ~)Standard plug (plug for new car assembly) * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.Part No. - Cross Reference Part No. (DENSO) -
- NAP ignition coilGenuine equivalent number 90048-52125, 90048-52125-000, 90048-52126, 90048-52126-000 * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.
- NGK Spark Plug (R ~)Racing plugs Full performance even in extremely tuned engines and extremely harsh driving conditions. Please select according to each engine and maximize its performance. The center electrode has a "copper cored" structure in which copper is sealed close to the tip so that a large amoun... Read MoreCross Reference Part No. (DENSO) -
- NGK Spark Plug (F ~)Standard plug (plug for new car assembly) * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.Cross Reference Part No. (DENSO) -
- NGK Iri series plugIridium plugs are iridium plugs with excellent ignitability and acceleration for tuning engines that require high heat value. The shape of the insulator has been renewed and three bands have been added to the corrugation, and the main metal fittings have also been plated with excellent corrosion ... Read MorePart No. -
- NTK (NGK) NGK Spark Plug O2 sensor Daihatsu * 93443 NGKMain Compatible Genuine Part No. 89465-B2101 Compatible Manufacturer DAIHATU
- NGK Spark plug (G ~)The center electrode has a "copper cored" structure in which copper is sealed close to the tip so that a large amount of heat can be released quickly. This provides an ultra-wide range plug that is resistant to burning and smoldering. Uses new ceramic insulator. The register plug has an... Read MoreCross Reference Part No. (DENSO) - Terminal Shape Separate type
- Champion Champion spark plugSpecification (Number of used) 2 Representative Model 1200FX・FL・XL・1340FL・FXfrom S$9.69Min. 2 days