Remote Engine Starters / Keyless Entry System
- Bullcon Auto door mirror controller Coupler type for ToyotaSince it has both remote control key interlocking type and ACC interlocking type operation functions, you can select the operation type according to your preference. (Selectable at the time of installation) Easy OFF function adopted! * If the vehicle switch is set to the retracted side, this prod... Read MoreWarranty Period 1 year Compatible Manufacturer Toyota, Subaru
- Bullcon Auto door mirror controller Honda exclusive coupler typeSince it has both remote control key interlocking type and ACC interlocking type operation functions, you can select the operation type according to your preference. (Selectable at the time of installation) Easy OFF function adopted! * If the vehicle switch is set to the retracted side, this prod... Read MoreWarranty Period 1 year Compatible Manufacturer For Honda onlyfrom S$149.90Min. 12 days
- Bullcon Auto door mirror Remote control key interlocking typeThe door lock retracts the door mirror, and the unlock unlocks the door mirror. Since the door mirrors are stowed after getting off, you can also check the rear safety when getting off. Also, by connecting the key detection line, malfunctions during driving can be prevented. * Please check the ma... Read MoreInput Power (V) 12 Warranty Period 1 yearfrom S$149.90Min. 11 days
- PROTECTA Scan lock RF (non-contact type)You can increase the number of vehicle door keys to a maximum of 7. You can lock and unlock the door by holding the one with the IC chip registered in advance through the outer glass over the in-vehicle unit. If you have an IC chip, you can use the attached sticker such as a driver's license,... Read MoreIncluded Accessories RFID card, RFID sticker Power Input (DC-V) 12 (for minus ground cars only)from S$399.90Min. 7 days
- Bullcon Automatic door mirror option Relay unit type 1Required when installing ADL-11 / ADK-98 on a switch type [D] vehicle. (Mainly Toyota cars)from S$49.99Min. 12 days
- Bullcon Auto door mirror controller Daihatsu exclusive coupler typeSince it has both remote control key interlocking type and ACC interlocking type operation functions, you can select the operation type according to your preference. (Selectable at the time of installation) Easy OFF function adopted! * If the vehicle switch is set to the retracted side, this prod... Read MoreWarranty Period 1 year Compatible Manufacturer For Daihatsufrom S$149.90Min. 12 days
- Bullcon Auto door mirror controller Lexus IS exclusive coupler typeSince it has both remote control key interlocking type and ACC interlocking type operation functions, you can select the operation type according to your preference. (Selectable at the time of installation) Easy OFF function adopted! * If the vehicle switch is set to the retracted side, this prod... Read MoreWarranty Period 1 year Compatible Manufacturer Dedicated to Lexus ISfrom S$359.90Min. 12 days
- SCIBORG Screw tap (4 pieces)Required for direct wiring without using an OBDII coupler.Suitable for 0.65-0.8mm wirefrom S$9.69Min. 3 days
- Bullcon Automatic door mirror ACC interlocking typeWhen the engine key is set to ACC, the door mirror returns, and the door mirror is retracted about 10 seconds after the key is turned off. Also, by connecting the key detection line, it is possible to store it about 10 seconds after removing the key. * Please check the manufacturer's website ... Read MoreInput Power (V) 12 Warranty Period 1 yearfrom S$139.90Min. 12 days
- Bullcon Auto-door mirror controller Nissan exclusive coupler typeSince it has both remote control key interlocking type and ACC interlocking type operation functions, you can select the operation type according to your preference. (Selectable at the time of installation) Easy OFF function adopted! * If the vehicle switch is set to the retracted side, this prod... Read MoreWarranty Period 1 year Compatible Manufacturer Nissan onlyfrom S$149.90Min. 12 days
- MIRAREED LED light sound sensorA bullet-shaped LED light with a sound sensor that lights up in response to sound. Creates a moody space with beautiful light. By sticking and fixing with a mounting stay, it can be easily placed inside the pillar, under the seat, or on the floor mat. With the rotation angle adjustment function, ... Read MoreRated Voltage (DC V) 12 (for domestic cars)Discontinued
- SCIBORG Auto door lock system (with emergency anti-lock function)Door lock at 20km / h! Set the shift to "P" to unlock the door! With an emergency unlock function that unlocks after about 9 seconds when sudden deceleration is detected! No complicated wiring work is required just by attaching it to the OBD2 coupler! It can be securely attached without... Read MoreDiscontinued
- SCIBORG Auto door lock system (with SL20 series ESS function)Door lock at 20km / h! Set the shift to "P" to unlock the door! With an emergency unlock function that unlocks after about 9 seconds when sudden deceleration is detected! With an emergency braking display (ESS) function that automatically blinks the hazard when sudden braking is detecte... Read MoreConform to For Toyota cars onlyDiscontinued
- DELTA Keyless entry system kitKeyless entry kit with answerback function Keyless kit (4 actuators included). Non-keyless cars are very inconvenient. If you insert the key every time, the body will be scratched and the paint will come off very often. Let's make it keyless to reduce important car scratches and improve conve... Read MoreIncluded Accessories 4 actuators, 2 remote controlsDiscontinued
- Amon Industry Cable branch boxUses 24K plating that has low contact resistance and is resistant to corrosion. Branch the 22sq cable into four 8sq cables.Included Accessories With hexagon wrench 3 / 4mm Size About 69L × 25W × 24Dmm Applicable Power DC12V1200W(MAX)、DC24V2400W(MAX)Discontinued
- PROTECTA Scan lock (password entry type)Must-see for those who surf and have outdoor experience! Touch the unit attached to the inside of the vehicle with your finger through the outer glass and operate the keys! You can lock and unlock the door by entering the password. You can set a free security code between 4 and 10 digits. (Over 1... Read MoreCurrent Consumption (mA) 11 Power Input (DC-V) 12 (for minus ground cars only)Discontinued
- SCIBORG Auto door lock system (SL20 series) linked to vehicle speedDoor lock at 20km / h! Set the shift to "P" to unlock the door! With an emergency unlock function that unlocks after about 9 seconds when sudden deceleration is detected! Lightweight and compact type with integrated coupler!Discontinued
- Just Corp. Car verification case (plain product) / thick two-fold typeFor those who want a car verification box with plenty of space! The gusset in the pocket is 3 cm !! You can safely put in a thick instruction manual! In addition, it is very convenient with a middle bag, pocket, and business card holder (3 pieces)! Recommended for car dealers! Ideal for storing c... Read MoreMaterial PVC Color BlackDiscontinued
- SCIBORG Auto door lock system linked to vehicle speedDoor lock at 20km / h! Set the shift to "P" to unlock the door! No complicated wiring work is required just by attaching it to the OBD2 coupler! It can be securely attached without burdening the vehicle! Ensuring passenger safety (preventing tampering with children, measures against car... Read MoreDiscontinued
- NAPOLEX Glove box partition plate setIt is a partition plate set that can neatly organize the glove box that is easy to mess up when you put other small items such as a car verification storage case and an instruction manual. Since the partition plate can be attached in any position, it can be adjusted according to the stored items.... Read MoreMass (g) 250Discontinued
Filter by categories