Automotive Cutting & Milling Tools
Cutting is an operation that uses a blade to scrape off unnecessary parts of the material during plating and painting. We mainly use tools such as spot cutters, scissors, and drills. There are various types of spot cutters, such as those with a modified cross-sectional shape of the blade and those using tungsten carbide with high altitude. By applying a spot cutter lube, cutting performance is improved and wear of the cutting edge can be suppressed. Using a joint that can extend the length of a spot cutter or drill will improve workability.
- MonotaRO Spot cutter Cobalt high speed TiN coatingDemonstrates sharpness and durability due to the cross-sectional cutting edge shape. A high-performance spot cutter that supports recent difficult-to-cut materials. For spot welding removal * Do not use for anything other than its intended purpose. * Never touch the rotating tools and chips. * Be... Read MoreMaterial Cobalt heiss Surface Treatment TiN coating
- Ishihashi Seiko Spot cutter high speed homo processingThe unique cross-sectional cutting edge shape provides the best sharpness and durability. Carefully selected high-speed steel material is homogenized, and the use of a small amount of cutting oil further extends the life. Using an air drill or an electric drill for 10 mm or more, around 800 rpm i... Read MoreSurface Treatment Homo processing Classification of the Hazardous Non-dangerous goods
- Ishihashi Seiko Spot cutter high-speed titanium coatingThe unique cross-sectional cutting edge shape provides the best sharpness and durability. Carefully selected high-speed steel material is homogenized, and the use of a small amount of cutting oil further extends the life. Using an air drill or an electric drill for 10 mm or more, around 800 rpm i... Read MoreClassification of the Hazardous Non-dangerous goods Surface Treatment Titanium coating
- Ishihashi Seiko Spot cutter high speed TiALN coatingThe unique cross-sectional cutting edge shape provides the best sharpness and durability. Carefully selected high-speed steel material is homogenized, and the use of a small amount of cutting oil further extends the life. Using an air drill or an electric drill for 10 mm or more, around 800 rpm i... Read MoreClassification of the Hazardous Non-dangerous goods Surface Treatment TiALN coating
- MonotaRO Spot cutter Carbide TiALN coatingDemonstrates sharpness and durability due to the cross-sectional cutting edge shape. A super-performance spot cutter that supports recent difficult-to-cut materials. For spot welding removal * Do not use for any other purpose. * Never touch the rotating tools and chips. * Be careful not to get in... Read MoreBlade Length (mm) 27 Blade Diameter (mm) 8 Shank Diameter (Φmm) 8 Overall Length (mm) 80 Material Carbide (CARBIDE) Surface Treatment TiALN coating
- OHTSUKA BRUSH MFG. Bulldog spot cutterIn order to achieve a good bite to the weld nugget, the tip shape has been uniquely designed. By applying a smoothing treatment, which is a unique technology, to the cutting edge, cutting resistance is actually reduced. High-grade powder highs are used for the cutter material! Compared to general... Read MoreRoHS directive (corresponding to 10 substances) Correspondence
- NIPPEI KIKI Spot Ace Cutter QUATROHigh durability with original 4-flute & ceramic coating. The 4-flute tip, which pursues durability, always catches the cutting surface even if the hand drill's peculiar blurring occurs, enabling speedy and stable work. Cobalt high-speed steel HSS-Co material is coated with a unique cerami... Read MoreSet Contents 5 replaceable blades, 1 shank Shank Diameter (mm) 6.35 (Hex axis) Overall Length (mm) 74 (shank + replaceable blade) Classification of the Hazardous Non-dangerous goodsfrom S$199.90Min. 2 days
- Cyuo Token Spot cutterA super-performance spot cutter that can sharpen recent difficult-to-cut members such as ultra-high-strength steel sheets and ultra-super-hard-tensile steel sheets at once, and can handle more than 10 conventional drills.Material Super cobalt VR material Feed angle (mm) 50~180 Overall Length (mm) 80
- RUKO Spot Cutter (Cobalt High Speed Steel)Drilling with high accuracy is possible by suppressing core shake and burrs. For removing spot weldingMaterial Cobalt heiss Classification of the Hazardous Non-dangerous goodsfrom S$22.99Min. 2 days
- BIC TOOL Gekko Kintaro LongAstonishing sharpness + durability of moonlight technology. Compatible with the latest ultra-super steel sheets. Spot cutter Polishing machine Loken S-2000 (No. 1 sharpening only) Re-polishing is possible. Like Kintaro-ame, it maintains new performance even after re-polishing. Car spot welding re... Read MoreRecommended Tool (Polishing machine) ROKEN S-2000 Recommended Rotation Speed (min -1 [rpm]) 1000~1200 Overall Length (mm) 150 Drill Diameter (Φmm) 8.2 Shank Diameter (Φmm) 9 Classification of the Hazardous Non-dangerous goodsfrom S$259.90Min. 2 days
- Isco Spot cutter ceramic coating longIf it is the length of a normal spot cutter such as a step part, rocker panel, rear member, etc., it is effective when the tip of the air drill body hits the body and the cutter does not enter the welded part straight. High-strength steel plate automobile body, etc.Overall Length (mm) 150 Blade Diameter (mm) 8.2 Dimension (mm) 8.2×150 Color Black bio red Classification of the Hazardous Non-dangerous goods
- Cyuo Token Spot cutter (for Spotle)By using a cemented carbide exclusively for RC-30N, the cutting time has been reduced to 1/10 compared to conventional products for cutting ultra-high-strength steel sheets. Lifespan is comparable to hundreds of drills.Allowable Rotation Speed (min -1 [rpm]) (Cutting edge) 1000-2500 Mass (g) 25 Overall Length (mm) 39 Feed angle (mm) 50~650 Cutting Tip Diameter (Φmm) 8 Classification of the Hazardous Non-dangerous goods Material Tempered cemented carbide Size Φ8.0X39
- KOTO Spot drill 85A spot drill with a ceramic coating. A spot drill that suppresses the generation of heat in accordance with low rotation. Considering the size of the nugget, Φ8.5mm is used.Specification In a special case Classification of the Hazardous Non-dangerous goodsfrom S$109.90Min. 4 days
- Isco Spot cutter multilayerTungsten carbide, which is said to be the second hardest material after diamond, is used, and due to its unprecedented durability and special 3-flute shape, it is an excellent tool that can cut things that cannot be cut with a normal cutter. Ultra high-strength steel plate automobile bodyColor Black silver Classification of the Hazardous Non-dangerous goods Material Tungsten carbide (tungsten carbide)from S$239.90Min. 4 days
- JTC Stainless scissorsExcellent sharpnessOverall Length (mm) 205 RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$46.99Min. 6 days
- NIPPEI KIKI Spare blade for spot ace cutter QUATRO (Quattro)Spot ace cutter QUATRO dedicated spare bladeClassification of the Hazardous Non-dangerous goodsfrom S$349.90Min. 32 days
- NIPPEI KIKI Spot ace cutter replacement bladeSize 19(H)x12(W) Material Cobalt high speed SKH55-CO Classification of the Hazardous Non-dangerous goods
- Isco Spot cutter ceramic coatingHigh-strength steel plate automobile body, etc.Color Black violet Classification of the Hazardous Non-dangerous goodsfrom S$139.90Min. 4 days
- BIC TOOL GEKKOUKINTARO (Spot Weld Drill / Cutter)Astonishing sharpness and durability of moonlight technology. Spot cutter Polishing machine Loken S-2000 (No. 1 sharpening only) Re-polishing is possible. Like Kintaro-ame, it maintains new performance even after re-polishing.Drill Diameter (Φmm) 8.2 Overall Length (mm) 80 Shank Diameter (Φmm) 9 Classification of the Hazardous Non-dangerous goodsfrom S$159.90Min. 2 days
- RUKO TIALN Coat Spot DrillClassification of the Hazardous Non-dangerous goodsfrom S$47.99Min. 6 days
- RUKO Carbide spot drillCarbide drill born in Germany. For high-strength steel, ALTIN has a longer life of about 20% to 30% than TILAN coated steel. Heat resistance of 900 degrees. Due to automatic sensor hole processing, it does not come off the spot. * Please use at a rotation speed of 800 rpm or more. * If the carbid... Read MoreCoating AlTiN Base Material Carbide Classification of the Hazardous Non-dangerous goodsfrom S$149.90Min. 4 days
- Isco Elbe spot cutter, non-coatedAutomobile body, general steelDimension (mm) 8.2×80 Color Black Material Heiss Classification of the Hazardous Non-dangerous goodsfrom S$159.90Min. 4 days
- SHINANO Spot cutterThe speed can be adjusted according to the hardness of the steel plate.Air Consumption (m3/min) 0.37 Mass (kg) 0.82 Drilling Thickness (mm) 10 Rotation Speed at No Load (min-1[rpm]) 1100~2000 Overall Length (mm) 176 Compressor (kW) 2.2 Vibration 3-axis composite value (m / s 2 ) 3.9/0.8 Suitable Hose Inner Dia. (Φmm) 6.5 Noise Level (dB(A)) 80/(91) Classification of the Hazardous Non-dangerous goodsfrom S$399.90Min. 7 days
- NIPPEI KIKI Spot ace cutterCobalt cutter for air drills or speed change drills High-speed tool steel (highest grade cobalt high-speed steel SKH55-CO) is used, and titanium coating surface treatment is applied to improve durability and sharpness performance. In addition, the center punch is not required, and the lower plate... Read MoreSet Contents 1 spot cutter, 4 replacement blades Material Cobalt high speed SKH55-CO Classification of the Hazardous Non-dangerous goods
- RUKO Spot drillMass (g) 30 Flute Length (mm) 38 Trusco Part No. 766-0111 Blade Diameter (Φmm) 8 Shank Diameter (Φmm) 8 Overall Length (mm) 80 Classification of the Hazardous Non-dangerous goodsfrom S$47.99Min. 3 days
- RUKO Spot cutter (carbide)Flute Length (mm) 12 Material Carbide (tungsten carbide) Classification of the Hazardous Non-dangerous goods Surface Treatment Titanium aluminum coatingfrom S$139.90Min. 3 days
- BIC TOOL Dream spot cutterThe world's first astonishing fastest spot cutter. It is a new shape tool. The shape of the cutting edge is different from the conventional product. Since it cuts lightly, no pushing force is required. The number of continuous holes is 3 to 4 times more stable than before. The center is stabl... Read MoreCutting Tip Diameter (Φmm) 8.2 Overall Length (mm) 80 Shank Diameter (Φmm) 9.0 Classification of the Hazardous Non-dangerous goodsDiscontinued
- BIC TOOL Spot cutter polishing machineLow cost type. Do not use until ultra-high tension. Recommended for those who use it less frequently.Included Accessories (Holder pipe) Φ8.0, Φ8.2 Outer Dimensions, Width W x Depth D x Height H (mm) 235×110×150 Power Input (V) AC100(50/60Hz) Suitable Whetstone CBN#170 Classification of the Hazardous Non-dangerous goodsDiscontinued
- Ishihashi Seiko Spot cutterHigh-speed drilling is possible with drastic reduction of runout. It is an essential item for automobile sheet metal. Dedicated drill for spot welding removal.Flute Length (mm) 24 Overall Length (mm) 80Discontinued
- Ishihashi Seiko TIN spot cutterHigh-speed drilling is possible with drastic reduction of runout. It is an essential item for automobile sheet metal. Durability has improved compared to non-coated products. Dedicated drill for spot welding removal.Flute Length (mm) 24 Overall Length (mm) 80Discontinued
- Ishihashi Seiko IS TA spot cutterHigh-speed drilling is possible with drastic reduction of runout. It is an essential item for automobile sheet metal. It can also cut ultra-high-strength steel sheets. Dedicated drill for spot welding removal.Flute Length (mm) 24 Overall Length (mm) 80Discontinued
- BIC TOOL Drill jointThe Drill Joint DJ-100 is a tool that allows you to extend your spot cutter or drill. "Spot peeling" and "drilling" of places where workability has been poor will be much faster. There are two types of joints, 150 mm and 200 mm. You can also connect the two. By replacing the s... Read MoreClassification of the Hazardous Non-dangerous goodsDiscontinued
- BIC TOOL GEKKOU (spot cutter)A new grooving tool that opens up the possibility of grooving to the forefront of global competition. Excellent biting property, excellent durability with 8% cobalt that cuts lightly with astonishing sharpness without blurring. Re-grindable (no thinning required) * Please use a super cutter for 7... Read MoreClassification of the Hazardous Non-dangerous goodsDiscontinued
- KOTO Spot drill setA dedicated drill set developed exclusively for high-strength steel sheets. A dedicated low-speed air drill for maximizing the coating drill.Material / Finish Iron / paint, plating Classification of the Hazardous Non-dangerous goodsDiscontinued