Car Wash Supplies
Use car wash tools according to the application, such as sponges and brushes for body car wash, and microfiber towels for wiping water after car wash. Some types of car wash sponges have a handle, so you can wash your car without getting your hands dirty. If you use a brush with horse hair that is soft and firm against dirt such as bumpers, you can also remove fine dirt. Tires are particularly susceptible to dirt and foreign objects, so clean them with a tire brush.
Other Related Pages
- MonotaRO Sponge compression type for car washA sponge that foams well in car shampoo, is soft to the touch, and is gentle on the car body. The package is compressed, but when the package is removed, it swells into a sponge with a thickness of about 50 mm. With hook holes for convenient storage. For vehicle washing and cleaning work. * Do no... Read MoreMaterial Polyurethane foam Color yellow Suitable Usage Car wash
- SCOTT PRO Shop Towels Heavy DutyCan be widely used both dry and wet. The texture when wet with water or chemicals is the feel of a cloth. With excellent absorption performance, it quickly absorbs liquids and oils. A versatile non-woven wiper that does not fluff easily Wiping off oil stains on machines, parts and toolsSpecification Roll type 60 cut Material Pulp, polypropylene non-woven fabric Classification of the Hazardous Non-dangerous goods RoHS directive (corresponding to 10 substances) Correspondence
- MonotaRO Microfiber Towel for Car WashA microfiber cloth for car washing. Soft and thick pile type. Ultra-fine fibers can be used to wipe off water droplets and remaining dirt without damaging it. For wiping the body and glass with water and wiping wax * If you use the product with foreign matter on it, the surface may be damaged. * ... Read MoreMaterial Microfiber
- MonotaRO Microfiber towelIt has good water absorption and is ideal for wiping off water droplets after washing the car. The remaining dirt is also scraped off with ultrafine fibers. It is gentle on the car body and is ideal for wiping off wax. For wiping the body and glass with water and wiping wax * Do not use chlorine ... Read MoreMaterial Microfiber
- MonotaRO Sponge car wash three packA set of 3 sponges for car wash is a great deal. A sponge that foams well in car shampoo, is soft to the touch, and is gentle on the car body. For vehicle washing and cleaning work. * Do not use for any other purpose.Material Polyurethane Classification of the Hazardous Non-dangerous goods Suitable Usage Car wash
- MonotaRO Sponge wax For solid half-slipA wax sponge for automobile bodies that is compatible with solid and semi-neri. A 3-pack that is convenient for replacement and usage. Wax car wash of car body * Never use the car body for anything other than waxing. Sand and dust adhering to the sponge or body may damage the car body, so be sure... Read MoreSuitable for Solid wax, semi-nerix wax Material Polyurethane Suitable Usage Wax car wash
- MonotaRO Microfiber glove for car washSince it is a glove type, it can be used even in places where it is difficult to wash with a sponge, and you can easily work according to the body line of the car. Removes dirt strongly with microfiber fiber. It is also convenient for wiping off wax. When washing the car. * Sand and dust adhering... Read MoreMaterial 80% polyester, 20% polamide
- WAKO Spa Plus Tire wax spongeNo unpainted corners of the tire. A patterned type that does not get tired and can be waxed without getting your hands dirty. Economical with a replacement head. For waxing tires. It is arched and can be applied firmly to the edges.Mass (g) About 134 Type Body Material (Handle) ABS・PP Material (Head) PE・PU Classification of the Hazardous Non-dangerous goods Suitable Usage Tire wax
- SOFT99 Corporation Compound sponge 2PA special sponge that can be polished evenly by hand and has a beautiful glossy surface comparable to a professional buff finish. Uses density urethane foam for easy work. I'm glad that 2 pieces can be used properly depending on the roughness of the compound.Material Polyethylene / Polyurethane Mass (g) 15 Classification of the Hazardous Non-dangerous goods Suitable Usage Compound polishing
- MonotaRO Microfiber cloth for glossy finishUltra-fine particle fibers with suede texture remove dust and oil stains cleanly. It also has excellent water absorption, so it can also be used to wipe off water after washing the car. For glossy finish * Do not use chlorine bleach as it will damage the fibers. *Using the product with foreign ma... Read MoreMaterial Microfiber
- MonotaRO Drainer Silicon WiperFor draining work after washing the car. It will be easier to wipe the towel. The tip of the blade is T-shaped. As it is a bar type, it is easy to use and convenient to hold in various places. * Sand and dust adhering to this product or the body may damage the car body, so be sure to remove the a... Read MoreMaterial Body (PP) / Blade (silicon) Mass (g) 200 Type Blade T shape
- MonotaRO Paper waste high absorption industrial box typeA paper waste with excellent water absorption and oil absorption. It uses a material that does not tear easily even when it gets wet, and can be squeezed even when it gets wet. It can be used to wipe off oil stains and water on machines and tools. A box type that is easy to store. For maintenance... Read MoreSpecification Box type, 500 cut Material Pulp Color White Classification of the Hazardous Non-dangerous goods
- Prostaff Wheel Demon Junior"Junior" with a pattern is born in the popular "Onijinte" series! Since it is a patterned type, you can easily wash the wheels without getting your hands dirty. Twisted microfiber entangles stubborn dirt and brake dust, and the mountain-shaped sponge shape inside firmly remove... Read MoreMaterial Microfiber Mass (g) 39 Classification of the Hazardous Non-dangerous goods Suitable Usage Wheel cleaning
- MonotaRO Passage car wash brush + packingA water-flow type car wash brush that can be fitted with a hose (inner diameter 15 mm). A hard-to-use car wash brush that uses natural fiber packing with hard hair and strong elasticity. Cleaning of farm equipment, trucks, bodies, undercarriage, undercarriage, and mats. * Do not use on fragile it... Read MoreMaterial Pattern: PE, Brush: Pakin Color Pattern: Black, Brush: Yellow Classification of the Hazardous Non-dangerous goods Suitable Usage Car wash
- Prostaff Easy bucketIt is a bucket that can be used for riding, which is convenient for washing ordinary cars to high-roof cars. A large capacity type of 10L, which is very useful for hand washing and shampoo car washing. It can also be used as a storage box, so car wash supplies can be organized compactly.Mass (g) 716 Capacity (L) 10 Classification of the Hazardous Non-dangerous goods
- Amon Industry 2WAY brushYou can use it properly according to the dirt and location with a soft and hard brush. For removing gaps such as emblems, dirt on wheels, and clogging of wax.Material PP Mass (g) 84 Type 2WAY type Classification of the Hazardous Non-dangerous goods Suitable Usage Tire and wheel cleaning
- WAKO Spa Plus Car Wash Brush PackingStrongly scrapes off dirt. For tires and trucks. For cleaning tires, trucks, farm equipment, etc. of cars and motorcyclesMass (g) About 163 Type Patterned type Material (Handle) Polyethylene Material (Bristle) Mexican fiber Classification of the Hazardous Non-dangerous goods Suitable Usage Car wash
- SOFT99 Corporation Fukupica 4.0With a new formulation that is gentle on the coating film, it can now be used on professional-coated vehicles. * When used for hydrophilic coating, it becomes water repellent temporarily. It embraces dirt inside the 3-layer hybrid sea and prevents scratches due to dragging. With low friction proc... Read MoreMass (g) 315 Classification of the Hazardous Non-dangerous goods
- AION Super absorbent chamA super-water-absorbing chamois for coated vehicles that greatly reduces wiping resistance and is gentle on the coating film. The fine continuous pores quickly absorb water droplets, and the drainage is good, so the water absorption capacity is restored by the amount of squeezing. Repeated wiping... Read MoreMass (g) 185 Classification of the Hazardous Non-dangerous goods
- SOFT99 Corporation Water Absorption Super ClothThe ultra-fine fibers that make up the cloth have a triangular cross-sectional shape, creating innumerable gaps in the cloth and demonstrating incredible water absorption, greatly shortening the wiping time after car washing. Ultra-fine fibers also have a scraping effect, so even light stains can... Read MoreClassification of the Hazardous Non-dangerous goods
- SOFT99 Corporation God Training Wheel BrushA brush-shaped brush that can clean the gaps between nut holes and valve holes. Soft resin ring prevents scratches. For wheel cleaningClassification of the Hazardous Non-dangerous goods
- Chubu High-Pressure Hose 3/8 size high pressure washer hose (1005 + with nipple)Compared to conventional products, the outer layer rubber of the hose contains a wear-resistant polymer, which makes it slippery and easier to work with. You can now select the metal fittings on both ends of the hose + nipple + spring from the conventional iron or stainless steel. It is generally... Read MoreRegular Pressure (MPa) 23 Hose Inner Diameter (Φmm) 9.5 Minimum Burst Pressure (MPa) 70 Reinforcing Layer With wire blade Hose Outer Diameter (Φmm) 15.6 Classification of the Hazardous Non-dangerous goods
- WILLSON Double water absorption chamoisSmooth draining! The new material, micro nylon fiber, absorbs water droplets remaining on the body glass with twice the force (compared to our company) compared to conventional chamois. Achieves smooth draining in a big size, making it ideal for RVs.Material Micro nylon fiber Classification of the Hazardous Non-dangerous goods
- JET INOUE Long car wash brush headIt reaches every corner even in high places! It is very convenient for washing buses and trucks! The brush tip is processed to prevent scratches! Cleaning and careSuitable for 593402 Material Brush part: PP, Resin part: PE Type Brush head Classification of the Hazardous Non-dangerous goods Suitable Usage Car wash
- SOFT99 Corporation Clean WiperLonger reach! Draining wiper for cars. Safe design that does not damage the car. It's very good after car wash and rain.Material Natural rubber, PP, ABS Color Black Mass (g) 400 Classification of the Hazardous Non-dangerous goods
- SOFT99 Corporation Premium water absorption clothA high-density cloth with a basis weight of 360 g / m 2. Demonstrates amazing water absorption with abundant fiber content! * Metsuke amount / 1m 2 fabric weight. The heavier the fiber, the greater the amount of fiber and the thicker it is. (-General microfiber cloth is 260-310g / m 2 ) With thic... Read MoreMass (g) 66 Classification of the Hazardous Non-dangerous goods
- MonotaRO Car wash sponge + rotating typeWhen you press the black button on the head, the sponge rotates so you can wash it vertically and horizontally. It is also ideal for hard-to-reach places. For car washing in hard-to-reach places * Please use it after wetting it with water. * It is even more effective when used in combination with... Read MoreClassification of the Hazardous Non-dangerous goods Suitable Usage Car wash
- WAKO Foil spongeThe long-haired bore takes in dirt and removes fine dirt firmly! Smooth washing like a mouton! Since the sponge in the center is thin, the gaps and details of the wheel can be washed cleanly. Since it uses a fluffy boa fabric, the painted surface of the wheel is not easily scratched and can be wa... Read MoreMass (g) 57 Classification of the Hazardous Non-dangerous goods Suitable Usage Wheel cleaning
- Maru-T Tohoku Ishibashi Shinano DX + IM-10 + 95011Car wash / cleaning brush A water-flowing type that makes it easy to mix hair, which is ideal for hard stains! For water-permeable tires and agricultural equipment such as sticky mud stains and tractors in tire houses * This product does not guarantee that all models and painted surfaces will not... Read MoreMass (g) 215 Bristle Mixed hair (PET, Pakin, Palm) Material (Handle) Polyethylene Classification of the Hazardous Non-dangerous goods
- Prostaff Glove for wheels Onito 2WAYA microfiber glove exclusively for wheels that thoroughly pursues the ease of washing the wheel. Further evolved from the popular conventional product (P124)! The shape of the five fingers remains the same, but the materials on both sides have been changed to make it even easier to use. The "... Read MoreMass (g) 62 Classification of the Hazardous Non-dangerous goods
- SurLuster Washing gloveSoft natural wool that is kind to your car! A creamy, foaming glove type for speedy car washing.Material wool Classification of the Hazardous Non-dangerous goods Suitable Usage Car wash
- Prostaff Kakikure Shine MaruA versatile electric handy polisher that can be used simply by setting the battery. As it is a compact type that does not require cordless and charging, it can be used quickly and easily not only for automobiles, but also for motorcycles, tombstones, washbasins and sinks at home. A set of accesso... Read MoreMaterial Microfiber Mass (g) 393 Classification of the Hazardous Non-dangerous goods
- SOFT99 Corporation Mouton MasterThe moderate elasticity and density of the selected wool creates fine, high-quality foam that gently cleanses the body. A new type of car wash mitt that is glove-shaped with a split tip and is easy to wash in small parts and every corner. For coated vehiclesMaterial Australian natural shearling, polyester Mass (g) 80 Classification of the Hazardous Non-dangerous goods Suitable Usage Car wash of coating construction car
- WAKO Drainer wiper fixed typeUses high quality rubber made in Japan. A convenient item that can drop water drops after washing the car at once.Classification of the Hazardous Non-dangerous goods
- SOFT99 Corporation Micro ChamoisUses 0.05 denier class ultra-fine fiber non-woven fabric. The surface is brushed and the skin is specially urethane-treated, so it has a feel close to that of genuine leather and has amazing water absorption. It doesn't harden even when it dries, so it's very convenient because you don... Read MoreMass (g) 45 Classification of the Hazardous Non-dangerous goods
- JTC A / C system simple washing machine* Please use the separately sold JTC1409B. * This product is a simple cleaning type. For cleaning individual parts of the vehicle's air conditioner system, hoses, etc. * Cannot be used for expansion valves, receivers, and capacitors with integrated receivers.Capacity (L) 1 Classification of the Hazardous Non-dangerous goods RoHS directive (corresponding to 10 substances) Correspondence
- SOFT99 Corporation God Training Wheel SpongeThe synergistic effect of the uneven shape and ultra-fine fibers removes persistent stains on the wheel! The delta shape head and high elasticity urethane sponge can be used to clean various wheel shapes. For wheel cleaningClassification of the Hazardous Non-dangerous goods
- Prostaff Demon hand + back handClean to the back of the wheel! A fiber sponge with a handle for wheels that reaches the dirt in the back. The long handle with a total length of about 325 mm penetrates deep into the wheel and removes dirt. The "microfiber twisted surface" that cleanly removes oil stains and brake dust... Read MoreClassification of the Hazardous Non-dangerous goods Suitable Usage Wheel cleaning
- SOFT99 Corporation Ex sweepSpecially processed body-friendly carefully selected materials! Uses polyester filaments that are extremely soft and less likely to get caught due to fluffing. After twisting the fibers, the tips of the hair are loosened appropriately, and the effect of the exquisitely opened hair tips catches di... Read MoreClassification of the Hazardous Non-dangerous goods
- AION Multi cloth plus for coating construction vehiclesIdeal for everyday care of coated vehicles. It can be used for multiple purposes such as wiping with water, wiping with dry cloth, applying coating agent, and wiping with finish. For washing cars with water. For wiping off water droplets.Material Material: Polyamide Mass (g) 50 Classification of the Hazardous Non-dangerous goods
Filter by categories