A full release stop mechanism is adopted. The length of the woven rope can be arbitrarily adjusted, and a simple winder is used. Can be used in workplaces with a height of 6.75m or less.
Mass (g) About 1190 Type Rewind type Buckle Pass through Hook FS-90 Lanyard, Strap Width (mm) 15 Lanyard, Length (mm) 1500 Type of Shock Absorber First kind Lanyard 1 hook
Mass (g) About 1305 Type Rewind type Method Woven rope Buckle Pass through Hook FS-99, shock absorber Lanyard, Length (mm) 1400 Type of Shock Absorber First kind lanyard width (mm) 15 Lanyard 1 hook
Economy type with both ease of use and safety. Can be used in workplaces with a height of 6.75m or less.
Color Blue Size M Mass (g) About 900 Type Rope type Buckle Pass through Hook FS-99 Lanyard, Diameter (mm) 10 Lanyard, Length (mm) 1500 Type of Shock Absorber First kind Lanyard 1 hook
February 2019 enforced "standard for fall prevention equipment" compliant product. A constant take-up reel type fall arrest device that pursues ease of use and economy. Since the rope is stored automatically, the rope does not get tangled during work, and work can be done smoothly.
For ... Read More
Type Rewind type Belt Color Navy Function (Emergency lock) None Buckle Pass through Hook Standard (1 lock 51S hook) Lanyard, Length (mm) 1600 Type of Shock Absorber First kind Lanyard 1 hook
Mass (g) About 1275 Type Rewind type Method Woven rope Belt Color Blue Buckle Pass through Hook FS-99, shock absorber Lanyard, Length (mm) 1400 Type of Shock Absorber First kind lanyard width (mm) 15 Lanyard 1 hook
An economy type with a large diameter hook that is both easy to use and safe. Comes with a hook hanger to hang when not using the hook.
Size M Mass (g) About 895 Type Rope type Method Eight beats Belt Color Blue Buckle Pass through Hook FS-99, with shock absorber Lanyard, Diameter (mm) 10 Lanyard, Length (mm) 1500 Type of Shock Absorber First kind Lanyard 1 hook
Lightweight model with a one-touch buckle that is easy to put on and take off.
Mass (g) About 1290 Type Rewind type Method Woven rope Buckle One touch Hook FS-93 (lightweight), shock absorber Lanyard, Length (mm) 1400 Type of Shock Absorber First kind lanyard width (mm) 15 Lanyard 1 hook
The definitive rope-type and lightweight safety belt! It can be used in workplaces with a height of 6.75 m or less.
Mass (g) About 895 Type Rope type Buckle Pass through Hook FS-93 (light weight) Lanyard, Diameter (mm) 11 Lanyard, Length (mm) 1700 Type of Shock Absorber First kind Lanyard 1 hook
With a one-touch buckle that is easy to put on and take off. Insert the insertion plate into the main body and make a clicking sound to complete the installation. It has a double safety structure in which the upper and lower release levers cannot be pushed unless the insertion plate is pushed in ... Read More
Mass (g) About 1385 Type Rewind type Method Woven rope Buckle One touch Hook FS-93, shock absorber Lanyard, Length (mm) 1400 Type of Shock Absorber First kind lanyard width (mm) 15 Lanyard 1 hook
Equipped with the industry's first one-hand (one hand operation) mechanism. This is the industry's first winder that can be operated with one hand from unwinding to storing the woven tape. The woven tape can be wound automatically by simply pulling it out a little. Can be used in workplac... Read More
Color Black Size L Mass (g) About 1150 Type Rewind type Buckle Pass through Hook FS-93 (light weight) Lanyard, Strap Width (mm) 15 Lanyard, Length (mm) 1450 Lock mechanism Lock type Type of Shock Absorber First kind Lanyard 1 hook
Mass (g) About 1355 Type Rewind type Method Woven rope Buckle One touch Hook FS-99, shock absorber Lanyard, Length (mm) 1400 Type of Shock Absorber First kind lanyard width (mm) 15 Lanyard 1 hook
Bestseller with large diameter hook. The hook is directly hooked on the single pipe to improve work efficiency.
Mass (g) About 1040 Type Rope type Method Three strokes Buckle Pass through Hook FS-90 with shock absorber Lanyard, Diameter (mm) 11 Lanyard, Length (mm) 1600 Type of Shock Absorber First kind Lanyard 1 hook
With a one-touch buckle that is easy to put on and take off. Insert the insertion plate into the main body and make a clicking sound to complete the installation. It has a double safety structure in which the upper and lower release levers cannot be pushed unless the insertion plate is pushed in ... Read More
Mass (g) About 1320 Method Woven rope Buckle One touch Hook FS-93 (lightweight), shock absorber Lanyard, Length (mm) 1400 lanyard width (mm) 15
Mass (g) About 1025 Type Telescopic Method Telescopic strap Buckle Pass through Hook FS-99, with shock absorber Type of Shock Absorber First kind lanyard width (mm) 32 Lanyard 1 hook
A lightweight rope-type safety belt that uses aluminum alloy for the buckle and hook.
Size M Mass (g) About 870 Type Rope type Method Eight beats Belt Color Yellow Buckle Pass through Hook FS-93 (lightweight) with shock absorber Material (Catch) Aluminum Lanyard, Diameter (mm) 11 Lanyard, Length (mm) 1600 Type of Shock Absorber First kind Lanyard 1 hook
With a retractable strap, the strap is automatically wound up when working or carrying, and it is a standard for fall arrest equipment that does not get in the way. New standard torso belt type fall arrest equipment.・The 2-way switching lock mechanism with fixed length locks the strap in the sho... Read More
Mass (g) About 1120 Type Rewind type Belt Color Black Buckle Pass through Lanyard, Length (mm) About 1650 Lock mechanism Lock type Type of Shock Absorber Grade 1 Lanyard 1 hook
A 2-way low-wrap red fluorescent reflective sticker allows you to confirm safety from a distance. A lock device with a two-stage switch for free and gear mechanisms.
Mass (g) About 1200 Type Rewind type Belt Color Black Buckle Pass through Lanyard, Strap Width (mm) 17 Lanyard, Length (mm) 1650 Material (Waist Belt) Nylon Lanyard (Strap) Aramid fiber RoHS directive (corresponding to 10 substances) Correspondence Lock mechanism Lock type Type of Shock Absorber First kind Lanyard 1 hook
It is a body belt type fall prevention device with an auxiliary band. Auxiliary band: With reflective tape. Body belt: One-touch buckle. Lanyard: Sword Aluminum hook Free ring "Bellows" are used.
High-altitude workers with a work floor of 2 m or more and a work floor of 6.75 m or less.
Type Telescopic Buckle One touch Type of Shock Absorber First kind Lanyard 1 hook
The lanyard can be fixed to the required length and can be stored by pulling it a little when winding. With a lock mechanism, it will stop at a short fall distance when it crashes. New standard compliant product. First-class shock absorber.
Color Black Mass (g) 1290 Type Rewind type Buckle Pass through Material (Catch) Aluminum Lanyard, Length (mm) 1450 Lock mechanism Lock type lanyard width (mm) 15
The lanyard can be adjusted to the required length, and the locking mechanism stops it with a short fall distance even in the event of a crash. The auxiliary rope is always retractable. New standard compliant product. 2 hooks.
Color Black Mass (g) 1930 Type Rewind type Material (Catch) Aluminum Lanyard, Length (mm) 1450 Material (Adjusting Buckle) Aluminum Lock mechanism Lock type lanyard width (mm) 15
It is a body belt type fall prevention device. Comes with a first-class shock absorber. A lightweight rope-type safety belt that uses aluminum alloy for the buckle and hook. It is a lightweight type.
Please use it when the drop height does not allow the full harness to be used.
* For those with e... Read More
Size M Type Rope type Type of Shock Absorber Grade 1 Lanyard 1 hook
Vertical reel type set that does not disturb the waist area
New standard compatible body belt type lanyard combination set
* Fall prevention equipment (safety belt) and fall prevention equipment (safety belt) related equipment are consumables, and their performance will deteriorate due to wear du... Read More
You can fix the length and wind it up with the touch of a button, or you can use it to expand and contract like a seat belt. It has a built-in lock mechanism that stops at the shortest drop distance.
Color Black Mass (g) 1100 Type Rewind type Buckle Pass through Lanyard, Length (mm) 1400 Lock mechanism Lock type Type of Shock Absorber Grade 1 Lanyard 1 hook
Double lanyard set with auxiliary rope
New standard compliant SEG waist belt lanyard and auxiliary rope set
* Fall prevention equipment (safety belt) and fall prevention equipment (safety belt) related equipment are consumables, and their performance will deteriorate due to wear during use, so re... Read More
Size M Mass (g) 1810 Type Retractable / telescopic Belt Color Black Buckle Pass through Type of Shock Absorber Grade 1 Lanyard 2 hooks
Size M Mass (g) About 1285 Type Rope type Belt Color Blue Buckle One-touch buckle Lanyard, Effective Length (mm) 1400 lanyard width (mm) Woven rope: 15
A small and lightweight waist belt lanyard set that can be easily removed when not in use. Aluminum detachable carabiner for easy removal. Super small reel. No winding or locking device. Detachable space width 4 cm. It does not take up space around your waist. A free/auto stop switching mechanism... Read More
Size L Mass (g) 620 (lanyard only) Type Torso belt type Belt Color Black Lock mechanism None Type of Shock Absorber Grade 1 (4kN) Lanyard 1-chome
It is a body belt type fall prevention device. Comes with a first-class shock absorber. With Noviron lanyard specifications, it is shrunk with natural rubber and does not easily get caught in structures when moving. It is a lightweight type.
Please use it at a drop height where the full harness c... Read More
Small space vertical lanyard and body belt set
New standard compliant SEG body belt lanyard set
* Fall prevention equipment (safety belt) and fall prevention equipment (safety belt) related equipment are consumables, and their performance will deteriorate due to wear during use, so replace them a... Read More
Type Telescopic Belt Color Black Buckle Pass through Type of Shock Absorber Grade 1 Lanyard 1 hook
Prevents falling accidents by eliminating the state of no torso when changing hooks. When changing the hook of the lanyard when moving for work at height, the hook of the auxiliary rope can be hooked to the structure in advance so that the body is in a no-body state (*The hook is not locked, and ... Read More
Specification With shock absorber Size M Mass (g) about 1930 Type Rewind type Buckle Aluminum buckle Hook FS-93 Lanyard, Strap Width (mm) 15 Lanyard, Length (mm) 1400 RoHS directive (corresponding to 10 substances) Correspondence Lanyard Two-sided rack
You can fix the length and wind it up with the touch of a button, or you can use it to expand and contract like a seat belt. It has a built-in lock mechanism that stops at the shortest drop distance.
Mass (g) 1200 Type Rewind type Buckle Pass through Lanyard, Length (mm) 1400 Lock mechanism Lock type Type of Shock Absorber Grade 1 Lanyard 1 hook
With a large hook, it can be used at any construction site. A plain weave belt with a waist is used. A safety belt for general work.
Mass (g) 750 Type Rope type Buckle Pass through Lanyard, Diameter (mm) 10 Lanyard, Length (mm) 1500 (including hook) three-strike rope Type of Shock Absorber Grade 1 Lanyard 1 hook