A belt clip type cutter insert that can be easily attached and detached. Because it is a clip type, it sticks to the waist and does not hang around. With water repellent finish and reflective line tape.
Tough design comfort and security! Lightweight and durable! 1680 denier fabric with ballistic processing that is resistant to friction is used for the surface fabric. It does not easily lose its shape and is easy to use.
A holster with a lock that does not come off due to violent movement One-touch release with your thumb. 45 degree rotation holster (3 step adjustment) that allows you to select your own angle to pull out smoothly Connected to the cutter with a plastic safety rope mounting ring that is resistant t... Read More
A cutter knife is stored in the center, and small cutter knives and felt-tip pens are stored on both sides. Even if you forget to store the cutter blade, it has a durable resin bottom guard (* Normally, the blade is stored in the instrument body. Please use) Made of light and durable polyester ca... Read More
Material Polyester canvas Color Body / black, line / yellow Mass (g) 50
Tough design comfort and security! Lightweight and durable! 1680 denier fabric with ballistic processing that is resistant to friction is used for the surface fabric. It does not easily lose its shape and is easy to use.
The surface is made of thick nylon with a water-repellent finish. With a reflective function line that is convenient for night work. L-shaped cutters, pens, and seals can be stored on the side.
Non-slip function! Since rubber is attached to both sides, it is hard to slip even if you put it in with the stopper of the mini cutter removed! It can be widely used for construction, civil engineering, aerial work, etc. Since it moves back and forth, it does not get in the way even with cancer.... Read More
Mass (g) 220 RoHS directive (corresponding to 10 substances) Correspondence
The surface is made of thick nylon with a water-repellent finish. With a reflective function line that is convenient for night work. In addition to the cutter, it can store small work items such as scissors and pens.
Uses high-density 2520 denier 100% nylon that is resistant to abrasion and nail penetration. Excellent visibility with reflective tape. There is no warp on the edge of the pocket and it does not hurt your fingers. Durable 5-layer fabric. Two-stage storage of snips and booster scissors. Metal rein... Read More
Material 100% nylon (2520 denier) Color Black Mass (g) 252
For storing the cutter For storing in the commercially available cutter L For storing small items, etc. Cutter difference suitable for electrical work and light sky work Cutter difference with excellent workability The material is light and the material is soft to reduce the burden on the waist. ... Read More
Genuine leather products become even more glossy after long-term use. The cases are familiar with the shape of tools and can be used for a long time. It has excellent durability and wear resistance, and can be used hard.
For storing cutters, etc.
Material Cow tanned leather Shape Pliers, cutter 2 steps Mass (g) 80 2018 Trusco page 4 2260
The birth of true "black" that is particular about black!
* Please note that there may be slight differences in color pattern, shape and size due to the use of natural materials and handmade items.
You can insert a cutter knife and convex, which are frequently used in the field, at the same time! A lightweight resin body that does not easily lose its shape! One-touch plate that does not come off easily! Two cutter knives and convex can be inserted!
* Some products may not fit or may be loos... Read More
The commitment of craftsmen who are familiar enough to use it for all craftsmen who are particular about leather!
* Please note that there may be slight differences in color pattern, shape and size due to the use of natural materials and handmade items.
Non-slip function! Since rubber is attached to both sides, it is hard to slip even if you put it in with the stopper of the mini cutter removed! It can be widely used for construction, civil engineering, aerial work, etc. Since it moves back and forth, it does not get in the way even with cancer.... Read More
Mass (g) 180 RoHS directive (corresponding to 10 substances) Correspondence
The cases are familiar with the shape of tools and can be used for a long time. It has excellent durability and wear resistance, and can be used hard.
For storing sheet metal scissors.
Specification With eyelet holes Material Black floor leather Shape 2nd grade Color Black Mass (g) 230 2018 Trusco page 4 2261
Genuine leather products become even more glossy after long-term use. The cases are familiar with the shape of tools and can be used for a long time. It has excellent durability and wear resistance, and can be used hard.
For storing Rasha cutting shears 240mm, 270mm, lottery, and magic.
Material Cow tanned leather Shape Rasha iron, cutter case Mass (g) 110 2018 Trusco page 4 2260