Nail & Bolt Bags
A nail / bolt bag is a type of bag that is lowered from the waist to store nails and bolts that are used when working at construction sites. The nail bag is made of sturdy denier fabric or leather, and is a convenient item for safely carrying pointed nails. Some of them are equipped with pockets, tool holders, etc., and can store tools such as hammers, so you can organize your work tools neatly. Most of the nail bags are attached to the belt part, but it is recommended to purchase after confirming because the applicable belt width varies depending on the product.
Other Related Pages
- MonotaRO Screw cupA convenient cup that can store and carry screws. Since it has a carabiner, it can be hooked on a belt loop, and since it also has a belt loop, it can be used by passing it directly through the belt. As a portable storage for screws and nails * Do not use for any other purpose. * Please store wit... Read MoreIncluded Accessories Carabiner Color Black
- DBLTACT Genuine Leather Nail and Tool BagGenuine leather nail bag! A model for higher-grade craftsmen!
- DBLTACT Nail bagEmphasis is placed on ease of use with a large number of pockets. A large nail bag with a large capacity. It does not lose its shape and is easy to use.
- Tajima (TJM DESIGN) Detachable waist bag 3 steps of nail bagDetachable waist bag for construction work sitesMass (g) 560
- PROSTAR KAWATEC Master beam tool nail bagMaterial Ratchet cutter, hammer holder: leather Material (Base Fabric) Surface: Kawatec Inner surface: Polydobi
- KOZUCHI Evolution temporary frame bagLight and durable. Evolution = a new type of nail bag that has evolved.Material fabric/polyester hardware/steel plating
- DBLTACT Nail bag1680 denier fabric with ballistic processing that is resistant to friction is used for the surface fabric. A nimble design that double-layers a tough outer cloth and a tough inner cloth.Material 1680 denier fabricfrom S$28.99Min. 2 days
- KIYO (KH) Evolution bag nail bagA novel design with the right side raised. The contents are hard to spill even if you lean forward. Easy to access like the side pockets of trousers. Uses a manufacturer's original reinforcement method that widens the opening. The U-shaped cut belt loop on the back makes it easy to wear even ... Read MoreMaterial 1680 denier nylon fabric
- DBLTACT Nail bag1680 denier fabric with ballistic processing that is resistant to friction is used for the surface fabric. It does not easily lose its shape and is easy to use.Material 1680 denier fabric Color Black
- Tajima (TJM DESIGN) Detachable waist bag Nail bag 2 steps smallDetachable waist bag for construction work sitesMass (g) 445from S$79.99Min. 2 days
- MEXES Nexus temporary frame bag with Sumitsubo case"A popular and convenient waist bag with a chalk line case. Comes with a case that can hold a sumi tsubo. It is a durable nail bag that is reinforced inside for carpenters and temporary frame shops. The material is polyester 1680 denier. "from S$58.99Min. 6 days
- KIYO (KH) SAKURA seriesCollaboration of camouflage pattern and colorful SAKURA color fabric 1680 denier tough nylon fabric. The patented pocket that does not easily come off the bottom is diagonally cut so that it is easy to take out and hard to fall off. Tool storage member storage * Supports 60 mm width through the b... Read MoreMaterial 1680 denier nylon
- PROSTAR KAWATEC temporary frame nail bag super sturdyLightweight and durable. Moreover, it can be washed with water and does not fade. The surface base fabric uses the new 21st century material "KAWATEC" created by the ultimate computer technology. The inner base fabric is made of "Polydby", an ultra-durable material that is res... Read More
- GISUKE (Takagi) Mini nail bagLightweight and compact. Excellent functionality.Material Artificial leatherfrom S$14.99Min. 5 days
- DBLTACT Cordless case1680 denier fabric with ballistic processing that is resistant to friction is used for the surface fabric. It does not easily lose its shape and is easy to use.Material 1680 denier fabric Color Black Function Bit insertion
- KIYO (KH) Strong Allin Nail Bag W TypeThe better the storage capacity of the nail bag, the more pleasing it will be. Equipped with two pockets on the front of the two-tiered body with wide gussets. On the left side, there is a new inkpot, and on the right side, there is a holder for a spirit level and small items. There are four pen ... Read MoreMaterial High density 1680 denier nylon fabric Color Black
- DBLTACT Nail bagNew high-class texture! Easy to use without losing its shape! A large suede-like special fabric is used for the large full-face pocket. A nimble design that double-layers a tough outer cloth and a tough inner cloth.Material Polyester suedefrom S$29.99Min. 3 days
- PROSTAR KAWATEC temporary frame nail bag super sturdy (with gusset)Lightweight and durable. Moreover, it can be washed with water and does not fade. The surface base fabric uses the new 21st century material "KAWATEC" created by the ultimate computer technology. The inner base fabric is made of "Polydby", an ultra-durable material that is res... Read MoreMaterial (Base Fabric) Surface: Kawatec Inner surface: Polydobifrom S$87.99Min. 6 days
- PROSTAR KAWATEC Nail bag with temporary frame gussetLightweight and durable. Moreover, it can be washed with water and does not fade. The surface base fabric uses the new 21st century material "KAWATEC" created by the ultimate computer technology. The inner base fabric is made of "Polydby", an ultra-durable material that is res... Read MoreMaterial Trim pocket: nylon dobby Material (Base Fabric) Surface: Kawatec Inner surface: Polydobi
- KIYO (KH) Evolution bag (for left waist) Nail bagLeft-up type with the opposite pocket cut. Recommended for those who work with a bag attached to the left waist. Since the safety belt is attached to the left side, the normal type is recommended for those who work at heights, but for those who are not so, those who attach the tool bag to the lef... Read MoreMaterial 1680 denier nylon fabric
- NEXUS Temporary frame nail bagStrong durability with inner reinforcement processing Large D-ring hook makes it easy to remove safety cords, etc. Inner storage pocket with inner bit storage pocketMaterial Complete leather
- ROUTE66 Route 66 BISU CUPROUTE66 brand biscup. Convenient for storing small parts such as screws and course threads! In addition to the carabiner, there is also a belt loop, so it can be attached to the belt. Storage of small items such as course threads and screws.Specification With carabiner Material Polyesterfrom S$12.99Min. 6 days
- NEXUS Nail bag smallOuter bit storage pocket Strong durability with inner reinforcement processing With a large D-ring hook, safety cord etc. can be easily removedMaterial Complete leatherfrom S$85.99Min. 6 days
- TRUSCO Floor nail bagThis product uses high quality leather. The shallow bottom makes it easy to take out nails.Material Cow floor skin
- PROSTAR Nail bag with gussetRigid DNA, ultra-rugged material, 1680 denier adopted. A storage case with excellent water repellency and waterproofness, using a foamed polyethylene sheet and a special PVC sheet on the back. It is reinforced with caulking with a cover in places that are easily torn when tools are taken in and o... Read Morefrom S$56.99Min. 6 days
- Sei Yokoduna Nail bag with gussetThe more you use it, the better it will become familiar.Material Cowhide split RoHS directive (corresponding to 10 substances) Correspondencefrom S$86.99Min. 4 days
- JEFCOM (DENSAN) Pocket belt (3 pockets)Large capacity for storing and carrying frequently used parts such as screws and nails (3 pockets) With a resin plate that does not easily lose its shape and has a mini buckle that allows you to open and close the zipper smoothly with one hand, it can be easily attached to a stepladder or ladder.Mass (g) 340from S$49.99Min. 3 days
- KIYO (KH) Strong Allin Nail Bag with Curve MeasureAs a bulky tool, there is a "steel square" as a must-have item that everyone needs. The 25 x 50 size steel square can be stored by inserting it outside. If it is 15 x 30 size, it can be stored in the back pocket. Can be stored in the back pocket. The back pocket has a structure that is ... Read MoreMaterial High density 1680 denier nylon fabric Color Blackfrom S$79.99Min. 6 days
- NEXUS Temporary Nail Bag W Pocket NinjaStrong durability with inner reinforcement processing With a large D-ring hook, it is easy to remove safety cords, etc. With inner bit storage pocket Inside storage pocket With curved scale storage pocketMaterial Complete leather Color Whitefrom S$109.90Min. 6 days
- NEXUS Temporary Nail Bag W Pocket Ninja TypeStrong durability with inner reinforcement processing With a large D-ring hook, it is easy to remove safety cords, etc. With inner bit storage pocket Inside storage pocket With curved scale storage pocketMaterial Complete leather Color Blackfrom S$109.90Min. 9 days
- BEST TOOL Gokutaku black canvas temporary frame nail bagThe maximum capacity of the two-stage storage space and the two subdivided pockets that can hold thick tools on the front are very convenient. Interior tools (rollers, convexes, spirit levels, brushes, etc.) and carpenters / building tools (convex) -Ideal for storing gems, spirit levels, folding ... Read MoreMaterial Cotton canvas Mass (g) 440 Finish Processing Strong water repellent finishfrom S$63.99Min. 5 days
- KIYO (KH) Strong Allin Nail Bag Type BUses strong allin fabric, which is a durable material woven with 4 twisted nylon threads at high density. The first gusset part is fixed with caulking studs on the reinforcement, and the front pocket part is fixed with double caulking studs. It is a gem that does not lose its shape and can be use... Read MoreMaterial Super high density 2200 × 2D MATTfrom S$63.99Min. 6 days
- Samurai BLACK With nail bag ink square differenceRoHS directive (corresponding to 10 substances) Correspondencefrom S$44.99Min. 4 days
- Fukuro Club Legend Choi NailsMaterial Genuine leather, micro leather Mass (g) 209from S$47.99Min. 3 days
- Samurai BLACK Canvas nail bagMade of canvas (lightweight) Second-stage pocket (loose gusset width) that can be used by dyeing the fabric twice to emphasize black Reinforced on the bottom, drained on the bottom 2 places Embroidered logo, belt loop width is compatible with Y-shaped harnessMaterial No. 4 canvas Color Black RoHS directive (corresponding to 10 substances) Correspondencefrom S$38.99Min. 4 days
- GISUKE (Takagi) Nail bagAnti-twist processing inside the belt loop.Material Cowhide leather + polyesterfrom S$34.99Min. 4 days