Abrasive Material
Abrasive materials refer to a variety of abrasive materials used for polishing operations. The classification can be broadly divided into abrasive grains, sand and paste, diamond, glass polishing, stone polishing, and blast machine abrasives. The abrasive grains, sand and paste are mixed with abrasives, oil, liquids, etc. there is. Choose the best product for each material and process. Pastes containing diamond abrasive grains are oil-soluble and water-soluble, and can be used depending on the object. Some products specialize in polishing glass and stone.
Other Related Pages
- Koyo-Sha NEW Sunlight (Polishing Compound)A slightly fragrant type that does not have an unpleasant odor (petroleum odor). Removes hard-to-remove stains (such as cigarettes) and small scratches, and restores a beautiful luster. The best cleaner for daily care. Apply an appropriate amount of this product to a soft cloth and rub it with yo... Read MoreRoHS directive (corresponding to 10 substances) Correspondence
- Koyo-Sha SisarFor rough polishing of hard metals such as iron and stainless steel. It has the sharpest sharpness and is ideal for removing scratches and polishing the base. For rough polishing of all metalsType Solid abrasive Color Pink Suitable Material Iron, stainless steel, etc. Process Rough polishing Applicable buff Sisal Buff RoHS directive (corresponding to 10 substances) Correspondence
- NAKANISHI (NSK) Diamond PowderA diamond micropowder with a uniform and accurate particle size distribution for precision finishing.from S$44.99Min. 2 days
- SOFT99 Corporation Rust EraserYou can remove stains with red rust and kogation just by rubbing. Simply rub any rust in your home to remove it. You can also remove persistent stains and oily magic. Detergent power is further improved when used with detergent or water. Remove red rust and kogation. * Do not use on works of art,... Read Morefrom S$6.69Min. 2 days
- MonotaRO Blue Polishing Compound 67gIt fits well in the buff and gives a gloss. For mirror finish of stainless steel * Do not use for anything other than its intended purpose.Specification For finishing Type Solid abrasive Mass (g) 67 Suitable Material Stainless steel
- MonotaRO Blast Abrasive A type (brown molten alumina)It is a brown molten alumina abrasive and is widely used in general. It can be used as a sandblast or general abrasive. Rust removal, paint peeling, carbon removal, base adjustment before painting * Do not use for any other purpose.Hardness New Morse: 12, Knoop: HK2020
- MonotaRO Polishing Compound White Bar 850GA solid oil-based abrasive for polishing general metals. Rotate the felt disc or cloth buff with a power tool to apply it. For semi-finishing of stainless steel, aluminum and chrome plating. * Do not use for anything other than its intended purpose.Type Solid abrasive Mass (g) 850
- MonotaRO Blast Abrasive GB Glass BeadsHigh quality glass beads that have cleared the quality standards of domestic manufacturers. Since it is a spherical particle, there is almost no cutting action, and the amount of polishing of the object can be reduced. For sandblast cleaning and parts regeneration. For cleaning various molds (rub... Read MoreSpecific Gravity 2.55
- MonotaRO Blast Abrasive WA type (white molten alumina)A white molten alumina abrasive with a high alumina content. Ideal for items that do not like residual iron or discoloration. It can be used as a sandblast or general abrasive. Base adjustment before painting, rust removal, paint peeling, stainless steel processing and plating peeling, carbon rem... Read MoreIngredient Aluminum oxide Hardness New Morse: 12, Knoop: HK2050
- Koyo-Sha Green Bar (Polishing Compound)The best gloss (mirror surface) can be obtained when used with offset felt. When used with offset sisal, it has a high-grade quasi-mirror finish (gloss finish that follows the mirror finish). Mirror finish of metal in generalType Solid abrasive Color Green Suitable Material All metals Process Finish polishing Applicable buff Sisal buff, cotton buff, felt buff RoHS directive (corresponding to 10 substances) Correspondence
- Fuji Manufacturing Fuji Glass BeadsIt is a spherical particle and has almost no cutting action. It has a wide range of grain size and a wide selection range, and can create a delicate top surface. [Generation of beautiful pear-skin texture] Cleaning without damaging various molds (rubber molding, die casting, etc.) such as sandbla... Read MoreType Semi-hard glass
- MonotaRO White Polishing Compound 67gIt has a good balance of grinding power and gloss, and is ideal for erasing scratches. For semi-finish polishing of stainless steel and aluminum * Do not use for anything other than its intended purpose.Specification For intermediate finishing Type Solid abrasive Mass (g) 67 Suitable Material Stainless steel, aluminum
- MonotaRO Tripoly 700GA solid oil-based abrasive for base polishing. Apply to felt disc or foil before use. For iron, stainless steel, aluminum and general metal finishes. * Do not use for anything other than its intended purpose.Type Solid abrasive Mass (g) 700
- CHUKYO KENMA Sabitoru (Polishing Compound)A safe and harmless elastic cleaner born in Germany. Since it is a completely water and oil resistant type, it can be used as a dry wet type depending on the application. It can be used almost where sandpaper can be used. For surface finishing of wood work. Removes rust and stains on the painted ... Read More
- Steam Ship Valve Compound (Wheelborundum)It is made by mixing and kneading abrasives such as GC / C carborundum, industrial oil and various greases into a paste. Used for lapping metal and stone materials such as cast iron, brass, copper and aluminum. Ideal for precision machining from rust removal due to roughness and fineness. * Do no... Read More
- SK (Niigata Seiki) Polishing powderRegardless of the size of the polished area, only the required amount can be dissolved in water, oil, etc. and used, so it can be adjusted according to the purpose of use.
- MonotaRO Green Bar 1050GA solid oil-based abrasive for general luster. Apply to felt disc or foil before use. For final finishing of brass, cast / forged products, precious metals, etc. * Do not use for anything other than its intended purpose.Type Solid abrasive Mass (g) 1050 RoHS directive (corresponding to 10 substances) Correspondence
- H&H Rust EraserJust rub it like an eraser to remove stubborn rust and dirt! [Roughness] Kogation, rust, etc. stuck to the grill, gas range, frying pan, etc. Corrosion and strong stains on bicycles, automobiles, etc. due to aging. Mold and dirt on the joints of the bathtub. Soil stains on the floor and rust on t... Read More
- MONAMI Valve CompoundAbrasive material Carbon random GC is kneaded with oil, and it is a very versatile product for polishing and grinding, from polishing valve shafts to removing rust. Carbon Random GC (Green Carbon Random) GC is a green silicon carbide abrasive with high SiC purity. An excellent abrasive that has t... Read MoreCapacity (g) 200
- Uyemura Red BarEspecially suitable when polishing power is required.Mass (g) 800 Suitable Material Ferrous, non-ferrous
- MonotaRO Tripoli Polishing Compound 67gIt has a particularly strong grinding power and is ideal for removing scratches on the emery buff. For finish polishing of iron, aluminum, copper, etc. * Do not use for anything other than its intended purpose.Specification For base Type Solid abrasive Mass (g) 67 Suitable Material Iron, aluminum, copper, etc.
- Koyo-Sha White BarFor medium polishing of all metalsType Solid abrasive Color White Mass (g) 340~390 Suitable Material All metals Process Medium polishing Applicable buff Sisal buff, hard cotton buff RoHS directive (corresponding to 10 substances) Correspondence
- Fuji Manufacturing Fuji Random WAIt is a white molten alumina abrasive with a large amount of alumina, and is ideal for products that dislike residual iron and discoloration. A high-purity alumina-based abrasive made by melting calcined alumina in an electric furnace, adjusting the crystal size and structure, and refining it. Du... Read MoreType Hard type ceramic RoHS directive (corresponding to 10 substances) Correspondence
- YANASE Blue bar GLThe finest product for the final finish. For the highest gloss finish of general metals with well-balanced cutting force and gloss. The highest gloss finish for metals in general.Suitable Material General metal RoHS directive (corresponding to 10 substances) Correspondence
- TRUSCO Blue stick (chromium oxide)For finish polishing. For scratch removal and mirror finish by applying to the felt buff series, brass, forged products, steel, stainless steel, etc.Mass (g) 430from S$24.99Min. 2 days
- Koyo-Sha TripoliUsed for blinding emery buffs. Or for polishing aluminum and resinType Solid abrasive Color Light pink Mass (g) 870~920 Suitable Material Aluminum, resin, etc. Process Rough polishing RoHS directive (corresponding to 10 substances) Correspondence
- YANASE No Chrome 5000Unused chrome product For the finest mirror finish Mirror finish of non-ferrous metal (aluminum, brass, zinc, etc.) Mirror finish of precious metalSpecification Used buffs / caraco buffs, emery buffs Mass (g) 250 RoHS directive (corresponding to 10 substances) Correspondence
- Koyo-Sha Prince LimeFor medium polishing of hard metals such as iron and stainless steel. For rough polishing of soft metals such as aluminum, copper, and brass.Type Solid abrasive Color White Suitable Material Iron, stainless steel, etc. Process Medium polishing Applicable buff Sisal buff, cotton buff RoHS directive (corresponding to 10 substances) Correspondence
- Uyemura White stickFocusing on polishing power, you can obtain gloss without fogging.Mass (g) 900
- TRUSCO Abrasive for ResinIt has very few buffs and is suitable for finishing transparent resin. Glossy finish of resin (plastic, acrylic, celluloid, etc.). Apply to the calico finish buff, flannel finish felt, and buff series.Mass (g) 350
- Koyo-Sha AloxGet the best gloss finish. When used with offset sisal, it has a high-grade quasi-mirror finish (gloss finish equivalent to mirror finish). Non-chrome. Mirror finish of all metals, non-ferrous metals such as aluminum and titaniumType Solid abrasive Color White Process Finish polishing Applicable buff Cotton buff, felt buff RoHS directive (corresponding to 10 substances) Correspondence
- ICHIGUCHI Green BarIt is a solid oil-based abrasive. Apply to felt disc or foil before use.Type Solid abrasive Mass (g) 180 RoHS directive (corresponding to 10 substances) Correspondence Act on Promoting Green Procurement Conformity
- SOKEN INDUSTRIES CO., LTD Finishing AbrasiveThe most popular finishing abrasive.Suitable Material White precious metal
- YANASE Resin abrasive 24PFor synthetic resins such as plastic, acrylic and celluloid. For resin and super gloss finish. It has few buffs and is suitable for finishing transparent resin. Buffs used ... Characo buffs, tea and buffs. resinMass (g) 500 Suitable Material Resin RoHS directive (corresponding to 10 substances) Correspondence
- Koyo-Sha DungeeAbrasive for finishing resin, painted surface, and plastic. Since the object is sensitive to heat, it is necessary to use a soft cotton buff and reduce the rotation speed of the buff. For finishing resin, painted surfaces, and plasticsType Solid abrasive Color Beige Mass (g) 470~510 Suitable Material Resin, painted surface, plastic Process Finish polishing Applicable buff Cotton buff RoHS directive (corresponding to 10 substances) Correspondence
- menzerna polishing compounds CompoundMenzelna is a compound maker with a history of over 100 years. It is used in musical instruments, precious metals, and industrial products in a very wide range of fields. Of course, it is also used for paint finishing in the automobile industry, and boasts a track record and reliability that is a... Read More
- Farecla Extra compoundHas specific gravity and maintains grindability. Ideal for removing yuzu skin after painting. Ideal for adjusting the skin of a cured coating film.RoHS directive (corresponding to 10 substances) Correspondence
- Uyemura Blue barNot only good luster, but also moderate machinability and buffing.Mass (g) 500 Suitable Material All metal
- TRUSCO Non-chromium abrasiveThe main component is an abrasive made of aluminum oxide. Non-chrome abrasives are applied to the felt buff series for scratch removal and mirror finishing. Since the finished surface is finer than the blue stick, it is also used for buffing after using the blue stick. Mirror finish of steel, sta... Read MoreMaterial Aluminum oxide, fatty acid Color Light green Mass (g) 370 Suitable Material Steel, stainless steel, aluminum, etc.
- Koyo-Sha Blue bar G-546Used for cotton buffs. Best gloss. Iron and stainless steel finish.Type Solid abrasive Color Green Mass (g) About 480 Suitable Material Iron, stainless steel, etc.