Pipe Saws
- KAKUDAI MFG Grinding saw replacement blade (2 pieces)It can also be attached to Super Saw E7.from S$29.99Min. 4 days
- MIYAKO Hole saw for PVCA hole saw for PVC pipes. MB149T-Use dimension 60 (50 yo) when using for 75 x 50 (P) and 100 x 50 (P), and use dimension 89 (75 yo) when using for 100 x 75 (P). * For electric drill rotation only. * Do not use impact drills, hammer drills, or vibration drills. * Please read the instruction manual... Read MoreCenter drill diameter (Φmm) 6×87from S$87.99Min. 5 days
- SANEI World saw α spare bladeWorld Saw α spare blade 1 pieceMaterial Steelfrom S$9.89Min. 3 days
- KAKUDAI MFG Sawing machineFor cutting and drilling of wood, new building materials, control panels, gypsum board, PVC, etc.from S$24.99Min. 5 days
- KAKUDAI MFG Hole saw for bathtubYou can drill holes in the enamel layer by inserting a diamond hole saw into the super steel hole. Also, because it is a magnet type, the diamond hole saw will not fall even if it is turned downward. In this case, replace the center drill for enamel and insert the stop sleeve to make a hole. For ... Read Morefrom S$279.90Min. 5 days
- SANEI Route world sawFor cutting and drilling when passing pipes through walls such as wood, plywood, and gypsum boardMaterial Steelfrom S$22.99Min. 3 days
- MIYAKO Mbso replacement bladeFor drilling circles and ovals of wood, plywood, etc. * Select the blade according to the intended use.Specification For routing Suitable Model MB167Sfrom S$17.99Min. 5 days
- MIYAKO MbsoUses a rubber and resin composite grip that fits in your hand. For PVC pipes and copper pipes * Select the blade according to the intended use.Specification 18 Yama Replacement Blades MB167SKfrom S$19.99Min. 5 days
- MIYAKO MbsoUses a rubber and resin composite grip that fits in your hand. For drilling circles and ovals of wood, plywood, etc. * Select the blade according to the intended use.Specification For routing Replacement Blades MB167SKfrom S$24.99Min. 5 days
- MIYAKO Mbso replacement bladeFor PVC pipes and copper pipes * Select the blade according to the intended use.Specification 18 Yama Suitable Model MB167Sfrom S$8.79Min. 5 days
- MIYAKO Mbso D typeThe angle of the blade can be changed. For PVC pipes and copper pipes * Select the blade according to the intended use.Specification 18 Yama Replacement Blades MB167DKfrom S$19.99Min. 5 days
- SANEI Leading world saw blade2 spare blades for Sanei faucet R394Material Steelfrom S$27.99Min. 3 days
- MIYAKO Mass dedicated hole sawSeal packing for mass A hole saw for mass suitable for MSP600. Convenient for drilling vinyl mass, resin board, plywood, gypsum board, etc. * The dynamic drill driver is for rotation only. * Do not use impact drills, hammer drills, or vibration drills. * Please read the instruction manual and use... Read Morefrom S$74.99Min. 5 days
- MIYAKO Mb sawThe tip is a woodworking drill. The saw blade has a round bar shape and can be cut into various shapes.from S$37.99Min. 5 days
- MIYAKO Mbso D type replacement bladeFor PVC pipes and copper pipes * Select the blade according to the intended use.Specification 18 Yama Suitable Model MB167Dfrom S$8.79Min. 5 days
- SANEI Speed saw taperFor cutting PVC pipes, etc. Since the tip is thin, it is easy to aim at the cut part. Ideal for work in narrow spaces where pipes are adjacent to each other. You can use it repeatedly by replacing it with the optional blade (R3930F). Remove the mounting screw, pull out the spare blade, and replac... Read MoreMaterial Copperfrom S$19.99Min. 3 days
- TOTO Carbide hole saw for enamel busA hole saw for cutting metal parts and making through holes for connecting hooks. Make a hole with Φ54 and attach U packing to make the inner diameter Φ50.Specification For Φ54Discontinued
- SANEI Speed saw taper bladeShipping unit 5 pieces. Spare blade for speed saw taper (R3930) sold separately. For cutting PVC pipes, etc. Since the tip is thin, it is easy to aim at the cut part. Ideal for work in narrow spaces where pipes are adjacent to each other. Remove the mounting screw, pull out the spare blade, and r... Read MoreMaterial CopperDiscontinued