Hydraulic Auxiliary Equipment
Other Related Pages
- Taisei Kogyo Filter elementThe most standard T-type connection medium pressure in-line filter. You can customize it according to your purpose from abundant options, including an indicator that can detect differential pressure (visual electrical contact type). The oil flow direction can be easily changed from right to left ... Read MoreType of Filter Material General filter paperfrom S$44.99Min. 2 days
- DAIKIN INDUSTRIES LT cooler (water-cooled oil cooling equipment)An oil cooling device (water-cooled) that has a large cooling capacity with a small amount of water. For fresh water and construction water. (Seawater cannot be used) With brazing that reliably transfers the heat of the fins. The threaded fins stir the oil. It can be installed 360 ° freely. The l... Read More
- Taisei Kogyo suction filterA tank internal filter for general hydraulic oil. It is a stainless wire mesh type. The standard filtration accuracy is 60, 100, 150, 200 mesh.Type of Filter Material Wire mesh (SUS)from S$119.90Min. 24 days
- Taisei Kogyo Suction StrainerA tank internal filter for general hydraulic oil.Type of Filter Material Wire mesh (SUS)
- Taisei Kogyo Air BreatherIt can be easily installed by simply providing an Rc female screw seat on the tank side. The structure is simple and the elements can be easily cleaned and regenerated.How to Use Installed on top of reservoir tank
- Taisei Kogyo Suction FilterA suction tank internal filter for general hydraulic oil. For general hydraulic oil. * When attaching or detaching to the pipe, hang a spanner on the hexagonal part of the mouthpiece.Type of Filter Material Notch wire
- OHTSUKA Pipe clamp heavy seriesThere is a gap (E) to ensure the correct clamping force.Type Single clampfrom S$15.99Min. 2 days
- Masuda Manufacturing Suction strainer W-MSN typeIt is a suction filter inside the tank. The filter medium is a stainless steel wire mesh with low pressure loss, and if it becomes clogged, it can be used repeatedly and economically by cleaning it. It can be used not only for general mineral oil but also for flame-retardant hydraulic oil.
- Iehara Light Kogyo Air vent C typeCan be used indoors and outdoors, especially outdoors Prevents oil from boiling Prevents dust from the outsideHeat Resistance Temperature (℃) 115(MAX)
- Taisei Kogyo Filter ElementThe most popular replacement filter paper filter element for general hydraulic fluids. Made by ISO14001 certified factory For general hydraulic oil.
- Masuda Manufacturing Air Breather MSA TypeWidely used in hydraulic systems for industrial machines, machine tools, ships, etc. Light alloy is used for the material, and it has excellent toughness and durability. The structure is concise and easy to disassemble and maintain. Excellent safety due to the semi-flammable structure.
- Masuda Manufacturing Suction Strainer MST TypeSince it is made of all-light alloy, there is no deterioration of oil due to accelerated oxidation. Made of all-light alloy, it is extremely solid, lightweight, and has no disconnection or opening. Cumulative clogging does not increase resistance. Since the shape of the gap is special and the sur... Read Morefrom S$35.99Min. 2 days
- Taisei Kogyo Suction FilterA tank internal filter for flame-retardant hydraulic oil. Made of all stainless steel. The standard filtration accuracy is 60, 100, 150, 200 mesh. * When attaching or detaching to the pipe, hang a spanner on the hexagonal part of the mouthpiece.Type of Filter Material Wire mesh (SUS)from S$49.99Min. 2 days
- Taisei Kogyo Cartridge Filter for CF06 / 08Suitable for CF-06、CF-08 Filtration (μm) 10
- KANTO Kizai KNF Suction Strainer Filter* We do not deliver to private homes (detached houses / apartments). * Depending on the delivery location, the delivery date may be postponed and additional shipping charges may be incurred.
- Masuda Manufacturing Air Breather MB TypeUses SPCC pressed products as the material. It is compact, inexpensive, and comes in a variety of sizes.
- Iehara Light Kogyo Air release type BRADesigned to be low from the mounting surface Made of metal, it has excellent strength and chemical resistance.Material C3604
- OHTSUKA Pipe clamp standard seriesBy using a pipe clamp, you can lay out the pipes in an orderly manner. This facilitates work and maintenance, reduces plumbing costs and days, and reduces Contributes to improving work safety. It also has the effect of reducing piping vibration, which contributes to environmental conservation.from S$9.59Min. 2 days
- DAIEI GIKEN KOGYO Oil Strainer CS SeriesThe suction resistance of the strainer is 6.65 kpa or less at the maximum flow hydraulic oil viscosity of 150 SSU. Install so that the total suction resistance, including the strainer, does not exceed 16.6 kpaHg. If the suction resistance increases due to clogging, remove the strainer, shake it i... Read MoreMesh Size 150
- FUJI SPECIAL Iron-plated tube clamp both pressersMaterial SS41 Surface Treatment Unichrome plating treatmentfrom S$4.69Min. 2 days
- Taisei Kogyo Filter ElementA screw-in type line filter with a maximum working pressure of 0.5 MPa. A magnet can be attached as an option. Indicators and relief valves cannot be installed.Type of Filter Material General filter paper
- Iehara Light Kogyo Air release type PNA-FDesigned to be 30% lower than the conventional C type. Designed to prevent the cap from returning easily. Comes with a filter to cut dust inside and outside.Material Nylon resin Heat Resistance Temperature (℃) (Body) 80 (MAX)from S$5.99Min. 2 days
- Iehara Light Kogyo Air release PNA-G typeAir is discharged when the working pressure is reached. Suitable for transportation with working oil. The cap does not return easily. No dust from the outside is sucked. Discharge The working pressure can be changed (optional).Material Nylon resin Heat Resistance Temperature (℃) (Body) 80 (MAX)
- Taisei Kogyo Filter elementMaximum working pressure 3.5MPa Impulse test 0-3.5MPa x 107 times Type 351 has a screw connection, and type 352 has a phase flange connection. This product is a bottom-drawing type T-type filter.Type of Filter Material General filter paperfrom S$44.99Min. 2 days
- Taisei Kogyo Filter elementInstalled on the reservoir tank, it prevents contamination from entering at the same time as the air sucked into the tank. It can be easily installed by simply providing an Rc female screw seat on the tank side. (AP-02-24) For AP-32 and 48, JIS5K.FF flange is standard equipment. The standard spec... Read Morefrom S$7.49Min. 2 days
- Iehara Light Kogyo Air release type AHigh heat-resistant temperature, excellent weather resistance and chemical resistance Prevents boiling of oil Prevents dust from the outsideMaterial Phenolic resin Heat Resistance Temperature (℃) 170(MAX)from S$10.99Min. 6 days
- Masuda Manufacturing Cartridge filter LPF typeIt consists of a cartridge equipped with a relief valve and a connection port, and an integrated element and casing.from S$119.90Min. 2 days
- Taisei Kogyo Filter elementMaximum working pressure 1MPa Impulse test 1MPa x 107 times A filter that is directly attached to the top of the tank. Both screwing and flange (optional) piping connections are possible. The relief valve structure of TRF-16, 20 and 24 is different from this figure. Use Φd3 holes and tighten them... Read MoreType of Filter Material General filter paperfrom S$57.99Min. 14 days
- OHTSUKA Pipe clamp Twin clamp seriesBy using a pipe clamp, you can lay out the pipes in an orderly manner. This facilitates work and maintenance, reduces plumbing costs and days, and reduces Contributes to improving work safety. It also has the effect of reducing piping vibration, which contributes to environmental conservation.
- Taisei Kogyo Filter ElementThe shape of the suction filter with case does not cause air accumulation inside. The standard element is stainless steel wire mesh 60, 100, 150, 200 mesh. The clogging of the filter element can be confirmed by the indicator. The built-in relief valve prevents the risk of clogging. * The value in... Read MoreType of Filter Material Wire mesh (SUS)from S$97.99Min. 14 days
Filter by categories