It is a tool that temporarily expands the frame, such as removing the hub stuck to the frame and replacing the tires and tubes with the wheels attached to the frame. Since the attachment moves according to the angle of the frame, it will not slip or be scratched even with a steep frame. Since the... Read More
Mass (g) 880 Maximum Width (mm) (Open) 160 / (Close) 80 Overall Length (mm) 305~405
It is convenient for deburring the inside of the pipe and enlarging the hole. For repairing and enlarging holes in metal plates. Outstanding sharpness and durability. Ideal for repairing and enlarging holes in aluminum plates, thin iron plates, etc.
* Please wear protective goggles when working.
RoHS directive (corresponding to 10 substances) Correspondence
A convenient tool for removing burrs inside pipes after cutting fork columns and handles. A spare blade can be stored inside the main body
Metal pipe, drilling work, deburring of cut surface
Blade Length (mm) 10 Overall Length (mm) 148 Mass (g) 35 Included Accessories K-35-1 / 2/3 replacement blade x 1 each
Set a T-shaped handle and 3 size taps
* When using tap dies, be sure to lubricate with cutting oil.
Mass (g) 95 RoHS directive (corresponding to 10 substances) Correspondence Set Contents M3×0.5、M4×0.7、M5×0.8(ISO) Included Accessories T-shaped tap handle
A Y-shaped head is used for the crank wrench, which is the most popular head of Park Tool. The laser-cut spanner mouth is highly accurate and fits the nut.
A gauge that checks and corrects distortion of the derailleur hanger (pedestal). The most common cause of shift change defects is the distortion of this derailleur hanger. Also supports through axle type frame ends. Install the instrument in the screw hole where the derailleur is attached, rotate... Read More
A tool used to replace the inward hook type stand spring. The left side is for outward facing and the right side is for inward facing type stands. The spring can be installed easily and quickly using the principle of leverage.
A belt wrench that is convenient for maintenance of the rear suspension. The rubber-coated strap bites firmly without damaging the slippery parts on the surface.
A tool that allows you to easily remove the headset when replacing the headset. Insert it into the head tube from the side that has not spread, and when the spread part gets caught in the head cup, hit the head with a hammer and remove the head cup.
Cutting guide for pipes with a large diameter of 45 mm. It is compatible with 1.5 inch fork columns and can easily cut aero type seatposts that were difficult to cut straight. In addition to the groove used when using a normal metal saw, a groove used when using a CSB-1 spare blade for carbon res... Read More
Jaw Opening Width (mm) (Maximum) 89 Pipe Diameter (Φmm) 32~45 Dimension (mm) About 150 × 83 × 55 Mass (g) About 740
A tool that press-fits a ball race into a fork column. Oversized columns such as MTB as well as standard size fork columns can be used by replacing the attached adapter ring.
* Some models such as suspension forks and carbon columns cannot be used.
FFS-2 can be used not only for frames and forks, but also for almighty such as modifying cranks and handlebars. Vinyl-coated hooks and fulcrums are less likely to damage the object.
Considering workability, the upper attachment and shaft are assembled from the handle to one, and a two-piece structure with the lower attachment is used. In addition, the specifications are designed with consideration for worker safety so that the shaft will not come off accidentally during work... Read More
Method Built-in bearing type Shaft Diameter (Φmm) 18 Dimension (Φmm) (Attachment) 25.8, 29.7, 34.8, 39.7, 46 Mass (kg) 1.9 Suitatible Head (Long) 80-220mm
A press-fitting tool that allows you to easily and quickly install a one-piece crank hanger or head one. It has a convenient structure that allows you to remove the main body immediately after press-fitting by simply pressing the push lock. Stepped pushes and pedestals can be used for regular siz... Read More