Hub Cleaning Brushes
The hub hair is a rider's goods that is attached to the hub axle in the center of the bicycle wheel. The hub axle is cleaned using the rotation of the wheels during driving. By attaching hub hair, it is possible to keep the hub part, which is difficult to clean, clean. In addition to single colors such as red, black, and purple, there are multiple types of colors, including three colors, so that you can enjoy coordination according to the design of the bicycle. Various hair hardness and length. Some hub hairs are compatible with auto light bicycles.
- WINTEC Hub hairBy riding a bicycle, the hub will be clean. Please attach it to the hub axle of your bicycle and use it for cleaning the hub axle.Color Red
- Sanyu Hub hairJust by attaching this, the wheel will clean the hub part, which is difficult to reach, as it turns.Discontinued
- CAPTAIN STAG Hub hairConvenient for cleaning the hub axle. * Colors different from the image may arrive. Please note.Color RGB Mass (g) 10Discontinued
- Sanyu Deluxe color hub hairJust by attaching this, the wheel will clean the hub part, which is difficult to reach, as it turns.Color Tricolor Quantity 1 set (24 pairs)Discontinued
- Sanyu Hub hair for interiorJust by attaching this, the wheel will clean the hub part, which is difficult to reach, as it turns.Discontinued
- Sanyu Hub hair for interior (for auto light hub)Just by attaching this, the wheel will clean the hub part, which is difficult to reach, as it turns.Discontinued