Shoe Covers
- R250 Waterproof Silicone Shoes CoverJust put it on the shoes you are wearing. Aero and rainy silicone shoe cover. Originally it is a rain cover for ordinary shoes, but if you hollow out the cleat part with scissors, it is an excellent aero shoe cover for cycle shoes that can also be used as a simple rain shoe cover. Since it is a s... Read More
- Nikko Shoji 70 Bicycle shoe coverFully waterproof shoe cover with reflective tape. Comfortable without getting your shoes wet even on a bicycle on a rainy day. Squeezing the elastic cord prevents it from slipping off. With size adjustment magic tape on the heel. Comes with reflective tape for peace of mind even at night.Material Polyester, PVCfrom S$19.99Min. 5 days
- Pearl Izumi Windbreak + print + shoe coverA shoe cover that can handle temperatures of 5 ° C. Uses "Windbreak?" Material that is both windproof and heat-retaining to protect your feet from cold wind. It is an item that asserts individuality from your feet with a sharp geometric pattern. Can be coordinated with the Windbreak Jac... Read Morefrom S$119.90Min. 7 days
- Pearl Izumi Windbreak + Road + Half + Shoe CoverA half-type shoe cover that is convenient to carry and can handle temperatures of 10 ° C. It is easy to put on and take off because it uses "Windbreak?" Material that has both windproof and heat retention and is a type that is fastened to the ankle with Velcro. Retroreflective placement... Read MoreColor Blackfrom S$79.99Min. 7 days
- Pearl Izumi Rain + racer + shoe coverIt is a rain shoe cover that fits the shoes perfectly using stretchable material. When used in combination with rainover pants, biking in the rain is even more comfortable. * Made for riding a bicycle, please avoid using it while walking due to the nature of the product. * It is recommended to we... Read MoreColor Blackfrom S$95.99Min. 7 days
- Pearl Izumi Coated shoe coverPolyurethane coated material reduces air resistance while driving. It is a shoe cover that can be used not only in road races and track events, but also in everyday driving scenes. Polyurethane coating processing. * It is made for riding a bicycle. Due to the nature of the product, please avoid u... Read Morefrom S$63.99Min. 10 days
- Pearl Izumi Heater shoe coverA shoe cover with a built-in heater for bicycles. A carbon fiber heater wraps around the instep to warm it. The double-layered batting structure keeps the heater warm without letting it escape, and the power of the heater warms the toes that make you feel cold. The heater and batting keep the fin... Read MoreRecharging Time (hours) About 6-7 (full charge) Color Blackfrom S$369.90Min. 10 days
- Pearl Izumi Windbreak + Light + Toe CoverA type of cover that keeps only the toes warm, which is convenient when the toes are a little cold. It can be worn on the inside of the shoe cover in the midwinter, and it is an item that can further enhance the windproof and heat retention function of the toes. With retroreflection, visibility a... Read MoreColor Blackfrom S$55.99Min. 8 days
- Pearl Izumi Heater + shoe coverA shoe cover with a built-in heater for bicycles. A carbon fiber heater wraps around the instep to warm it. The double-layered batting structure keeps the heater warm without letting it escape, and the power of the heater warms the toes that make you feel cold.・ Heater and batting keeps the fing... Read MoreColor Blackfrom S$369.90Min. 7 days
- Pearl Izumi Coating + shoe coverPolyurethane coated material reduces air resistance while driving. It is a shoe cover that can be used not only in road races and track events, but also in everyday driving scenes. * Made for riding a bicycle, please avoid using it while walking due to the nature of the product.from S$63.99Min. 7 days
- Pearl Izumi Knit + shoe coverA 10 ° C-compatible knit shoe cover that has excellent elasticity of a tightly knitted knit material, moderate wind resistance and heat retention, and can also be used as an accent for coordination. Retroreflectives at the back of the ankle also ensure night visibility. Make a notch perpendicular... Read MoreSize Ffrom S$55.99Min. 7 days
- Pearl Izumi Rain + shoe coverIt can be easily attached and detached with a fully open fastener. The size can be adjusted with Velcro on the sole of the foot, and it can be used for casual shoes as well as road bike shoes. When used in combination with rain pants (2357), biking in the rain is even more comfortable. * Made for... Read MoreColor Blackfrom S$87.99Min. 7 days
- Pearl Izumi Windbreak light socks coverA thin windproof item that can be worn over socks to prevent cold air from inside the shoes. The appearance of your favorite shoes is windproof, and the soles have a non-slip material that conveys power to the pedals. * "Nanofront" is a polyester nanofiber developed by Teijin Frontier C... Read MoreColor Blackfrom S$79.99Min. 10 days
- Pearl Izumi Coating + long + shoe coverIt is a length (+4 cm) model of the coated shoe cover (86). Polyurethane coated material reduces air resistance while driving. It is a shoe cover that can be used not only in road races and track events, but also in everyday driving scenes. * It is made for riding a bicycle. Due to the nature of ... Read Morefrom S$79.99Min. 7 days
- Pearl Izumi Windbreak + Light + Socks CoverA thin windproof item that can be worn over socks to prevent cold air from inside the shoes. The appearance of your favorite shoes is windproof, and the soles have a non-slip material that conveys power to the pedals. * "Nanofront (R)" is a polyester nanofiber developed by Teijin Fronti... Read MoreColor Blackfrom S$79.99Min. 7 days
- MARUTO (Okubo Seisakusho) Bicycle shop shoe coverBicycle rain protection shoe cover With a hook-and-loop fastener that can be fully opened, it can be attached and detached even while wearing rainwear. The pedal part uses a non-slip tarpaulin fabric.Color Beige Finish Processing PU coating Material Polyester Suitable Size Sneaker indication: 22-28cm (unisex) Included Accessories Storage bagDiscontinued
- Pearl Izumi Rain racer shoe coverIt is a rain shoe cover that fits the shoes perfectly using stretchable material. When used in combination with rain pants (2357), biking in the rain is even more comfortable.Color BlackDiscontinued
- R250 Shoe cover plusAnother piece when it's really cold with just the shoe cover・ It is the toes that get the coldest. Cover only that toe. Left and right set (There is no distinction between left and right.) Be sure to wear the shoe cover from above. Especially recommended to combine with a sock type shoe cove... Read MoreSize Free size Mass (g) 30Discontinued
- Pearl Izumi Premium shoe coverThe best warmth is achieved by using "Windbreak Titanium" material, which boasts high heat retention due to the windproof property of titanium film and the effect of far infrared rays. A flagship model of the shoe cover that protects your feet from the cold by increasing heat retention ... Read MoreColor BlackDiscontinued
- Pearl Izumi Windbreak light to coverA type of cover that keeps only the toes warm, which is convenient when the toes are a little cold. It can be worn on the inside of the shoe cover in the midwinter, and it is an item that can further enhance the windproof and heat retention function of the toes. Retroreflective toes and sides als... Read MoreColor BlackDiscontinued
- Pearl Izumi Windbreak road half shoe coverA cycling shoe cover that supports temperatures of 0°C to keep you warm even when riding in the coldest season. Uses "Windbreak (R)" material that combines wind resistance and heat retention. The inside is double-filled from the toe to the instep to increase heat retention. Two retroref... Read MoreColor BlackDiscontinued
- Pearl Izumi Premium + shoe coverThe best warmth is achieved by using the "Windbreak Titanium" material, which boasts high heat retention due to the windproof property of the titanium film and the effect of far infrared rays. A flagship model of the shoe cover that protects your feet from the cold by increasing heat re... Read MoreColor BlackDiscontinued
- Pearl Izumi Premium shoe coverThe best warmth is achieved by using "Windbreak Titanium" material, which boasts high heat retention due to the windproof property of titanium film and the effect of far infrared rays. A flagship model of the shoe cover that protects your feet from the cold by increasing heat retention ... Read MoreColor Black Mix Rate (%) Polyester 87, polyurethane 13Discontinued
- Pearl Izumi Rain shoe coverIt can be easily attached and detached with a fully open fastener. The size can be adjusted with Velcro on the sole of the foot, and it can be used for casual shoes as well as road bike shoes. When used in combination with rain pants (2357), biking in the rain is even more comfortable. With a ded... Read MoreColor BlackDiscontinued
- Pearl Izumi Windbreak print shoe coverShoe covers for temperatures up to 5°C. Uses "Windbreak (R)" material that combines wind resistance and heat retention to protect your feet from cold wind. It is an item that asserts individuality from the feet with a sharp geometric pattern. Can be coordinated with the windbreak jacket... Read MoreDiscontinued
- Pearl Izumi Windbreak Winter MTB Shoe CoverA convenient shoe cover that can be used for both MTB shoes and road shoes and is compatible with temperatures of 5°C. The "Windbreak (R)" material, which combines wind resistance and heat retention, is used, and the soles and rear part are Velcro type, making it easy to put on and take... Read MoreColor BlackDiscontinued
- Pearl Izumi Windbreak thermo shoe cover 7906-3A cycling shoe cover that supports temperatures of 0°C to keep you warm even when riding in the coldest season. Uses "Windbreak (R)" material that combines wind resistance and heat retention. The inside is double-filled from the toe to the instep to increase heat retention. Two retroref... Read MoreColor BlackDiscontinued
- Pearl Izumi Windbreak + Road + Shoe CoverA standard item for winter shoe covers that can handle temperatures of 5 ° C. The "Windbreak?" Material, which is both windproof and heat-retaining, has been adopted, and the rear part has been updated with a fully open fastener, making it even easier to put on and take off, and usabili... Read MoreColor BlackDiscontinued
- Pearl Izumi Windbreak print shoe coverA shoe cover that can handle temperatures of 5 ° C. The "Windbreak" material, which is both windproof and heat-retaining, protects your feet from the cold wind. You can also coordinate with the windbreak jacket (3555-BL) and windbreak print tights (6020-3D). * This shoe cover is made on... Read MoreMix Rate (%) polyester 95%, polyurethane 5Discontinued