Bicycle Key Holders
Key holders are mainly intended to prevent key loss by attaching to a key. There are two types, a general shape type and a bracelet type that attaches to the wrist, and there are other uses such as a light type that can find the keyhole etc. even in a dark place and a whistle that can inform the surroundings in an emergency. There is also a key ring that combines. A type using a reflective material can be attached to a bag to help ensure safety at night.
- KAWASUMI SEISAKUSYO Bracelet keychainA key chain that you can attach to your wrist when shopping, etc., will free you from loss.Material Polyurethane Color Yellow Mass (g) 5 RoHS directive (corresponding to 10 substances) Correspondence
- WINTEC Key ring with bellIt is a commonly used key chain. To prevent loss of bicycle keys * Color cannot be specified due to assortment.
- Fuji Honsha No.12 Key ring with bellColor Assortment (Green, Red, Blue 10 each)from S$39.99Min. 2 days
- KAWASUMI SEISAKUSYO Key ring with bell Clear 6 colors assortmentKey chain with a bell with a stylish clear color A set of 6 colors assortedColor Assorted RoHS directive (corresponding to 10 substances) Correspondencefrom S$34.99Min. 2 days
- WINTEC Key ring star-shaped phosphorescentLuminescent type that glows faintly in the dark when exposed to lightfrom S$4.79Min. 9 days
- YUTAKA MAKE Paramate keychainNormally, it is used as a key chain or decoration, and in case of emergency, it becomes a rope when the bracelet is untied, and it becomes a rope that can be used for various purposes such as binding in case of emergency. For decorationRoHS directive (corresponding to 10 substances) Correspondencefrom S$6.39Min. 7 days
- Fuji Honsha No.80 Cute mascot key ringA rich set of types and colors. With a bell! For bicycles and house keysfrom S$79.99Min. 6 days
- Fuji Honsha No.85 Glowing (phosphorescent) mascot key chainLuminescent type that glows in the dark! With bells! For bicycles and house keysfrom S$119.90Min. 6 days
- Fuji Honsha Key ring with bell (two-tone)A simple belt type with a bell. Accented with different colors on the outside and inside of the belt. For bicycles and house keysfrom S$119.90Min. 6 days
- YUTAKA MAKE Paramate key chainThe parachute cord (paracord) with good coloring is woven and finished. In an emergency, you can untie the stitches and use it as a rope. * Cannot be used for securing the body or hanging luggage.from S$7.49Min. 3 days
- Asahi Cycle BK for right side of cycle mirror with reflectorA reflector is attached to the back of the mirror for safe driving at night. Mirror (for general car)Color Black Mass (g) 150from S$25.99Min. 6 days
- WINTEC Joint coil holderIt is coiled and can be freely stretched. Connect with the key to prevent loss.Color Red
- B.free Anchor binaConvenient 3 hooks! Keys can be sorted according to usage.from S$4.69Min. 7 days
- CAPTAIN STAG Keychain StringA key chain with a bell. To prevent loss. Color cannot be specified due to assortment.Mass (g) 5from S$4.19Min. 2 days
- Kawasumi bracelet keychainOne-touch telescoping When you get off your car, motorcycle, or bicycle, you can rest assured that the key bracelet style will not get in the way when shopping. The next time I use the key, I always have it at hand. Attachment and detachment with an elastic ring One-touch Vectran core included fo... Read Morefrom S$5.49Min. 7 days
- Fuji Honsha Keychain clear string with bell 30 pieces roseAs ONE Part Number 64-9547-57from S$36.99Min. 7 days
- WINTEC Whistle with key ring LED lightMulti-function keychain with LED light and whistle Turns on when you press the button, turns off when you release it * Batteries cannot be replacedMaterial Transparent ABS resin Mass (g) About 11 Light Source High brightness white LED Battery 2 LR41 buttonsDiscontinued
- KAWASUMI SEISAKUSYO Clip reflector (character)Reflects on car lights to improve visibility at night. Built-in magnet allows you to sandwich it in thin cloth, etc. With a chain that can also be used as a key chain, it can be hung on a bag or school bag ReflectorDiscontinued
- KAWASUMI SEISAKUSYO Clip reflector (animal)Reflects on car lights to improve visibility at night. Built-in magnet allows you to sandwich it in thin cloth, etc. With a chain that can also be used as a key chain, it can be hung on a bag or school bag ReflectorDiscontinued
- WINTEC Flashlight keychainFlashlight type key chain. It's small, but it shines well.Color RedDiscontinued
- KAWASUMI SEISAKUSYO Clip reflector (cross)Reflects on car lights to improve visibility at night. Built-in magnet allows you to sandwich it in thin cloth, etc. With a chain that can also be used as a key chain, it can be hung on a bag or school bag ReflectorDiscontinued
- WINTEC Name stickerIt is an anti-theft product. Please use it to prevent theft of your bicycle.Discontinued
- WINTEC Blue eye (LED keychain)It's small, but it shines well. To prevent loss of bicycle keys. It is convenient to illuminate the keyhole when using a bicycle at night.Color White Lighting color BlueDiscontinued