Batteries
Batteries are power devices that supply power. By attaching batteries to many devices, they can be used with power. It is used in equipment that requires batteries, used in everyday places such as homes. The use of batteries is particularly suitable for devices that run on low power, such as table clocks and remote controls. There are batteries of various sizes, such as alkaline batteries and lithium batteries, and many batteries can be reused by charging them from the outside.
Other Related Pages
- MonotaRO Alkaline Dry Cell Batteries AAPowerful and long life! Design with obvious size. Uses 0 (zero) mercury. Batteries may leak, overheat, explode, or cause injury or equipment failure depending on the usage pattern, usage environment, storage environment, etc., so be sure to observe the following. * If the alkaline solution of the... Read MoreType AA Voltage (V) 1.5
- MonotaRO Alkaline Dry Cell Batteries AAAPowerful and long life! Design with obvious size. Uses 0 (zero) mercury. Batteries may leak, overheat, explode, or cause injury or equipment failure depending on the usage pattern, usage environment, storage environment, etc., so be sure to observe the following. * If the alkaline solution of the... Read MoreType AAA type Voltage (V) 1.5
- Mitsubishi Electric Alkaline battery + AAALong-lasting power.Type AAA type
- MonotaRO Alkaline button batteriesIt is a low-cost and economical button battery. The operating voltage is as high as 1.5V and has a high capacity. Flashlights, calculators, electronic dictionaries, game consoles, Demand is increasing due to the miniaturization of devices such as thermometers. There are many varieties that are th... Read MoreNominal Voltage (V) 1.5
- Panasonic Alkaline Batteries AARecommended for use Long-term storage of 10 years is possible. Uses a liquid leakage prevention manufacturing method. By improving the negative electrode material, both safety and power generation efficiency are improved by improving anti-leakage and reactivity. * According to the recommended usa... Read MoreType AA
- Panasonic EVOLTA batteries AAThe longest in the industry! D-size to AAA-size can be stored for a long time of 10 years! Demonstrates superior performance over alkaline dry batteries in a wide range of discharge currents, from small currents to large currents. Suitable for equipment that uses a large amount of current continu... Read MoreMass (g) 24 Type AA Voltage (V) 1.5
- MonotaRO Alkaline Dry Cell Batteries AA High PowerA high-quality alkaline battery that can be used up to a large current range. Ideal for devices that use large currents in an instant, such as digital cameras and photo flashes. When used with a digital camera, it lasts 1.5 times longer than a Monotaro alkaline battery. Batteries may leak, overhe... Read MoreType AA Voltage (V) 1.5
- Panasonic Alkaline Battery AAA SizeRecommended for use Long-term storage of 10 years is possible. Uses a liquid leakage prevention manufacturing method. By improving the negative electrode material, both safety and power generation efficiency are improved by improving anti-leakage and reactivity. * According to the recommended usa... Read MoreType AAA type
- TOSHIBA Alkaline Batteries AAAlkaline batteries that have both long-lasting power and cost performance For equipment that requires continuous high output, such as digital cameras and work lights
- Mitsubishi Electric Alkaline battery + AAAType AAA type Voltage (V) 1.5 Quantity per Set (pieces) 4 pieces RoHS directive (corresponding to 10 substances) Correspondence Act on Promoting Green Procurement Conformityfrom S$2.49Min. 2 days
- ESCO 205x66x36mm battery case (for AA / clear)Can be stacked for storing and carrying batteriesColor Clear Suitable Battery AA batteries Number of Storage AA x 24 (upper row 12, lower row 12)from S$16.99Min. 3 days
- ELECOM Battery case / for AAAIt doesn't rattle and fall in the case. A battery case for AAA batteries that can be stored compactly without the batteries snapping into place.Other Set of 2 Material Polypropylene Number of Storage (pieces) 4 x AAA batteries Suitable Battery AAA batteriesfrom S$6.49Min. 11 days
- Mitsubishi Electric Alkaline Batteries AALong-lasting power.Mass (g) 96 Type AA Operating Temperature Range (℃) -20~60 Voltage (V) 1.5
- MonotaRO Alkaline Dry Cell Batteries DPowerful and long life! Design with obvious size. Uses 0 (zero) mercury. Batteries may leak, overheat, explode, or cause injury or equipment failure depending on the usage pattern, usage environment, storage environment, etc., so be sure to observe the following. * If the alkaline solution of the... Read MoreType Single 1 type Voltage (V) 1.5
- MonotaRO Alkaline Dry Cell Batteries CPowerful and long life! Design with obvious size. Uses 0 (zero) mercury. Batteries may leak, overheat, explode, or cause injury or equipment failure depending on the usage pattern, usage environment, storage environment, etc., so be sure to observe the following. * If the alkaline solution of the... Read MoreType Single 2 type Voltage (V) 1.5
- MonotaRO Alkaline Battery Square 9VIt is safe because it uses 0 (zero) mercury and 0 (zero) cadmium. Recommended usage period 2 years Batteries may leak, overheat, explode, or cause injury or equipment failure depending on the usage pattern, usage environment, storage environment, etc., so be sure to observe the following. * If th... Read MoreType 9V type (alkali) Voltage (V) 9 Quantity per Set (pieces) 1 piece
- MonotaRO Silver Oxide Coin Cell Battery SR44It is compatible with the LR44 and features a very stable voltage. Ideal for use in high-tech equipment, cameras, calipers, quartz watches, and precision equipment such as light meters. It also has a long life and lasts longer than the LR44. SR44: Games, calculators, cameras, pedometers, calipers... Read MoreType SR44 (silver oxide) Nominal Voltage (V) 1.55
- Panasonic EVOLTA Dry Cell AAADemonstrates high performance in all current ranges! You can experience longevity in various devices. The internal volume and strength are increased, and it lasts longer. The longest in the industry! Long-term storage with a recommended usage period of 10 years is possible! You can use it safely ... Read MoreType AAA type
- Panasonic Alkaline battery square 9VLong-lasting large current power. For equipment that uses a large amount of current continuously.Voltage (V) 9
- MonotaRO Alkaline Dry Cell Batteries AAA High PowerA high-quality alkaline battery that can be used up to a large current range. Ideal for devices that use large currents in an instant, such as digital cameras and photo flashes. When used with a digital camera, it lasts 1.5 times longer than a Monotaro alkaline battery. Batteries may leak, overhe... Read MoreType AAA type Voltage (V) 1.5
- maxell Alkaline Battery Single TypeShrink pack Large current, suitable for continuous use. Excellent liquid leakage resistance and storage stability. Uses 0 mercury and 0 cadmiumType Single 1 type Voltage (V) 1.5 Quantity per Set (pieces) 4 pieces Act on Promoting Green Procurement Conformity
- Panasonic Alkaline Battery Single TypeRecommended for use Long-term storage of 10 years is possible. Uses a liquid leakage prevention manufacturing method. By improving the negative electrode material, both safety and power generation efficiency are improved by improving anti-leakage and reactivity. * According to the recommended usa... Read MoreType Single 1 type Voltage (V) 1.5
- Panasonic N alkaline button batteryFor cameras, calculators and games.Standard LR44 Voltage (V) 1.5
- maxell Alkaline Battery AAType Single 2 type Voltage (V) 1.5 Quantity per Set (pieces) 4 pieces Act on Promoting Green Procurement Conformity
- Panasonic Evolta dry cell single 1 formDemonstrates high performance in all current ranges! You can experience longevity in various devices. The internal volume and strength are increased, and it lasts longer. The longest in the industry! Long-term storage with a recommended usage period of 10 years is possible! You can use it safely ... Read MoreType Single 1 type
- Panasonic Alkaline battery single 2 formRecommended for use Long-term storage of 10 years is possible. Uses a liquid leakage prevention manufacturing method. By improving the negative electrode material, both safety and power generation efficiency are improved by improving anti-leakage and reactivity. * According to the recommended usa... Read MoreType Single 2 type Voltage (V) 1.5
- maxell Button-shaped Silver Oxide BatteryUses 0 (zero) mercury and lead! Leakage prevention design! Leakage resistance is more than twice that of LR button batteries! Stable device operation with gold coating (24K)! With liquid leakage compensation. * If misused, liquid may leak. * If the liquid leaks while observing the warnings and pr... Read MoreType Silver oxide Nominal Voltage (V) 1.55
- TOSHIBA Alkaline battery AAA sizeAlkaline batteries that have both long-lasting power and cost performance For equipment that requires continuous high output, such as digital cameras and work lights
- TOSHIBA Alkaline battery single 1 formAlkaline batteries that have both long-lasting power and cost performance For equipment that requires continuous high output, such as digital cameras and work lightsType Single 1 type Voltage (V) 1.5
- Panasonic Alkaline battery EVOLTA single 2 formDemonstrates high performance in all current ranges! You can experience longevity in various devices. The internal volume and strength are increased, and it lasts longer. The longest in the industry! Long-term storage with a recommended usage period of 10 years is possible! You can use it safely ... Read MoreType Single 2 type
- maxell Alkaline Battery AALong-lasting & power Compatible with various AA size devicesType AA Act on Promoting Green Procurement Conformity
- MonotaRO Manganese Dry Cell Batteries 9V SquareIt is suitable for use with table clocks, wall clocks, remote controls, etc. that are used for a long time with a small amount of power. Batteries may leak, overheat, explode, or cause injury or equipment failure depending on the usage pattern, usage environment, storage environment, etc., so be ... Read MoreType 9V type Voltage (V) 9
- MonotaRO Manganese Dry Cell Batteries AAIt is suitable for use with table clocks, wall clocks, remote controls, etc. that are used for a long time with a small amount of power. Batteries may leak, overheat, explode, or cause injury or equipment failure depending on the usage pattern, usage environment, storage environment, etc., so be ... Read MoreType AA Voltage (V) 1.5 Quantity per Set (pieces) 4 pieces
- Mitsubishi Electric Alkaline battery + EXD series + square 9VEvolved high power Further long-lasting enduranceType 9V type Voltage (V) 9 RoHS directive (corresponding to 10 substances) Correspondence
- maxell Alkaline battery voltage AACompensation for liquid leakage for 10 years from single 1 type to AAA type! Liquid leakage prevention design using patented zinc alloy. Long-lasting triple power of "instantaneous power", "large horsepower" and "endurance". Demonstrates its power in digital cameras,... Read MoreType AA Act on Promoting Green Procurement Conformity
- maxell Alkaline battery AAA sizeLong-lasting & power Compatible with various AAA size devicesType AAA type Act on Promoting Green Procurement Conformity
- Panasonic Alkaline Battery EVOLTANEO AAPanasonic's No. 1 longest lasting! By adopting titanium power, the reaction efficiency of the positive electrode is improved and excellent storage performance is realized! Adopted "Liquid leak prevention 2 manufacturing method Ag +" that reduces gas with the power of silver! * If th... Read More
- Panasonic Alkaline battery AA 12VIt has the same size and shape as AA batteries, but has a voltage of 12V. High power even if it is small! It is useful in various small devices. For keyless entry etc. Lighter / car remote controlMass (g) About 6.0 Type Single 5 form Voltage (V) 12 Quantity per Set (pieces) 1 piece
- MonotaRO Manganese Dry Cell Batteries DIt is suitable for use with table clocks, wall clocks, remote controls, etc. that are used for a long time with a small amount of power. Batteries may leak, overheat, explode, or cause injury or equipment failure depending on the usage pattern, usage environment, storage environment, etc., so be ... Read MoreType Single 1 type Voltage (V) 1.5 Quantity per Set (pieces) 2 pieces
- maxell Alkaline Battery Voltage AAACompensation for liquid leakage for 10 years from single 1 type to AAA type! Liquid leakage prevention design using patented zinc alloy. Long-lasting triple power of "instantaneous power", "large horsepower" and "endurance". Demonstrates its power in digital cameras,... Read MoreAct on Promoting Green Procurement Conformity