Weeding Tools
Weeding tools are used to cleanly remove weeds such as cultivated plants and growing flowers. Anything that can be easily removed to deep-rooted weeds can be inserted straight into the soil, so we can weed without damaging the plants being grown. The most suitable for gardens where jagged blades remove weeds and the type that hook-shaped blades pull out while loosening the soil can easily remove even weeds in narrow places that are difficult to remove such as flower beds and planting . We have a wide variety of weeding tools that can be selected according to the scale you are growing.
Other Related Pages
- Murakuni Neck torsion sickleFor weeding, weeding, and weed removalMass (g) 155 Blade Hardness HRC46 Material (Handle) Bleached oak Material (Blade) S50C
- HOUKEN KIHAN Mitsuyama's scissors weeding sickleYou can weed and weed by pulling, weeding near the wall by pushing, and weeding such as concrete gaps at the cutting edge, and you can do versatile weeding with this one. For weeding and weeding.Mass (g) 140 Material (Handle) Aluminum alloy Material (Blade) Stainless steel (SUS420)from S$29.99Min. 2 days
- ESCO 210x1350mm Grass hoeWith steel, it has excellent sharpness. With vinyl sack. For grass cutting and soil diggingMaterial Blade: cutlery steel, handle: wood Mass (g) 890from S$58.99Min. 3 days
- GISUKE (Takagi) Absolutely grassless weeding toolShave / Shave with a flat blade to weed. Collect with a side blade / Collect with a serrated blade Made of rust-resistant stainless steel For weed control
- Golden Star Long Pipe Handle Dirt Remover Stainless Steel Combined TypeSoil removal of agricultural machinery, weeding wrapped around. Also for collecting and weeding work. For soil removal work of agricultural machinery * Be careful when handling the blade.Mass (g) 325 Material (Handle) Steel pipe Material (Blade) Stainless knife steelfrom S$29.99Min. 4 days
- Ishiguro metal Boasting stainless steel weedingYou can cut the roots of weeds and weed. Easy weeding with a sharp cutting edge!Material (Main Unit) Stainless steel special Mass (g) 40 Material (Handle) Polypropylenefrom S$10.99Min. 7 days
- Doukan Weeding softly thick thick long patternThe tough weeds that take root have been gently removed! Above all, the long aluminum pipe handle allows you to work without bending your hips. Just pull lightly in a comfortable posture while standing. Convinced that the blade width is just right for weeding the kiwa of garden stones.Mass (g) 400 Replacement Blades DK-811K
- OWL Very light 3 corner ho with knurled holesIt's really light. Weight reduction by adopting holes. Uses an aluminum pattern. Excellent soil separation. For grass cutting, soil raising, grooving, and soil gathering.Material (Head) Iron, (Pattern) Aluminum handle Mass (g) About 900
- Doukan Kezutaro Aluminum HandleIt is about 25% lighter than the wooden handle. It is less likely to bend or corrode even when it gets wet with rain or water. The handle will not bend even if left outdoors. Weeding work of Une Aze Giwa is easy.Mass (g) 500 Replacement Blades DK-800K
- Doukan Mud otaThe blade is finished with thin steel. The bending edge can bite into the mud along the deep radius of the rotor cover and remove the hardened mud. OK even in a narrow place. Work efficiency is further improved by the curve of the cutting edge.
- COMPAL Ice split and spring built-inThe sturdy head crushes ice and snow. The built-in effect of the spring absorbs the impact and reduces the burden on the arms, shoulders and hips. The handle is a durable metal scraper type that is convenient for removing ice. For crushing frozen roads and compressed snow
- Murakuni Stainless Neck Long SickleFor weeding, weeding, and weed removalMass (g) 165 Blade Hardness HRC48 Material (Handle) Bleached oak Material (Blade) 420J3
- Hiraki shoji L blade for exclusive use of AigamonPlease use this L blade for paddy fields, flat ground, etc.Suitable Model Suisui Cutter Aigamon AG-001
- Golden Star Grass cuttingYou can work while standing An excellent product that can be used for mowing, mowing, weeding, rake and other functions. * Be careful when handling the blade.Mass (g) 630 Material (Handle) Aluminum pipe Material (Blade) Carbon cutting steel
- Doukan Paddy Rake Mizusuka Toreta BigAquatic plant Toreta with a large blade width. Weeds of people in need can be squeezed with a powerful saw blade!Mass (g) 450 Replacement Blades DK-818K
- OWL Karugaru Weaving Triangular Blade with SteelMass (g) 400 Blade Shape Triangular blade
- HOUKEN KIHAN Tractor Combine HarvesterA special blade with a scraper and a saw blade. Used for removing mud from tractors and cleaning combines.Material (Blade) Special stainless steel
- Chikichi Stainless Weed RemoverFor weeding work. For work on small parts. Stainless steel blade that does not rust easily. Weed removalMaterial (Blade) Stainless steel, (Pattern) Wood Mass (g) 100 Material (Blade) Stainless steel
- Hiraki shoji Paddy weeding machine Suisui cutter AigamonBy using the "Suisui Cutter Aigamon" and a special blade developed exclusively for it, you can perform mowing (grass mowing / weeding) work at any site. Removal of weeds generated between the rows of rice fields (plowing effect and removal of weed roots also prevent re-germination. It... Read MoreMass (g) 1050 (excluding cutting blade)
- Ishiguro metal Stainless steel combine sickleFor cleaning agricultural machinery such as combinesMass (g) 225
- Asaka Industrial Golden Elephant One-Handed Triangle Steel HoeThe cutting edge uses a composite material and is heat-treated to have excellent wear resistance and sharpness, and the blade can be sharpened. It is easy to use because it has blades on both sides, and it is convenient for weeding work on slopes. Grass cutting workMass (g) 300
- HONEN MIYAWAKI Stainless steel sickleShave the soil and remove the grass!
- GREEN ART Weeding with wooden handle leverEasy to rust with W-plated iron Extract weeds from rootsSpecification W chrome plating Mass (g) 145
- Ishiguro metal Weeding NippersFor weed removal in the lawn. Pick and pull out the roots! Easy to pick with less force! Made of stainless steel so it can be washed with water!Mass (g) 61 Material (Blade) Stainless steel special Material (Handle) Polypropylene
- Yu-Ho Triangle Ho LIdeal for digging up rooted soil and shaving grassMass (g) About 970
- TAKAGI Shark Hawky that can sweep wet leavesIt is strong and has a knurled blade, so you can sweep wet leaves, dirt and mud!Size S
- MIKI LOCOS Koshiraku Weeding BoyIndustry's first! Tough and tough design using Egg pipe! 1: You can easily weed while standing! 2: You can work without bending your back, so it doesn't put a strain on your back! For weeding fields, ridges, and ridges. For weeding around lawns and flower beds.Material Iron, PP Material (Blade) Iron
- Doukan Kezutaro Jumbo Aluminum handleIt is about 25% lighter than the wooden handle. It is less likely to bend or corrode even when it gets wet with rain or water. The handle will not bend even if left outdoors. Jumbo is used for large areas with high swells such as white onions.Mass (g) 600 Replacement Blades DK-802K
- Doukan Rice field rakeWith a small blade width, you can catch aquatic plants between stocks! Flat blades can be used for weeding fields and leveling soil.Mass (g) 430 Replacement Blades DK-816K
- TOMITA CUTLERY Weed brush Tongari typeIdeal for weed control work that grows in gaps such as concrete, asphalt, and paving stones.Mass (g) 56
- Yu-Ho Standing sickleIdeal for cutting grass by sliding the soil surfaceMass (g) About 900
- Golden Star Crescent-Shaped Twisted SickleIt is a slender grass shaving that is convenient even in small places. Mowing weeds on the ground. * Be careful when handling the blade.Mass (g) 196 Material (Handle) Natural wood Material (Blade) Carbon cutting steel
- TOMITA CUTLERY Weed brushIdeal for weed control work that grows in gaps such as concrete, asphalt, and paving stones.Material PP Mass (g) 58
- Doukan Kezutaro Spare BladeIncluded Accessories 2 screws Suitable Model DK-800
- Ishiguro metal Wooden Handle Chrome Weed PullerIdeal for removing weeds from lawns and flower beds. With a lever, you can easily pull out weeds. The chrome-plated finish prevents rust.Mass (g) 150 Material (Blade) Steel
- Doukan Weeding softly thick one handRoughly with sharp eyes. It also removes the hard weeds that hit the ground. A wooden handle with an angle and thickness created from the ease of gripping and weeding, for one hand.
- YOSHIOKA EDGE-TOOL WORKS Nekiri Root Cutting ToolOne shot of root cutting.Material Forging
Filter by categories