All Category

Measuring Instruments

Measuring equipment is a general term for tools that measure various numerical values related to farm work and harvest. In order to make better crops, we measure various things such as soil, moisture and temperature, aim to grow in the optimal environment and harvest at the best time. Specifically, a soil acid humidity meter that measures the pH and humidity of soil moisture, a maximum / minimum thermometer that can be used for temperature management and seen in botanical gardens, a rice wheat moisture meter, a grain moisture meter, and the like. Also included in the measuring equipment category are the appropriate cutting date judgment device that measures the optimal harvesting date based on the daily temperature and the rice grain fluoroscope that checks the state of polished rice and brown rice.
View : Grid List
Filter

Items 1 - 40 of 115

Set Ascending Direction
  1. Soba Moisture Meter
    Kett Electric Laboratory Soba Moisture Meter
    PM-630 is a specialized instrument for measuring buckwheat moisture and volume weight. In addition to general gen soba, the measurement targets include datan soba, datan soba rice, and datan soba powder of "datan soba" whose demand has been increasing in recent years. The sample does no... Read More
    Operating Temperature Range  0~40℃  Mass (kg)  1.3  Dimensions, Width W x Depth D x Height H (mm)  125×205×215  Sample Volume (mL)  240  Other Functions  Average, auto power off  Power Supply  Battery 1.5V (AA Alkaline) x 4  RoHS directive (corresponding to 10 substances)  Correspondence  Type of Display  Digital LCD  Measurement Method  High frequency capacity type (50MHz) 
    Rating:
    100%
    from S$1,499.00
    Min. 7 days
  2. Rice Grinder
    Kett Electric Laboratory Rice Grinder
    A test scraper that uses a spiral roll. It is a standard accessory of the rice and wheat moisture meter Lyster f because of its good rubbing performance and operability. After rubbing, the rice is separated into the "rice husk saucer" and the brown rice is separated into the "sampl... Read More
    Mass (kg)  0.28  Dimensions (H x W x D) (mm)  70/80×112/145×45  Mass of Sample (g)  About 8  RoHS directive (corresponding to 10 substances)  Correspondence 
    Rating:
    89%
    from S$89.99
    Min. 2 days
  3. Soil Moisture Meter Tension Meter
    Takemura Denki Seisakusho Soil Moisture Meter Tension Meter
    A pF meter using a vacuum gauge. You can find the appropriate irrigation time for the crop by referring to the pF value. The meter part of DM-8 and DM-8M can be attached and detached.
    Rating:
    87%
    from S$169.90
    Min. 2 days
  4. Soil Acid Humidity Meter
    Takemura Denki Seisakusho Soil Acid Humidity Meter
    Electromagnetic soil acidity measuring instrument. The pH in the soil can be measured simply by inserting it directly into the soil. No need for consumables such as chemicals and batteries.
    Mass (g)  155  Measuring Range  3.5~7pH  Specification  Humidity measurement is possible  Included Accessories  Portable soft case 
    Rating:
    97%
    from S$149.90
    Min. 2 days
  5. Rice Wheat Moisture Meter
    Kett Electric Laboratory Rice Wheat Moisture Meter
    The Lysta series is used by many inspection agencies. The Lysta f2 is a moisture meter suitable for the major changes in the rice and wheat inspection system in Japan, that is, the inspection of rice by so-called "private inspection organizations".
    Mass (kg)  0.44  Operating Temperature Range  0~40℃  Dimensions, Width W x Depth D x Height H (mm)  164×94×64.5  RoHS directive (corresponding to 10 substances)  Correspondence  Measurement Method  Electric resistance type 
    Rating:
    95%
    from S$599.90
    Min. 2 days
  6. Soil Acidity Meter
    Takemura Denki Seisakusho Soil Acidity Meter
    It is a soil acidity measuring machine that can measure the approximate soil acidity (pH 4 to pH 7) by inserting it directly into the soil. If the soil is dry, the proper pH value cannot be measured, so sprinkle a bucket of water and wait for about 20 to 30 minutes before measuring. Insert it dir... Read More
    Dimensions, Width W x Depth D x Height H (mm)  45×45×160  Measuring Range (pH)  4~7  Mass (g)  97 
    Rating:
    94%
    from S$58.99
    Min. 2 days
  7. Colorimetric pH tester
    Takemura Denki Seisakusho Colorimetric pH tester
    It is a pH tester (measurement range pH4.0 to pH10.0) viewed by color. The accuracy is comparable to that of a glass electrode pH meter. It is possible to measure by applying the reagent directly to the sample soil. Ideal for soil management and water management. For soil management and water man... Read More
    Mass (g)  135  Measuring Range  4.0~10.0pH 
    Rating:
    83%
    from S$47.99
    Min. 2 days
  8. Garden thermo
    EMPEX INSTRUMENTS Garden thermo
    Rust resistant with stainless steel plate, waterproof and dustproof The scale color below 0 ° C is different and easy to distinguish.
    Operating Temperature Range (℃)  -30~+60  Display Unit  1℃  Dimension (mm)  314×45×8  Mass (g)  About 110  Temperature Display  Bar scale  Type of Thermometer  Bar thermometer  RoHS directive (corresponding to 10 substances)  Correspondence  Mounting Type  Wall hanging 
    from S$25.99
    Min. 2 days
  9. Rice Grain Fluoroscopic Device
    Kett Electric Laboratory Rice Grain Fluoroscopic Device
    This is a rice grain fluoroscope made to accurately check the presence, degree, and mixing rate of split grains in a short time when inspecting the quality of brown rice. It is designed so that about 100 grains of ordinary brown rice are lined up in the red line frame on the glass plate. Furtherm... Read More
    Mass (kg)  0.1  Dimensions, Width W x Height H x Depth D (mm)  80×19×90  RoHS directive (corresponding to 10 substances)  Correspondence 
    Rating:
    100%
    from S$58.99
    Min. 2 days
  10. Rice wheat moisture meter
    Kett Electric Laboratory Rice wheat moisture meter
    The Lysta f was developed by incorporating the opinions and requests of many conventional machines. We reexamined the conventional device from every angle, improved the points to be improved, inherited the points to be inherited, and completed it as a lyster f. The focus of development was to imp... Read More
    Mass (kg)  0.44  Operating Temperature Range  0~40℃  Dimensions, Width W x Depth D x Height H (mm)  164×94×64.5  RoHS directive (corresponding to 10 substances)  Correspondence  Measurement Method  Electric resistance type 
    Rating:
    90%
    from S$699.90
    Min. 2 days
  11. Soil Acidity Meter
    Takemura Denki Seisakusho Soil Acidity Meter
    It is an electromotive type that is activated by hydrogen ions in the soil and operates according to the pointer. The pH in the soil can be measured simply by inserting it directly into the soil. DM-1 can be measured by inserting it into a container.
    Mass (g)  155  Included Accessories  Portable soft case  Size  Φ50×165mm 
    Rating:
    100%
    from S$139.90
    Min. 2 days
  12. Soft carton
    Kett Electric Laboratory Soft carton
    Cartons are used for quality inspection of agricultural products, and are also used for grain receipt inspection at rice milling factories and milling factories. The conventional carton is made of thermosetting resin such as melamine resin because it has excellent heat resistance and chemical res... Read More
    Material  Elastomer 
    Rating:
    100%
    from S$119.90
    Min. 2 days
  13. Soil Acid Humidity Meter
    Takemura Denki Seisakusho Soil Acid Humidity Meter
    You can measure the approximate acidity (pH 4 to pH 7) of the soil by inserting it directly into the soil. Humidity can be measured with a simple operation
    Mass (g)  135  Measuring Range  4~7pH 
    Rating:
    60%
    from S$88.99
    Min. 2 days
  14. Pocket type multi tester (pH / EC)
    Takemura Denki Seisakusho Pocket type multi tester (pH / EC)
    PH.EC. temperature can be measured with one unit. Select the measured area with the touch of a button. Large screen that is easy to see. Agriculture such as soil and hydroponics, landscaping, aquaculture, fish farming, hot springs, factories, printing, wastewater treatment, cooling towers, boiler... Read More
    Measuring Range (pH)  0.0~14.0  Measuring Range (℃)  0~50  Measuring Range (μS/cm)  EC:0~1999  Measuring Range (mS / cm)  EC:2.0~20.0  Accuracy  pH: ± 0.1, EC: ± 1% (full scale)  Resolution  pH:0.1pH、EC:1μS/cm、0.01mS/cm 
    from S$399.90
    Min. 2 days
  15. Salt water selection meter
    Shinwa Rules Salt water selection meter
    It is colored so that you can see at a glance the specific gravity that matches the type of seed. A salt water sorter that measures the concentration of salt water and uses it to sort seeds. * Do not use for any other purpose.
    Measuring Range  0-35 heavy baume degree  Mass (g)  11  Material  Body: Glass  1 Scale  Single Baume degree  Accuracy (℃)  ± 1 double degree  Dimension (mm)  Φ11×205 
    from S$35.99
    Min. 2 days
  16. Rubber stopper for tension meter DM-8M
    Takemura Denki Seisakusho Rubber stopper for tension meter DM-8M
    from S$14.99
    Min. 2 days
  17. Rice wheat moisture meter
    SATO KEIRYOKI MFG Rice wheat moisture meter
    The large LCD panel makes it easy to see the measurement results and is easy to operate. For brown rice, unhulled rice, barley and wheat ・Make measurements three times or more and find the average value. The instrument can output the average value up to 9 times.・When drying progresses and the f... Read More
    Resolution  0.1% (however, 30% or more is 1%)  Dimension (mm)  175×72×100  Mass (g)  480  Operating Temperature Range (℃)  5 to 40 (no condensation)  Power Supply  AA batteries x 4 (included)  Temperature compensation (℃)  Automatic correction formula  Target of Measurement  Brown rice (fir), barley, wheat  Accuracy  ±0.5%(10~20%) 
    from S$439.90
    Min. 2 days
  18. Soil Moisture Meter Tension Meter
    Takemura Denki Seisakusho Soil Moisture Meter Tension Meter
    You can read the values directly without having to calculate the numbers. The pottery cup can be easily replaced. Comes with a waterproof vinyl cover. With 10 cm and 20 cm scales on the stick, insert it into the soil according to the crop. The meter part can be attached and detached. You can chan... Read More
    Measuring Range  0.0~2.6pF  Embedding depth (mm)  130~200  Dimension (Φmm)  20 x 320, (Porous cup) 18  Mass (g)  210  unit dimention (cm)  For pots20 
    from S$169.90
    Min. 2 days
  19. Fir roll unit
    Kett Electric Laboratory Fir roll unit
    RoHS directive (corresponding to 10 substances)  Correspondence 
    Rating:
    40%
    from S$88.99
    Min. 2 days
  20. Grain moisture meter
    Kett Electric Laboratory Grain moisture meter
    It is an electric moisture meter / electric grain meter specified by the agricultural product inspection standard. It is also possible to measure the water content and volume weight of cereals that are not subject to inspection. As the measurement principle, we have adopted a "high frequency... Read More
    Operating Temperature Range (℃)  0~40  Mass (kg)  1.3  Dimensions, Width W x Depth D x Height H (mm)  125×205×215  Sample Volume (mL)  240  Function  Average, auto power off  Power Input (V)  Battery 1.5 (AA Alkaline) x 4  RoHS directive (corresponding to 10 substances)  Correspondence  Type of Display  Digital (LCD)  Measurement Method  High frequency capacity type (50MHz) 
    from S$2,399.00
    Min. 2 days
  21. Fir roll (2 pcs / set)
    Kett Electric Laboratory Fir roll (2 pcs / set)
    RoHS directive (corresponding to 10 substances)  Correspondence 
    from S$44.99
    Min. 8 days
  22. Rice grain fluoroscope
    Kett Electric Laboratory Rice grain fluoroscope
    TX-200 is a device for observing the appearance quality of polished rice and brown rice. Light is transmitted from the back of the sample, and the shape and color tone are observed. It also comes with a sample plate that can be rotated while checking the angle, and a magnifying lens. Moreover, si... Read More
    Suitable for  (Sample) Milled rice, Brown rice  Mass (kg)  0.47  Storage Temperature Range (℃)  0~40  Operating Temperature Range (℃)  10~40  Dimensions (H x W x D) (mm)  80×162×134  RoHS directive (corresponding to 10 substances)  Correspondence 
    from S$329.90
    Min. 5 days
  23. Crusher
    Kett Electric Laboratory Crusher
    If a large sample is dried as it is with an infrared moisture meter, not only will it take time to heat to the center, but the surface may be scorched and accurate measurements may not be possible. The TQ-100 is useful in such cases. It is a roll mill made for the purpose of crushing a sample for... Read More
    Mass (kg)  1.2  Dimensions (H x W x D) (mm)  180×80×70  Mass of Sample (g)  About 5  RoHS directive (corresponding to 10 substances)  Correspondence 
    Rating:
    80%
    from S$859.90
    Min. 7 days
  24. Rice Moisture Meter
    Kett Electric Laboratory Rice Moisture Meter
    In response to the demand for measuring the moisture content of foreign rice, Lysta f5 focused on measuring foreign brown rice and polished rice. In addition to domestic brown rice and polished rice, short-grain, medium-grain, and long-grain rice from each country can be measured. It is a moistur... Read More
    Mass (kg)  0.44  Operating Temperature Range  0~40℃  Dimensions, Width W x Depth D x Height H (mm)  164×94×64.5  RoHS directive (corresponding to 10 substances)  Correspondence  Measurement Method  Electric resistance type 
    Rating:
    100%
    from S$779.90
    Min. 5 days
  25. Pocket Type EC Meter (Sensor Replaceable, 3-Point Calibration, Small Cup Type)
    Takemura Denki Seisakusho Pocket Type EC Meter (Sensor Replaceable, 3-Point Calibration, Small Cup Type)
    Easy-to-read large screen display. 3 ranges. EC and temperature are displayed at the same time. Cup type sensor. Battery level display. Self-diagnosis function.
    Accuracy  ±1%  Temperature Display  0~50℃  Measuring Range (μS/cm)  0~200.0、0~2,000  Resolution  0.1μS/cm、1μS/cm、0.01m S/cm  Calibration  Auto or manual (up to 3 points)  Measuring Range (mS / cm)  0~20.00 
    from S$359.90
    Min. 6 days
  26. Sake rice moisture meter
    Kett Electric Laboratory Sake rice moisture meter
    There is a high correlation between the water content and water absorption of raw rice for sake brewing, and highly refined raw rice is required for high-quality koji brewing. Lysta f4 achieves low moisture measurement up to 8%. Compared to ordinary rice, low-moisture raw material for sake brewin... Read More
    Mass (kg)  0.44  Operating Temperature Range  0~40℃  Dimensions, Width W x Depth D x Height H (mm)  164×94×64.5  RoHS directive (corresponding to 10 substances)  Correspondence  Measurement Method  Electric resistance type 
    from S$899.90
    Min. 5 days
  27. Pocket EC Meter (Sensor Replaceable, 2-Point Calibration)
    Takemura Denki Seisakusho Pocket EC Meter (Sensor Replaceable, 2-Point Calibration)
    Easy-to-read large screen display. 2 ranges. EC and temperature are displayed at the same time. Battery level display. Self-diagnosis function.
    Accuracy  ±1%  Calibration  Auto or manual (up to 2 points)  Resolution  10μS/cm 、0.10m S/cm  Measuring Range (mS / cm)  0~20,00  Measuring Range (μS/cm)  0~2,000  Temperature Display  0~50℃ 
    from S$269.90
    Min. 6 days
  28. Tension meter
    Takemura Denki Seisakusho Tension meter
    With 2 outputs and analog monitor output. In addition to irrigation signals and warning signals, upper and lower limits of irrigation can be set. The analog monitor output can be connected to a data logger. Since it is displayed in kPa, it can measure from pF1.0 to 3.0. With conversion value tabl... Read More
    Operating humidity (% RH)  35~85  Operating Temperature Range (℃)  10~50  Accuracy  ±0.2%、F.S±1digit  Power Input (DC-V)  12~24  Measuring Range (kPa)  0~-101.3  Dimensions (cm)  31 x 31 x 26 (display)  Output Voltage (V)  (Analog monitor) 1-5  Output Impedance (Ω)  About 1K  Mass (g)  90 (display) 
    from S$589.90
    Min. 6 days
  29. Pocket pH meter
    Takemura Denki Seisakusho Pocket pH meter
    Ideal for hydroponics. Waterproof type, easy operation with one button for calibration and measurement. Only the main body is sold.
    Resolution (pH)  0.1  Measuring Range (pH)  1.0~14.0  Dimension (mm)  163×45×30  Calibration  3 points (4.0 / 7.0 / 10pH)  Power Input (V)  4×1.5(LR44)  Mass (g)  90  Temperature Compensation  Existence (automatic)  Accuracy (pH)  ±0.1 
    from S$199.90
    Min. 6 days
  30. Pocket pH meter
    Takemura Denki Seisakusho Pocket pH meter
    Easy-to-read large screen display. Push button calibration. Battery level display. Waterproof type, floats on water (waterproof IP67). The sensor can be replaced. Built-in ASIS (IC for specific applications). Hold function self-diagnosis message. Includes a "soil measurement kit" that e... Read More
    Calibration  3 points  Temperature Compensation  Existence (automatic)  Waterproof Specifications  IP67 
    from S$299.90
    Min. 6 days
  31. Rice wheat moisture meter
    Kett Electric Laboratory Rice wheat moisture meter
    It is a rice and wheat moisture meter designed to meet the needs of producers. Moisture of fir, brown rice and wheat can be obtained by simple operation. Since it is a sample crushing method, it is possible to measure the moisture more accurately even if there is a moisture difference between the... Read More
    Operating Temperature Range  0 to 40 ° C, 95% RH (No condensation)  Dimensions, Width W x Depth D x Height H (mm)  250×240×125  Mass (kg)  3.5  Power Supply  AC100V(50/60Hz)  RoHS directive (corresponding to 10 substances)  Correspondence  Measurement Method  Electric resistance type  Additional Functions  Test mode, LCD contrast adjustment  Power Consumption (W)  Up to 4.5 
    from S$1,999.00
    Min. 7 days
  32. Small rice mill
    Kett Electric Laboratory Small rice mill
    It is a small rice mill that you should use when inspecting the condition and degree of contamination of spotted rice (black spot rice) by stink bugs, burnt rice, split rice, colored rice, glutinous rice, and glutinous rice. The sample brown rice extracted for inspection is refined in a short tim... Read More
    Mass (kg)  1.7  Dimensions, Width W x Depth D x Height H (mm)  110×152×176  Power Input (V)  AC100~240(50/60Hz)  RoHS directive (corresponding to 10 substances)  Correspondence 
    from S$999.00
    Min. 5 days
  33. Pocket type multi tester (pH, EC, TDS, salinity)
    Takemura Denki Seisakusho Pocket type multi tester (pH, EC, TDS, salinity)
    PH.EC.TDS.Salt and temperature can be measured with one unit. Select the measurement area with the touch of a button. Large screen that is easy to see. Waterproof type, with ATC Agriculture such as soil and hydroponics, landscaping, aquaculture, fish farming, hot springs, factories, printing, was... Read More
    Measuring Range (pH)  0.00~14.00  Measuring Range (mS / cm)  EC:2.00~20.00  Measuring Range (μS/cm)  EC:0.0~199.9、200~1999 
    from S$479.90
    Min. 6 days
  34. Fir roll (2 pcs / set)
    Kett Electric Laboratory Fir roll (2 pcs / set)
    RoHS directive (corresponding to 10 substances)  Correspondence 
    from S$22.99
    Min. 8 days
  35. Appropriate cutting time judgment device
    Kett Electric Laboratory Appropriate cutting time judgment device
    The ripening of paddy rice is said to be the optimum time for harvesting, when the daily temperature is measured from the day of heading and the accumulated value reaches a peak of about 1000 ° C. Early harvesting of paddy rice has many immature grains, and late harvesting has a risk of cracking.... Read More
    Mass of Main Unit (kg)  0.15  Power Supply  Battery 9V (alkaline)  RoHS directive (corresponding to 10 substances)  Correspondence  Type of Display  Digital (LCD)  Target of Measurement  Integrated temperature in the field  Measurement Method  Temperature detection by thermistor 
    from S$869.90
    Min. 7 days
  36. Piercing pH meter
    Takemura Denki Seisakusho Piercing pH meter
    You can directly pierce and measure pH. PH measurement of soil, ham, cheese, kamaboko, fruits, etc.
    Resolution (pH)  0.01  Measuring Range (pH)  1.0~14.00  Calibration  3 points (USA / NIST can be selected)  Temperature Compensation  None (automatic)  Accuracy (pH)  ±0.01 
    from S$779.90
    Min. 6 days
  37. Soil direct type pH meter
    Takemura Denki Seisakusho Soil direct type pH meter
    Easy-to-read large screen display. Push button calibration. Measured value hold function. Auto OFF function. Waterproof type (IP67). The sensor can be replaced. PH can be measured by piercing the soil directly.
    Resolution (pH)  0.01  Measuring Range (pH)  1.00~13.00  Calibration  3 points (USA / NIST can be selected)  Temperature Display  None  Temperature Compensation  None (automatic)  Accuracy (pH)  ±0.1 
    from S$799.90
    Min. 6 days
  38. Grass moisture meter
    Kett Electric Laboratory Grass moisture meter
    The HX-700 is a grass moisture meter that applies electrical resistance, and displays the moisture (%) by simply inserting a rod-shaped sensor into the grass that is being dried or stored. Insufficient drying during pasture storage causes fermentation rot, and overdrying leads to quality deterior... Read More
    Mass (kg)  0.5  Operating Temperature Range  0~40℃  Dimensions, Width W x Depth D x Height H (mm)  110×210×50  Measuring Range  8~30%  Power Supply  Battery 1.5V (AA Alkaline) x 6  RoHS directive (corresponding to 10 substances)  Correspondence  Measurement Method  Electric resistance type  Target of Measurement  Pasture 
    Rating:
    20%
    from S$1,699.00
    Min. 7 days
  39. Pocket EC / TDS / Salt & Tester
    Takemura Denki Seisakusho Pocket EC / TDS / Salt & Tester
    EC (conductivity) / TDS / salinity is displayed at the same time as the temperature. The standard solution is automatically recognized and can be easily calibrated with a one-push button operation. (Within calibration range) The TDS coefficient can be set according to the object to be measured. A... Read More
    Temperature compensation (℃)  Yes (automatic)  Power Input (V)  LR44(1.5)×4  Temperature Resolution (℃)  0.1/(0.1°F)  Temperature Measurement Range (℃)  0~50(32~122.0°F)  Temperature Accuracy  ±0.5℃(±0.9°F)±1LSD  Calibration  (Salinity) 1 point / manual  Dimensions (cm)  17×4.5×3  Operating Temperature (℃)  5~45  Measuring Range (mS / cm)  (Conductivity) 0.00-20.00 
    from S$229.90
    Min. 6 days
View : Grid List
Filter

Items 1 - 40 of 115

Set Ascending Direction