Construction Ground Related
Civil engineering-related tools are tools that are larger than shovels used to scoop and mix soil and sand, or to dig holes. Used for construction site work, landscaping, horticulture, agriculture, etc. It is characterized by rust-resistant aluminum and wood that is familiar to the hand. A concrete excavator suitable for mixing concrete, and a willow blade that is suitable for work in confined spaces where it is difficult to access. There are long handles that come in handy when bending reinforcing bars and wires.
Other Related Pages
- Asaka Industrial W spiral hole digging"Presser plate" Compresses and holds the soil firmly. Reduces soil collapse during pulling. "Double spiral blade" Two spiral blades dig into the soil to improve work efficiency. The wall surface of the "two vertical cutting blades" holes can be scraped off, making it... Read MoreMaterial Steel Finish Melamine resin baking finish
- Kanaguchi Seisakusho Landmaster (Hand)The most common hand hook product. It can be used for cargo handling work at any site. Each nail is a handmade forged product, so it has a tough finish. The grip uses yew oak from the Kyushu area, which is durable and can be used in harsh environments. The shape is easy to wrap in your hand, so y... Read MoreMaterial (Nail) S55C, (Pattern) Yew
- Mokuba BarbenderThe curved plate and curved rod are integrated, and the bender has a roll, so it can be bent easily. Bending work for iron wires, deformed reinforcing bars, etc.Mass (g) 2620
- RIDGID (Emerson Japan) 170 Long Handle Round Point ShovelType Round type Material Cutting edge: Steel, Handle: ashfrom S$139.90Min. 4 days
- TOMBO All stainless excavator concreteSince the cutting edge and handle are made of stainless steel (SUS304), it does not rust easily and there is little soil adhesion, so it is easy to clean. Excellent corrosion resistance, ideal for dairy, livestock, coastal areas, etc.Cutting Edge Shape Small mixed typefrom S$139.90Min. 3 days
- HIT Up type rebar cutter with universal benderReinforcing bars up to 13 mm can be cut and bent. When bending, the handle direction is from bottom to top. For cutting and bending reinforcing bars.Mass (g) 10500from S$559.90Min. 3 days
- ENERPAC Enapak manual cutter with built-in hydraulic pumpIt is a single-acting spring return type. It has a built-in hydraulic pump. Easy to operate with guillotine cutting. The receiving blade side can be opened with a simple operation. * Please read the instruction manual for safety when using.Material Steel Maximum Operating Pressure (MPa) 70from S$2,999.00Min. 32 days
- K/H Silicon remover with scraperYou can remove old caulking that has adhered to tiles, etc. High quality and excellent design. It has a scraper on the other side. For caulking removal work.Material Body: ABS resin, tip: stainless steel Mass (g) 75 2018 Trusco page 7 0055from S$33.99Min. 3 days
- BAHCO Non-sparking round shovelA non-magnetic, corrosion-resistant tool that does not scatter sparks. Manufactured according to international standards DIN and ISO. Certified by BAM (German Federal Materials Laboratory).Material Aluminum bronzefrom S$499.90Min. 4 days
- MonotaRO Pipe pattern excavatorIt can be used for various construction work, civil engineering, pavement, landscaping, agriculture, horticulture, etc. A standard type suitable for digging and scooping work. Water, electricity, gas construction, civil engineering, landscaping, etc. * Please do not use for any other purpose. * D... Read MoreMaterial (Handle) Steel pipe Material (Head) Iron (50Mn)
- MonotaRO Aluminum scoopMade of aluminum, it is light and does not rust. It can be used in various places such as snow removal, dairy farming, and livestock farming. Snow removal, dairy farming, livestock farming, etc. * Please do not use for any other purpose. * Do not use if there is something wrong with the tip, hand... Read MoreMaterial (Handle) Birch Material (Head) Aluminum
- Aka-Kanecho Medium coatingA wide range of irons from intermediate coating to rough finishing. Ideal for scooping wall material and spreading it flat on the wall. Intermediate coating work to apply the material to the baseMaterial (Steel board) iron, (pattern) wood
- MonotaRO Wooden handle excavatorIt can be used for various construction work, civil engineering, pavement, landscaping, agriculture, horticulture, etc. A standard type suitable for digging and scooping work. Also, because it has a wooden pattern, the more you use it, the more it fits in your hand. Water, electricity, gas constr... Read MoreMaterial (Handle) Oak Material (Head) Iron (50Mn)
- Asaka Industrial Golden Elephant ShovelThis quality that you can understand if you use it. Reliable brand gold elephant seal. The gold statue excavator, which has the oldest history in the industry, is an excellent product whose quality has been recognized by professionals.
- MonotaRO Excavator portableVersatile mobile excavator that can be stored, convenient as an in-vehicle mobile phone, can be used as an excavator, hoe, pick Used for camping, outdoor activities, digging holes in home gardening, etc. * Do not use for any other purpose. * Wear gloves when using and be careful not to get your h... Read MoreIncluded Accessories Storage bag Material (Handle) Steel pipe Material (Head) Iron (50Mn)
- MonotaRO Shovel All Stainless Steel SUS201Made of stainless steel, it is ideal for use in scenes where rust is disliked. In dairy, livestock, coastal areas, etc. where rust is disliked. * Please do not use for purposes other than the original purpose. * Do not use if there is something wrong with the tip, handle, or handle. * Be careful ... Read MoreMaterial Stainless steel (SUS201) Tip Shape Square
- MonotaRO Post hole diggersA compound excavator for digging vertical holes. Lightweight type with a fiberglass handle. For pilot hole digging work, digging work in narrow places * Do not use for anything other than its intended purposeMaterial Head: Iron (50Mn) Hole Diameter (Φmm) 120 Material (Handle) Fiberglass
- Aka-Kanecho Stainless Steel Intermediate Coat TrowelMade of stainless steel that is easy to clean and rust resistant. Since the surface of the iron plate is mirror-finished, dirt is easily removed and it is easy to clean. Ideal for Senyi walls and quick-drying cement. Intermediate coating work to apply the material to the base.
- Ohsho (Susa Seisakusho) Handhoe (Stainless Steel Plasterer)It can be used for kneading wall materials, cleaning field soil moats, and side ditches. Uses a color coated pipe.RoHS directive (corresponding to 10 substances) Correspondence
- KINBOSHI American RakeUsed for mowing grass collection work Ideal for cutting grass and collecting strawMass (g) 1200
- Asaka Industrial Golden Elephant Concrete ShovelSpecification JIS standard product Material (Handle) Steel Material (Head) Steel
- Midori Kanecho New Mortar Gote ProThe one-piece molding that does not rattle and the handle does not come off has a long life that is more than 10 times that of wooden iron. The finish of the coating is made so that the dotted groove on the back surface is hooked from the center to the left and right during use, so unevenness on ... Read MoreMaterial (Body) Plastic, (Pattern) Wood
- MonotaRO Mizobori excavatorSince the head is thinner than a normal excavator, it is ideal for working in narrow spaces and digging narrow grooves and holes. Buried work for water pipes, gas pipes, digging, etc. * Do not use for anything other than its intended purposeMaterial Iron (50Mn)
- Ishii Tools Mfg. Nuripita plusMortar iron. Abrasion resistance is about 10 times that of wooden iron. The material has excellent impact resistance and elasticity. It has the same usability (feel) as Japanese cypress wood. After use, the mortar residue accumulated in the groove and the dirt on the main body can be easily remov... Read More
- Aka-Kanecho Willow bladeA willow blade trowel that can be used for a wide range of purposes. Ideal for hard-to-reach places and plastering. Applying work to hard-to-reach places
- MonotaRO Pipe pattern mini excavatorIt can be used for various construction work, civil engineering, pavement, landscaping, agriculture, horticulture, etc. Compact type that can be widely used. Suitable for cleaning small and narrow places. Water, electricity, gas construction, civil engineering, landscaping, etc. * Please do not u... Read MoreMaterial (Handle) Steel pipe Material (Head) Iron (50Mn)
- Midori Kanecho Stainless Steel Finishing Trowel 0.3It is a hard random adhesive that does not allow the back metal to be removed. Since there is no caulking part, there are no scratches on the iron plate. It can be washed with thinner (organic solvent). It can also be used for diatomaceous earth. Finishing work for mortar walls and Seni walls
- KANESHIKA Fukuju Stainless KakuenDifferent flexibility, different backing, different strength, easy to apply, stable usability !! Proof of popularity with abundant achievements and evaluation. Achieves natural "bending" not only at the tip but also on the entire surface The smooth bending of the back metal makes it eas... Read MoreMaterial Stainless steel
- COMPAL CalscoA light and durable snow shovel that uses an aluminum pipe for the handle and polyethylene for the plate. For snow removal workMaterial Polyethylene
- Aka-Kanecho HiramejiIdeal for painting small parts such as bricks and tile joints. Please choose a joint trowel according to the tile joint. Coating and finishing work on joints and small areas * Please use the iron that suits your work location. * Do not use if the handle or iron is loose. * Please wash the used to... Read More
- MonotaRO Shovel Pipe Pattern PerforatedIt can be used for various construction works, civil engineering, pavement, landscaping, agriculture, horticulture, etc. Good soil separation! Work efficiency improvement Water, electricity, gas construction, civil engineering, landscaping, etc. * Although it is shown in black in the RB13 catalog... Read MoreMaterial (Handle) Steel pipe Material (Head) Iron (50Mn)
- Tomosada Kenki N Type Handy Grout InjectorIt is also safe to look up with a pair of measures to prevent spills from leaking to your hand. It can be operated quickly and accurately, and has a beautiful finish. You can choose the tip shape according to the construction site. Filling the gap with mortar (injection-press fitting). Filling wi... Read MoreOuter Diameter (Φmm) 61 (cylindrical)