Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Home belt wrench

Home belt wrench
Sales Price: -
Review Rating: 4.00
5 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Use it when screwing lid of big bottle does not open.
5
From Japan
On 2016-05-03 13:46:33
This is rarely used, but there is once, it is really helpful when it comes to time.
This review is about item#03343085.
Lid opening of bottled products in cold season
4
From Japan
On 2016-01-06 19:04:03
Since purchasing, there was not much time to use it, but the other day I used it for opening the lid of the homemade jam bottle. I slid a bit because the rubber was hardened, but I got wet a little, I could open it without any difficulty. I think that it will be few, but when it is called Isa, it is useful. Although it is good if the change of rubber is sold separately, since it is cheap unit price, is it also impossible?
This review is about item#03343085.
Overhaul of two wheel maintenance front fork
1
From Japan
On 2012-08-27 11:20:36
Used to loosen the outer nut of the fork without scratching. However, the belt broke from the root at one shot. After all it got a bruise but relaxed with a PYREN. I gave up on whether there was a problem with how to use it.
This review is about item#03343085.
Lid opening, oil filter wrench instead
5
From Japan
On 2012-06-06 23:28:11
Although it is also utilized for lid opening which is the original use purpose, it can be used sufficiently as a wrench of an oil filter. If you wipe off the oil stain of the belt and the filter well, it will hardly cause slippage. Although it did not slip by only the example of a long-term negligent vehicle, even if we tried to force strongly the force of the filter case as the case of the filter deforms at the root of the grip, things which the case deforms and does not do Yes, only at that time I removed it with 3 filtering wrench of 3 Peaks Giken (there is a similar thing even in Aemon) but I need to remove it premisedly to fix the case so severely As long as it is not a filter or a car with a restricted work space, most of the car models are sufficient for this one. However, when used in place of a filter wrench, the grip gradually becomes dirty with oil, so it would be better if you bought two from the beginning in case you use it as a lid opening.
This review is about item#03343085.
Lid opening
5
From Japan
On 2012-01-16 16:34:48
It is the strongest for opening the bottle lid. If the main body enters, it seems to be used also for removing motorcycle and car oil filter.
This review is about item#03343085.
1
Customer Who Viewed This Item Also Viewed
Belt Wrench
Strap wrench
Strap wrench
Bungee Cord
Strap wrench
Strap Wrench