Buy more than* S$200* and get FREE SHIPPING

* Announcement of Payment Method Change *
Credit card payment is now available via Paypal platform.
Paypal account is not essential.
In addition to Visa and MasterCard, American Express, and Discover are also available now.
(Availability of each brand in your country follows PayPal policy)

Customer Reviews of Steel Wire Brush

Steel Wire Brush
Sales Price: 2.19 SGD
Review Rating: 2.25
4 Customer Reviews
5 star 1
4 star 0
3 star 0
2 star 1
1 star 2
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Screw thread cleaning
1
From Japan
On 2018-03-14 15:24:57
Brass brush is soft. It can not be helped because it can not be purchased directly by looking at products. This time it was not suitable for use.
This review is about item#6151792.
Rust removal for iron fence painting
2
From Japan
On 2017-04-27 19:16:34
The wire is thin and soft. Depending on the application, it may be good, but it was not suitable for this work.
This review is about item#6151783.
I bought it as a cleaning brush dedicated to kitchen gas stove.
1
From Japan
On 2014-10-07 14:01:47
I wanted a wire brush which can be rinsed and did not rust, I chose stainless steel, I chose this product with a wire thickness of 0.2 mm with hardness not damaging the equipment of gas stove, but the actual thickness is 0.3 mm and hard It was too usable. If it was 0.2mm, it was not a problem but it is a pity that there is a mistake in the important part.
This review is about item#06151817.
Rusting off
5
From Japan
On 2013-12-02 19:29:29
I used it for rust removal which is not so badly attached to the water pipe and gas pipe. I felt a bit weak but I thought it was enough for light rust. This price is not in the home center.
This review is about item#06151792.
1
Customer Who Viewed This Item Also Viewed
Wire Brush
Wire Brush
Wire Brush
Wire Brush
Wire Brush Wave