Buy more than* S$200* and get FREE SHIPPING

* Announcement of Payment Method Change *
Credit card payment is now available via Paypal platform.
Paypal account is not essential.
In addition to Visa and MasterCard, American Express, and Discover are also available now.
(Availability of each brand in your country follows PayPal policy)

Customer Reviews of Model Robe -Nitril Model- Oilproof Thin Arm Cover - No.360

Model Robe -Nitril Model- Oilproof Thin Arm Cover - No.360
Sales Price: 11.99 SGD
Review Rating: 3.73
11 Customer Reviews
5 star 3
4 star 4
3 star 2
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Food manufacturing
4
From Japan
On 2018-11-06 17:27:15
It is good as it can hide up to the arm because it puts the middle of the water in tofu making. It is easier to work if the gloves are thinner a little more
This review is about item#48967301.
Used for occasion cleaning work
4
From Japan
On 2018-10-09 03:18:34
I used it for about two hours a day for 3 months, I liked that it does not get in the way of thin fingertips, but because of a small crack, it was torn at a stroke from that part, because it is inexpensive It can be convinced if it considers it as expendable items of regular replacement.
This review is about item#48967301.
When pickling
3
From Japan
On 2017-05-24 08:50:05
As clerical work, we use this glove for about 2 days a week all day, using stainless steel soaked in acid and use it to lift the product from about 50 cm depth and wash in hot water. Since the partner is metal, it can not be used because the tear of the needle hole can be made at the fingertip. (Others are okay at all) Why do I have to tear one of them and turn it over and use one side. Although it is saved if there is sale of two on one side.
This review is about item#48967301.
During milking
5
From Japan
On 2017-04-20 15:39:04
I think that the cuffs will not get wet so I am quite durable because I have a hand. It is hard to tear in the winter as the handed part is so soft. I found it at the home center but I am saved because it arrives as soon as it is monotaro but without it when I want it.
This review is about item#48967301.
I use it in the kitchen wash. The part of the rubber glove is thin, it is long to the shoulder mouth and covers the shopolitan arm so it is very easy to use and it is handy. I ordered only one on trial, but it was good so I will repeat!
4
From Japan
On 2017-04-17 21:12:20
The water gathers in the rubber glove why it is using, so if you remove the gloves and put your hands in again, it is bothersome! Is it a difficult point ...? It is!
This review is about item#48967317.
Washing
4
From Japan
On 2016-05-07 09:12:06
I think that it is good for washing small parts because the hand is thin.
This review is about item#48967317.
cleaning
2
From Japan
On 2015-04-15 14:49:37
Even L size feels small for men. The part of the arm was torn easily and it was torn by one specification. It is good that it is a little more durable, but it may be useless because it is thinner.
This review is about item#48967292.
During oil work
5
From Japan
On 2015-03-09 10:05:42
We are using it during oil operation. I have purchased it several times, but there is no problem. I hope the price is a bit cheaper. I wish I could introduce equivalent products.
This review is about item#48967292.
Fishing in the pond. Network up.
2
From Japan
On 2014-11-04 23:52:38
The glove part is too thin and I feel cold when dealing with water at the current time. It is cold in winter and can not be used. Suitable for summer and light work.
This review is about item#48967292.
Machine work
5
From Japan
On 2014-05-08 09:06:38
I use it in machining using oil. I can steam with sweat, but it is good that clothes sleeves are not stained with oil. It can be used many times, it is cheap and saved.
This review is about item#07613146.
When putting in hot pack
3
From Japan
On 2013-03-04 12:00:39
very convenient.
This review is about item#07613137.
1