Buy more than* S$200* and get FREE SHIPPING
Note
Due to Japanese national holidays as Golden Week, we will close 2019/4/27~2019/5/6 JST.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Slender Torsion Bit

Slender Torsion Bit
Sales Price: 22.99 SGD
Review Rating: 3.67
3 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Screw fastening
1
From Japan
On 2015-12-17 16:23:42
It is easy for the bit to deviate from the impact power. If the central part is too thin to give a shock, the shaft will be out of order and run out, it is not suitable for full-scale work.
This review is about item#10047195.
Carpentry work
5
From Japan
On 2013-05-18 08:19:00
The tip of the bit is thin, so the screw head is good. As the torque escapes moderately and there is a stickiness of the steel as it is, it is not first to say that the bit tip is flying or chipping. Work can be done very efficiently.
This review is about item#10047195.
Construction and civil engineering work
5
From Japan
On 2010-04-22 10:50:37
I used a lot of kinds of bits since the impact driver came out to this world, but for me personally it is a conson item for now. Again, in order to absorb wasteful impact at the slender part, the probability that the tip of the bit will be damaged will be lower. Ukeyeo ♪ Cono product is not a replacement because it lacks a bit like other products, but a bit As the mountain of the mountain decreases or becomes rounded, there is a danger of crushing the thread, so it was much more expensive to say that it will be replaced. In other words, the use time per one becomes longer, and even a slightly higher price will obviously decrease if you compare the number used annually. It is cost reduction somewhat meaning ♪ I have less time and labor to replace ... Since the tip part of the bit is also thin, it is also a good point to say that it is easy to fit the thread. I do not feel like using anything else now. Moreover, it is safe to say that it is the manufacturer's item of vessel. Again it seems that the material is better than any other shape.
This review is about item#10047186.
1
Customer Who Viewed This Item Also Viewed
12.7sq12 Angle Socket
True Torsion Bits
Torsion Bits
Advanced Slim Bits
19.0sq Short Socket
Slender torsion bit ST14
Slender bit AS14
Slim Torsion Bit
Tip slim bit
Cushion Bit
Slender Torsion Bit Belt
Torsion Bits
Slim Torsion Bit