Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of General Purpose Double Sided Tape 15M

General Purpose Double Sided Tape 15M
Sales Price: 2.79 SGD
Review Rating: 4.33
3 Customer Reviews
5 star 2
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
For attaching various oversized nameplates and others
5
From Japan
On 2016-02-24 15:38:18
The winding length may be short, but I want wide width
This review is about item#08399596.
Ring processing
3
From Japan
On 2013-04-12 15:09:48
· Since this double-sided tape was searching for a thing with a width of 100 mm this time, I bought it. At present I thought that it would be done with a compass cutter immediately after delivery, because I used it to paste parts of the ring, but I noticed that the protective seal was stuck on only one side, I thought that waste was thought However, it stuck to the underlay to the length you wanted to cut, pasted again from the top, peeled off together with the under protective material and processed. I managed to use it with confidence because it somehow became a protective seal on both sides. · It would be nice if there is a seal on A4 size, which is protected on both sides.
This review is about item#08399596.
Construction work
5
From Japan
On 2013-03-05 23:23:17
Early adhesion is also good, easy to use. The thickness is also thin, and it is good that the influence does not come out easily to the finish. It was easy to use.
This review is about item#08399666.
1
Customer Who Viewed This Item Also Viewed
Double-Sided Tape No.500
Double Sided Tapes
Easy Chain Series E16
Thin Work Gloves