Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of 3 steps of aluminum alloy step

3 steps of aluminum alloy step
Sales Price: 58.99 SGD
Review Rating: 5.00
5 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Putting in and out of things at high places, putting in and out of top bags and cabinets, changing ceiling lights, etc.
5
From Japan
On 2019-10-25 16:04:55
I bought it because the plastic part of the two-step platform that I had used so far was cracked, but until now it was cheap at the home center, but it was very solid and there was also a sense of stability I like it very much.
This review is about item#8296391.
Storage on a shelf
5
From Japan
On 2019-05-30 17:10:23
I bought a solid item with a load capacity of up to 100 kg. You can now safely lift and lower the package.
This review is about item#8296434.
Inspection work
5
From Japan
On 2017-04-05 10:35:18
I was looking for something that was not heavy and strong. I can use with confidence even if it is heavy with a nominal maximum use weight of 100 kg. There is almost no backlash and yore, folding is also smooth and comfortable to use. I think that the included leg cover also gets firmly attached and will not fall off even if it lifts up. I only want covers more.
This review is about item#8296407.
For high work
5
From Japan
On 2017-03-27 09:00:08
The stepping stone is solid, it is excellent in stability, even if it rides it is well-balanced and easy to use
This review is about item#8296407.
Communication work bench
5
From Japan
On 2013-12-02 20:25:38
I am satisfied that it has firm socks and foot socks
This review is about item#08296407.
1
Customer Who Viewed This Item Also Viewed
Professional Stepladder