Customer Reviews of Booster Cables ML
The reviews are automatic translation.
Showing 1 - 20 of 21 Reviews
At the time of the bucket

From Japan
On 2018-03-05 15:46:07
Although it is a cheap commodity, is not it easy to use even for people who are not familiar with written direction of connection etc.?
It would be better for you to make a storage bag a little more decent!
This review is about item#9918614.
General car maintenance

From Japan
On 2018-02-21 16:43:09
I am satisfied with the product. It is awesome if the insulation cover is attached to the outside of the alligator mouth.
This review is about item#38093675.
As an engine starting cable

From Japan
On 2018-02-19 11:39:31
Compared to other classes of the same class, the jaws of the clip are solid, and the cable is solid. It is a commodity which is also satisfactory in price.
This review is about item#38093675.
Maintenance, breakdown

From Japan
On 2017-12-15 14:16:02
I am saved very much with a solid product. Explanation is also polite and easy to understand
This review is about item#38093675.
Car stationary items

From Japan
On 2017-05-25 14:50:26
Purchase for the time of emergency. I am thankful as a standing item as it is bulky.
This review is about item#9988587.
Used and rented with battery

From Japan
On 2017-03-30 18:24:08
It is good to make and there is also the thickness of the cable, so I think the current flow is good.
This review is about item#38093684.
Battery jumping.

From Japan
On 2017-01-20 16:28:20
At the end of the year the battery of the car in the garage rose, I bought it for charging for jumping from the outside. After all, it seems that the battery was completely dead, it was not able to charge and I am indebted to purchase the battery.
This review is about item#38093684.
Battery raising

From Japan
On 2016-12-08 14:56:18
Although it is not used yet, it is an item that seems to be in a small case and has a cover on the clip part.
This review is about item#38093641.
For cars

From Japan
On 2016-04-25 10:33:05
It is cheap and sufficient.
This review is about item#38093641.
Used when the family car's battery goes up.

From Japan
On 2015-10-19 20:13:42
It was OK.
This review is about item#38093641.
Jumping start

From Japan
On 2015-03-23 22:22:28
Waniguchi was also solid, and even 4 ton cars could be used normally.
This review is about item#38093675.
In-car set items

From Japan
On 2015-02-12 23:02:59
Previously I had 3 meters, but it would be better if you had 5 meters.
This review is about item#38093666.
On-board tool

From Japan
On 2014-08-29 10:08:37
It is contained in a special bag and it is good for storage and carrying.
This review is about item#38093666.
Emergency portable use

From Japan
On 2014-07-07 14:00:08
I purchased it for portable use as a measure to raise the battery. I am planning to prepare for the trunk room. I saved it because it is stored in a special package. The cable connection method is also posted and it is easy to use even for beginners.
This review is about item#38093657.
Wire for electric wire transfer

From Japan
On 2014-06-03 19:47:12
I think that it is a solid product. I use it as a wire when I move the battery. I think that it is better to be lighter than copper wire at CCA.
This review is about item#38093675.
For charging

From Japan
On 2014-05-01 14:07:59
It is good that you can keep it as it is transparent. It is also good to be usable from light to large cars
This review is about item#38093675.
When the car battery goes up

From Japan
On 2014-03-30 11:01:06
The procedure is affixed to the cable itself, which is very easy to understand. That's a wonderful idea.
This review is about item#38093641.
Because I wanted to have one.

From Japan
On 2014-03-11 22:15:54
For the emergency of the battery, I bought it because I wanted to have it.
This review is about item#38093693.
During maintenance

From Japan
On 2013-11-01 13:09:43
The product was good, but the opening and closing part of the vinyl bag was broken.
This review is about item#38093666.
In case of emergency

From Japan
On 2013-01-24 17:06:05
If it is a car whose battery has completely gone up, I was in trouble because the cell did not rotate at all with the cable of 50 A place which I used up to now, but it seems to be able to put on if it is as thick as this much.
This review is about item#38093675.