Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Maximum Minimum Thermometer, Alarm

Maximum Minimum Thermometer, Alarm
Sales Price: -
Review Rating: 4.20
5 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
As an alarm when abnormal stop of commercial refrigerator
5
From Japan
On 2016-08-25 19:40:33
Usually, even when the business refrigerator malfunctions, the alarm sounds but why the other day? Breaker fell, losing all the power supply Naturally the alarm did not ring and it came to notice about 1 hour or so It was nearly wastefully discarding all of the products, so I was looking for something with a different power source and looking for alarmed items in the net I found the product and installed it quickly, the sensor which was a little worried can also hear the alarm volume firmly without an existing temperature sensor and error. Because there are many opening and closing in the daytime, the alarm switch is put in only at night. Since I am installing it, I am counting on it while expecting durability performance.
This review is about item#33192214.
Indoor thermometer
2
From Japan
On 2016-08-15 22:33:41
I was sorry that the following numbers are not displayed
This review is about item#33192214.
Water temperature control
4
From Japan
On 2013-11-13 20:08:04
I think that the necessary functions are provided, and the operation is simple and I think that it is good. The following dissatisfaction points are listed below (in order I want individual improvement). · Alarm sound is small (It is a plus if volume control function is available.) · I want you to make the outside air temperature sensor completely waterproof (now waterproofed and always in use underwater) · Simultaneous indication of inside and outside temperature (This is indispensable There is no thermometer with an alarm, although it is close to hope while choices are small, I think that the current price setting will be satisfactory if the above points are improved.
This review is about item#33192214.
Temperature control of tropical fish
5
From Japan
On 2013-10-23 13:14:46
Tropical fish thermos and heaters may fail when used for a long time, and it is valuable as an alarm in that case. However, it is meaningless unless it can withstand long-term use than thermo or heater.
This review is about item#33192214.
Thermal management of stadium space
5
From Japan
On 2013-07-23 18:08:46
Many items close to 10,000 yen may be classified as low price, but the LO HI setting of the alarm was also easy. The size is the same as the timer attached to the refrigerator, and I am satisfied not to take space.
This review is about item#33192214.
1
Customer Who Viewed This Item Also Viewed
Thermometer
Digital Thermometer
Digital Thermometer
Digital Thermometer Pc-9400
Max Min Thermometer
Digital Thermo Hygrometer
Digital Thermometer
Highest and Lowest Thermometer
Refrigerator Thermometer