Buy more than* S$200* and get FREE SHIPPING
Note
Due to Japanese national holidays, we will close 2018/12/29~2019/1/3 JST.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Metal Hand Lever Shear, Brake Cutter

Metal Hand Lever Shear, Brake Cutter
Sales Price: 329.99 SGD
Review Rating: 3.63
30 Customer Reviews
5 star 14
4 star 3
3 star 4
2 star 6
1 star 3
The reviews are automatic translation.
Showing 1 - 20 of 30 Reviews
Cutting of metal
3
From Japan
On 2018-11-20 15:19:31
I bought it twice during 4 or 5 years, but the spring has broken twice. I inquired, but I do not seem to be able to purchase only springs. It is a pity that the quality of the thing itself is good and the other parts are fine. I would be happy if you could purchase only springs.
Metal plate cutting
5
From Japan
On 2018-11-19 12:18:30
Working alone may be a little difficult (two holders and pressers required). Although it is possible for one person to use a vice etc. to prevent the metal plate from moving, wearing out is troublesome. If you do not need precision you do not mind holding down.
This review is about item#34906347.
Cutting of insulation building material
5
From Japan
On 2018-09-05 14:50:31
Sharpness is good, the blade is also strong and easy to work. Maintenance is easy and saved.
This review is about item#34906347.
Production of aluminum quad nut
5
From Japan
On 2018-08-16 17:41:33
I bought it to make 3 mm thick aluminum square nut. Up to now I've cut out from the flat bar with a cermet tipped saw, but because it cuts out small, the thing that I saw was flying with a great momentum, but with this cutting cutter it will not be such a thing just falling down. It meets my purpose of use. I think that it is okay to cut out without much effort. Improvement point thinks that the degree of completeness of the product will rise if including parts that will prevent collapse and I also took time to find what suits it. There is a similar indication in everyone's review.
This review is about item#34906347.
Metal cutting
5
From Japan
On 2018-06-15 11:37:18
1 mm thick 15 cm of stainless steel SUS 304 was cut without problems I did not curl as much as I thought When tried brass 3 mm thick 15 cm, I gave up about 5 cm when I cut it Even with total weight, 3 mm thick was hard, but this price is very satisfying Although I was looking for various things, although it is usually hydraulic, it will cost hundreds of thousands, so it costs less than 1/10
This review is about item#34906347.
Cutting of automobile tire
3
From Japan
On 2018-05-12 22:53:09
I bought it for the purpose of car tire cutting. It was low in rigidity, just caught and twisted the tire, it was not able to cut at all. I think the blade is somewhat, but the main body is still cheap and the material is normal iron. In rabbit there is insufficient rigidity of the main body, but it can not be helped if it is considered to be suitable for price. Because it is usual to cut the original steel sheet.
This review is about item#34906347.
Cut of metal plate of 1 ~ 2 mm
4
From Japan
On 2018-01-04 16:47:47
I cut the metal plate up to about 2 mm mainly. As other people say, it is useless unless you fix it with anchors etc., so those who purchase are cautioned. It is a bit disappointing that one side cut from the structure will become rounded, but it is good to cut out like crisp paper. Considering the amount and function, I think that it is a good product.
This review is about item#34906347.
Cutting of thin plate
5
From Japan
On 2017-12-03 19:34:53
The price cuts well as it is cheap. The accuracy of the parts is not good, but it gets quite satisfactory as it becomes a movement like twisting due to the force of the spring. (It is close to how to use scissors.)
This review is about item#34906347.
Copper plate used for cutting about 0.6 - 1.5 mm
5
From Japan
On 2017-11-07 12:42:19
Although I was worried about usability, I bought it carefully. Sharpness is also perfect and satisfactory.
This review is about item#34906347.
About 100 g of food conveying bracket
4
From Japan
On 2017-09-01 08:50:38
It was used for 2 mm polycarbonate cutting. Cutting surface is good, it is cut out I am satisfied. I feel bent because the hold down is bad. An external clamp is necessary. If you overtighten the pipe mounting bolt of the lever, the pipe will bend (a spacer is required inside the pipe).
This review is about item#34906347.
Cutting of material
5
From Japan
On 2017-06-30 08:58:27
3.2 mm ss 400 has expired. A5052 of 8 mm was impossible (laugh). A 1 mm brass plate can be cut like paper. The body size is not that large, but the lever is long. It seems to be solved by using a hydraulic jack. Since there is no table on which the material is to be placed and it is necessary to move the lever while holding down the material with one hand, it seems to be convenient if you make your own around this material, including material control. Also, it is quite heavy.
This review is about item#34906347.
Aluminum plate cut
5
From Japan
On 2016-06-27 05:23:48
I cut it with scissors and electric tools for metal so far. Once I got to cut it with old-fashioned large shearing at the factory of my acquaintance, I was surprised by its workability, "Is there anything that can be cut easily like this?" I got to this product as a result of searching various things at once. In the photograph I was imagining 50 ~ 60 cm, but actually it is 80 cm in length of the handle alone, in the state of the photograph it exceeds 110 cm and it is quite Gotsui so please be careful. We cut aluminum plates of 2 mm and 3 mm, but it is the best for now. Although it seems to be able to cut down to 30 cm, it can be cut in just a few seconds, even the work is fun for much simplicity. It became a goods I think that I bought the best in the past few years. I just thank Monotaro because I could buy it cheaply with coupons.
This review is about item#34906347.
Cutting of aluminum plate and PVC board
4
From Japan
On 2016-06-10 14:44:19
I do not know because the aluminum has not cut yet, but I bought it because the steel also expires. First I tried cutting 2 mm of PVC board, the work which had been hard worked ended in a few seconds of things and the cut was also very beautiful so I did a lot of post-processing as well. We are planning 3 mm of aluminum board in the near future, but it is a perfect score so far. Acrylic was broken indeed and it did not cut. It was 5 times bigger and heavier tool than I thought from the photograph.
This review is about item#34906347.
Metal Shear
1
From Japan
On 2016-04-25 13:03:26
After placing an order, I noticed that the campaign discount was not reflected, but I got frustrated by a childish answer. Is it possible to revise prices after ordering is a system problem or a personnel problem? Judging that it was a waste of time, the goods arrived late at a later date after paying at the normal price, but the package has damage, damage to the contents body as well. I felt the appeal of the campaign price, but the request for payment of regular price. Even if you inquire, only answers of meaning unknown. Those that arrived are iron scraps. I really regret it. I do not want to go shopping again.
This review is about item#34906347.
Cutting of hardened ribbon steel strip
5
From Japan
On 2016-04-08 14:25:44
I tried 0.5 mm thick quenched ribbon steel (hardness: Hv 500) at hand and it was easy to cut. I think that it is an outstanding tool for cost effectiveness!
This review is about item#34906347.
Site
2
From Japan
On 2015-10-29 00:04:35
Because there is no clearance adjustment function, it seems that the iron plate can only be cut to 1 t. If you modify it with a milling machine so that the clearance can be adjusted with a spacer, it may be able to go even at 9 tons.
This review is about item#34906347.
When cutting a thin plate
2
From Japan
On 2014-03-24 15:41:39
I bought it thought that it would be used at the work site, but I think that the commodity itself is satisfactory because it is difficult to cut unless it is fixed with an anchor.
This review is about item#34906347.
Cutting of aluminum and copper plates
5
From Japan
On 2013-09-04 13:27:56
Although I am not at work, but I make various things with my hobby, I had a hard time cutting the aluminum plate copper plate so that I can thank so beautifully, so easy. If detaching of the handle is easier.
This review is about item#34906347.
Cutting of iron, SUS and aluminum at t 0.5 ~ 2.3
2
From Japan
On 2012-12-16 00:08:22
In my power, it seems that the limit of cutting is stainless steel t 1.5 mm, mild steel plate t 1.6, aluminum t 3.0. If you can cut t2.0 stainless steel, I bought it with my own thought, but it seems to be difficult. It is possible to cut it if the width of t2.0 stainless steel is about 10 mm, but width 40 mm was impossible.
This review is about item#34906347.
Cut the thin plate
3
From Japan
On 2012-11-15 16:43:01
I cut various metal plates of 0.5 mm. Aluminum was cut without problems ○, iron plate remained without cutting last △, stainless steel was not cut longer than iron remaining length × was broken a few times not cut points, but burrs remain dirty . It is regrettable though it is unknown whether it is a plate thickness problem.
This review is about item#34906347.
1 2
Customer Who Viewed This Item Also Viewed
Steel Paper Cutter
Sheet Metal Folding Machine
Lever Shears
Lever Shears Spare Blade
Tabletop hand cutter
Guillotine cutter
DIN rail cutter