Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Anchor Hammering Tool

Anchor Hammering Tool
Sales Price: 64.99 SGD
Review Rating: 4.86
7 Customer Reviews
5 star 6
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
At the time of anchoring
5
From Japan
On 2019-01-04 15:24:37
It is high as a thing, but its usability is very good. Especially when there are obstacles such as angles, it is easy to shoot.
This review is about item#35482885.
When male anchor is driven
4
From Japan
On 2018-11-25 18:57:48
This product is recommended. It was something I knew with what a peer had, It is possible to hit the pin without damaging the screw thread, because it is made strong I liked it very much and bought it. I think that the price is somewhat higher, I would like to have four.
This review is about item#35482885.
Used as the anchor driving stick like the original use of the product
5
From Japan
On 2018-10-31 14:11:34
Work can be done without this, but if there is, it is more efficient. The barrel of the guide is designed to slide with a spring, covering the threaded portion prevents displacement of the punch, and by aligning the angle of the bar with the angle of the anchor, the pin can be stably and reliably driven. There is a reasonable weight, so it is better to drive with a lighter force than ever before.
This review is about item#35482885.
When an all anchor is settled
5
From Japan
On 2017-02-22 21:06:35
Working efficiency was very good because you can hit anchor pins stably without blurring.
This review is about item#35482885.
All anchor hammering
5
From Japan
On 2015-04-20 22:53:28
Usability is very good, but I wanted you to keep fall prevention installed.
This review is about item#35482885.
Drive all anchor
5
From Japan
On 2014-10-07 18:23:44
There is no need to worry about screw threads and worry of hitting the hand is alleviated and it can not be stopped once it is used.
This review is about item#35482885.
Electrical construction
5
From Japan
On 2014-03-06 16:40:43
There are no complaints from using it for a long time since fixing the control board etc. I strongly suggest that if you hit a part to hit the hammer a little more, it will be easy to use as it will not hit your hand when you lose it.
This review is about item#35482885.
1