Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Foot Operated Air Valve

Foot Operated Air Valve
Sales Price: 129.99 SGD
Review Rating: 4.00
1 Customer Reviews
5 star 0
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 1 of 1 Reviews
Air compressor discharge switch
4
From Japan
On 2015-07-28 15:10:21
Even though we used air for the cooling of the process, the manual lever was unsatisfactory during work and was also unsatisfactory for the compressor, which was unsatisfactory, interrupt setting in front of the nozzle switch and ease of operation became. Because the feeling of foot stance was about, I let the interior of a large caliber spring in between so that the reaction was satisfied. If there is explanation of the set sale with the one-touch nozzle, we will not go to the home center again. I can show attached photos if attached file, but sorry.
This review is about item#36921805.
1
Customer Who Viewed This Item Also Viewed
Foot Valve,Air Switch
Foot Switch Valve
Foot Switch for Air
Cool dumbo
Foot valve (4FN)
Foot switch S3 form a foot air valve
2 Way Changeover Valve
Foot valve
Foot Switch
Foot valve