Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Aluminum Bike Pump

Aluminum Bike Pump
Sales Price: -
Review Rating: 2.75
4 Customer Reviews
5 star 0
4 star 1
3 star 1
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Bicycle carry-on items
4
From Japan
On 2016-11-18 18:28:38
It is cheap and economical, making is solid and there is nothing wrong.
This review is about item#37601785.
Carry it with outdoor camping equipment
2
From Japan
On 2013-12-14 09:57:12
For emergency disposable use, or those not asking for satisfaction. Panarezer It is comparative verification from the viewpoint that the same shape is currently used. Both the U.S. type and the English type valve coincided with the mouthpiece, and we were able to put in the air without problem. The problem is that the screws at the connection between the pump handle and the shaft are long and remain on the shaft, so they rub against the pump body during pumping and get caught and there is no smooth operation feeling. Because the shaft is made of iron material, many lubricating oils are applied to rust preventive lubrication because of the iron material, but rust has occurred, and the hand became full of rust when touching the lubricating oil. The feet holding part is so poor that it is thought to be damaged in several times.
This review is about item#37601785.
Used for inflating bicycle tires
2
From Japan
On 2013-09-13 14:44:14
Although it expands when using the handle lever and folds after use, since the red pin which becomes the branch of the lever is not fixed, it falls out with Potri and falls. Is not it permissible to fix it?
This review is about item#37601785.
Puncture repair such as cross bike
3
From Japan
On 2011-07-11 14:10:19
Oil and air leak from the junction of aluminum and plastic from about 350 Kpa of air pressure so that it can not be used. However, it does not matter for minutes to use as a first aid on the go.
This review is about item#37601785.
1