Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Clutch Wire Stopper

Clutch Wire Stopper
Sales Price: 8.99 SGD
Review Rating: 4.12
8 Customer Reviews
5 star 5
4 star 0
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Use for snow removing machine clutch wire
5
From Japan
On 2017-05-06 00:03:45
Because of old type snow removing machine of type, I could not purchase genuine wire, purchased longer wire than genuine wire, cut the wire to the proper length, fixed this wire stopper and fixed it. Since the shape of the screw stop screw is bad and the wire has come out, it is being used as a screwdriver instead of a screw.
This review is about item#41448985.
Spares
5
From Japan
On 2017-05-02 20:19:37
You can use it as it is. No problem. Since I bought it together with other parts, the shipping cost was free and it was saved.
This review is about item#41448985.
To the engine relation for agricultural machinery
5
From Japan
On 2016-04-20 11:45:15
It is saved because there is no place to sell around.
This review is about item#41448985.
Vehicle maintenance
3
From Japan
On 2016-02-26 16:48:15
no problem
This review is about item#41448985.
Bike wire adjustment
3
From Japan
On 2015-10-27 19:38:46
It is convenient to have
This review is about item#41448985.
Emergency first aid measures
5
From Japan
On 2014-10-28 18:46:03
Even if you are maintaining in the bean, even though you are maintaining in the bean, you can use it in emergency first aid or when you cut the wire with position change etc, but we are not missing it at the moment. I think that it is more difficult for people who have holes through which to wire through both sides
This review is about item#41448985.
As motorcycle repair equipment
2
From Japan
On 2014-10-24 00:01:27
It seems easy to use and the quality seems to be good, just the structure that the wire can not penetrate, and it is highly likely to slip out if a heavy load is applied. I think that it is necessary to keep in mind that it can not be used normally for emergency purposes.
This review is about item#41448985.
Brake repair / processing of motorcycle
5
From Japan
On 2014-02-12 16:22:53
Because the motorcycle's brake cable was too long, 2.5mm wire (and outer tube) was trimmed and used for wire end. Since the cable insertion hole does not penetrate, use the other side by penetrating the other side. When that screw tightens the screw, you can make the cable "dogged" so it will be strong. Just attach the screw lock, tighten the screw, and secure with the nut. It is made of brass and durability is unknown, but for now it can be used without any problem. Is it okay with such things? Although I suspected it, I think that it can be used without problems as an emergency use of an accident that Tyco will slip through.
This review is about item#41448985.
1
Customer Who Viewed This Item Also Viewed
Clutch Cables
Circular Sleeve
1.5-3mm Wire Clip
Bolt Clipper
Clutch Cable
Double clip made of stainless steel
Clutch Cable Adjuster
Clutch Cable
Circular Sleeve
Inner Wire Cable
Wrench Screw Set
Inner Wire Set
(31236) Release Hawkball
Long Clutch Cable