Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pierce HEX, SUS410

Pierce HEX, SUS410
Sales Price: 4.89 SGD
Review Rating: 4.50
8 Customer Reviews
5 star 5
4 star 2
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Installation work of metal parts
5
From Japan
On 2019-02-18 15:55:57
We used for screwing work to galvanized steel sheet, but there is no problem at all as quality is external use I'm worried about the weather.
This review is about item#41731566.
Fastening of thin plate
4
From Japan
On 2018-11-01 11:22:55
Things are good. From 5 mm there is a small box sale, but regrettable that there is no 4 mm. It is expensive if you purchase in large quantities.
This review is about item#41731557.
Truck decoration
4
From Japan
On 2018-06-03 07:07:02
I bought it for decorating the truck. But stainless steel can not be fixed unless there is a pilot hole ... Steel can be used without problems.
This review is about item#41731584.
Exterior wall construction
5
From Japan
On 2018-02-07 08:51:24
It is convenient as it can be purchased in units of 1 piece. I am saved because there is no waste
This review is about item#41731636.
Repair of overseas marine air conditioners.
5
From Japan
On 2018-01-04 20:32:45
Because it was with steel incis bis, it was rusted and replaced. I was saved because I did not sell it to my home center. Variation of the screw part was also a lot size perfectly.
This review is about item#41731532.
repair
5
From Japan
On 2016-11-12 12:11:17
Mr. Mon's PB has a strong difference in winning but this is "hit". The sharpness was good.
This review is about item#41731593.
Mounting on thick steel plate
3
From Japan
On 2014-09-26 20:46:16
For installation on a thick steel plate, if it is not 5 mm or more it will be torn off. It is not a crosshair and this nut shape is easy to install.
This review is about item#41731593.
H Metal bracket mounted on steel
5
From Japan
On 2014-06-03 16:01:02
It is useful because it can be used without pilot holes in medium-size steel frame. Sharpness is also good, and there is strength, so it will not break on the way.
This review is about item#41731584.
1
Customer Who Viewed This Item Also Viewed
Hex Self-Drilled Screw
FRX Seal HEX
Pierce HEX (SUS410) (small box)
Hex Head Screw
DORISC Hex
Stainless Jack point hex
Uniqlo Jack point hex
Hex Self-Drilling Screw
LIVEHEX (SUS 410) (packed item)
FRXHEX, SUS410, Pack Product
Drill bis Long HEX (SUS410)
Hex Self-Drilling Screw