Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Waterproof Thermocouple Thermometer

Waterproof Thermocouple Thermometer
Sales Price: 56.99 SGD
Review Rating: 4.00
4 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Food temperature measurement
5
From Japan
On 2018-11-28 11:33:36
I use it in a food factory. Easy to carry, very convenient to use multiple.
This review is about item#48971115.
Production of pipe organ of pipe organ
5
From Japan
On 2016-02-10 22:39:42
It is used for casting temperature measurement when melting tin lead, flowing on a stone table to make a plate. Easy to measure and sufficient accuracy and accuracy.
This review is about item#48971115.
Used in food factory
1
From Japan
On 2015-08-12 06:35:24
Although listed as waterproof, this product is not even a drip-proof specification level. I used it under such circumstances as it took a little water, but it became impossible to use just by using 2 or 3 days. Because it was a situation that could be said as an initial malfunction, we suggested an immediate exchange, but we did not respond, but at the end of the 10 days or more after sending the item, "The cause of the malfunction is the circuit board due to the ingress of water into the inside It is thought that moisture has penetrated through the gap due to incomplete installation of the battery lid as a factor of moisture invasion.The actual item can not be repaired and it will be replaced with new item for a fee. " . Of course, the battery lid was not loose, and if you used it in the purchased state in the first place, I think that it is a line to respond as an initial malfunction. You can not help saying that it is a product with considerable problems selling it as a waterproof product even without drip-proof performance. Since the correspondence of the manufacturer is also the worst, I think whether it is better to purchase this product purchasing person as it is. Please note that it breaks immediately in situations where at least water takes even a little.
This review is about item#48971115.
For checking the center temperature of boil products
5
From Japan
On 2014-06-13 13:34:03
It is a comparison with the thermometer which used before. □ The display screen is large and it is very easy to see. □ Auto off setting is possible, very convenient. □ Since the used battery is CR 2032, we expect that the battery exchange frequency will increase. I think that it is a satisfactory item.
This review is about item#48971115.
1